<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8MP WiFI/BT bring up</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WiFI-BT-bring-up/m-p/1792415#M218965</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;we are working with custom board with same wifi/BT chip which is on EVK Azure wave. But while bring up BT we are facing the bellow error.&lt;/P&gt;&lt;P&gt;root@imx8mp-lpddr4-evk:~# modprobe moal mod_par=nxp/wifi_mod_para.conf&lt;BR /&gt;[ 267.670438] mlan: loading out-of-tree module taints kernel.&lt;BR /&gt;[ 267.730632] moal: unknown parameter 'mod_par' ignored&lt;BR /&gt;[ 267.736039] wlan: Loading MWLAN driver&lt;BR /&gt;[ 267.740482] wlan: Register to Bus Driver...&lt;BR /&gt;[ 267.744925] wlan_pcie 0000:01:00.0: enabling device (0000 -&amp;gt; 0002)&lt;BR /&gt;[ 267.751301] PCI memory map Virt0: 0000000093d84fb3 PCI memory map Virt2: 000000003b66dbc6&lt;BR /&gt;[ 267.759604] Attach moal handle ops, card interface type: 0x204&lt;BR /&gt;[ 267.766298] rps set to 0 from module param&lt;BR /&gt;[ 267.770670] No module param cfg file specified&lt;BR /&gt;[ 267.775162] rx_work=1 cpu_num=4&lt;BR /&gt;[ 267.778340] Enable moal_recv_amsdu_packet&lt;BR /&gt;[ 267.782385] Attach mlan adapter operations.card_type is 0x204.&lt;BR /&gt;[ 267.791900] Request firmware: nxp/pcieuart8997_combo_v4.bin&lt;BR /&gt;[ 268.413534] FW download over, size 622824 bytes&lt;BR /&gt;[ 269.115992] WLAN FW is active&lt;BR /&gt;[ 269.118976] on_time is 269115311500&lt;BR /&gt;[ 269.122490] Please add cal_data_cfg for 8887/8977/8997/8987/8978&lt;BR /&gt;[ 269.128612] woal_request_fw failed&lt;BR /&gt;[ 269.132043] Firmware Init Failed&lt;BR /&gt;[ 269.136737] Free module params&lt;BR /&gt;[ 269.139858] woal_pcie_probe: failed&lt;BR /&gt;[ 269.143350] wlan_pcie: probe of 0000:01:00.0 failed with error -14&lt;BR /&gt;[ 269.149668] wlan: Register to Bus Driver Done&lt;BR /&gt;[ 269.154048] wlan: Driver loaded successfully&lt;BR /&gt;root@imx8mp-lpddr4-evk:~# modprobe btnxpuart&lt;BR /&gt;root@imx8mp-lpddr4-evk:~# hciconfig&lt;BR /&gt;hci0: Type: Primary Bus: UART&lt;BR /&gt;BD Address: 00:00:00:00:00:00 ACL MTU: 0:0 SCO MTU: 0:0&lt;BR /&gt;DOWN&lt;BR /&gt;RX bytes:0 acl:0 sco:0 events:0 errors:0&lt;BR /&gt;TX bytes:4 acl:0 sco:0 commands:1 errors:0&lt;/P&gt;&lt;P&gt;root@imx8mp-lpddr4-evk:~# hciconfig hci0 up&lt;BR /&gt;[ 296.575703] Bluetooth: hci0: Opcode 0x c03 failed: -110&lt;BR /&gt;Can't init device hci0: Connection timed out (110)&lt;BR /&gt;root@imx8mp-lpddr4-evk:~# [ 298.592286] Bluetooth: hci0: Setting baudrate failed (-110)&lt;BR /&gt;[ 300.608296] Bluetooth: hci0: Setting wake-up method failed (-110)&lt;BR /&gt;[ 302.624090] Bluetooth: hci0: Setting baudrate failed (-110)&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Any idea that could help ?&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Sat, 20 Jan 2024 17:42:31 GMT</pubDate>
    <dc:creator>MJD</dc:creator>
    <dc:date>2024-01-20T17:42:31Z</dc:date>
    <item>
      <title>IMX8MP WiFI/BT bring up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WiFI-BT-bring-up/m-p/1792415#M218965</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;we are working with custom board with same wifi/BT chip which is on EVK Azure wave. But while bring up BT we are facing the bellow error.&lt;/P&gt;&lt;P&gt;root@imx8mp-lpddr4-evk:~# modprobe moal mod_par=nxp/wifi_mod_para.conf&lt;BR /&gt;[ 267.670438] mlan: loading out-of-tree module taints kernel.&lt;BR /&gt;[ 267.730632] moal: unknown parameter 'mod_par' ignored&lt;BR /&gt;[ 267.736039] wlan: Loading MWLAN driver&lt;BR /&gt;[ 267.740482] wlan: Register to Bus Driver...&lt;BR /&gt;[ 267.744925] wlan_pcie 0000:01:00.0: enabling device (0000 -&amp;gt; 0002)&lt;BR /&gt;[ 267.751301] PCI memory map Virt0: 0000000093d84fb3 PCI memory map Virt2: 000000003b66dbc6&lt;BR /&gt;[ 267.759604] Attach moal handle ops, card interface type: 0x204&lt;BR /&gt;[ 267.766298] rps set to 0 from module param&lt;BR /&gt;[ 267.770670] No module param cfg file specified&lt;BR /&gt;[ 267.775162] rx_work=1 cpu_num=4&lt;BR /&gt;[ 267.778340] Enable moal_recv_amsdu_packet&lt;BR /&gt;[ 267.782385] Attach mlan adapter operations.card_type is 0x204.&lt;BR /&gt;[ 267.791900] Request firmware: nxp/pcieuart8997_combo_v4.bin&lt;BR /&gt;[ 268.413534] FW download over, size 622824 bytes&lt;BR /&gt;[ 269.115992] WLAN FW is active&lt;BR /&gt;[ 269.118976] on_time is 269115311500&lt;BR /&gt;[ 269.122490] Please add cal_data_cfg for 8887/8977/8997/8987/8978&lt;BR /&gt;[ 269.128612] woal_request_fw failed&lt;BR /&gt;[ 269.132043] Firmware Init Failed&lt;BR /&gt;[ 269.136737] Free module params&lt;BR /&gt;[ 269.139858] woal_pcie_probe: failed&lt;BR /&gt;[ 269.143350] wlan_pcie: probe of 0000:01:00.0 failed with error -14&lt;BR /&gt;[ 269.149668] wlan: Register to Bus Driver Done&lt;BR /&gt;[ 269.154048] wlan: Driver loaded successfully&lt;BR /&gt;root@imx8mp-lpddr4-evk:~# modprobe btnxpuart&lt;BR /&gt;root@imx8mp-lpddr4-evk:~# hciconfig&lt;BR /&gt;hci0: Type: Primary Bus: UART&lt;BR /&gt;BD Address: 00:00:00:00:00:00 ACL MTU: 0:0 SCO MTU: 0:0&lt;BR /&gt;DOWN&lt;BR /&gt;RX bytes:0 acl:0 sco:0 events:0 errors:0&lt;BR /&gt;TX bytes:4 acl:0 sco:0 commands:1 errors:0&lt;/P&gt;&lt;P&gt;root@imx8mp-lpddr4-evk:~# hciconfig hci0 up&lt;BR /&gt;[ 296.575703] Bluetooth: hci0: Opcode 0x c03 failed: -110&lt;BR /&gt;Can't init device hci0: Connection timed out (110)&lt;BR /&gt;root@imx8mp-lpddr4-evk:~# [ 298.592286] Bluetooth: hci0: Setting baudrate failed (-110)&lt;BR /&gt;[ 300.608296] Bluetooth: hci0: Setting wake-up method failed (-110)&lt;BR /&gt;[ 302.624090] Bluetooth: hci0: Setting baudrate failed (-110)&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Any idea that could help ?&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 20 Jan 2024 17:42:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WiFI-BT-bring-up/m-p/1792415#M218965</guid>
      <dc:creator>MJD</dc:creator>
      <dc:date>2024-01-20T17:42:31Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP WiFI/BT bring up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WiFI-BT-bring-up/m-p/1793000#M219014</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223332"&gt;@MJD&lt;/a&gt;!&lt;BR /&gt;Thank you for contacting NXP Support!&lt;BR /&gt;&lt;BR /&gt;The command that you are using is incorrect, you wrote "modprobe moal mod_par=nxp/wifi_mod_para.conf" and the command is "modprobe moal mod_para=nxp/wifi_mod_para.conf"&lt;BR /&gt;&lt;BR /&gt;Best Regards!&lt;BR /&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jan 2024 12:47:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WiFI-BT-bring-up/m-p/1793000#M219014</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-01-22T12:47:15Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP WiFI/BT bring up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WiFI-BT-bring-up/m-p/1833553#M221652</link>
      <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;we got Wifi working but when we try to enable BT, we are facing issue has below&amp;nbsp;&lt;BR /&gt;root@imx8mp-lpddr4-evk:~# modprobe btnxpuart&lt;BR /&gt;root@imx8mp-lpddr4-evk:~# [ 5493.300152] audit: type=1334 audit(1711093391.224:22): prog-id=17 op=LOAD&lt;BR /&gt;[ 5493.307018] audit: type=1334 audit(1711093391.228:23): prog-id=18 op=LOAD&lt;BR /&gt;[ 5496.027423] Bluetooth: hci0: Opcode 0x c03 failed: -110&lt;BR /&gt;[ 5498.043427] Bluetooth: hci0: Setting baudrate failed (-110)&lt;BR /&gt;[ 5500.059421] Bluetooth: hci0: Setting wake-up method failed (-110)&lt;BR /&gt;&lt;BR /&gt;#Bluetooth&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Mar 2024 08:21:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WiFI-BT-bring-up/m-p/1833553#M221652</guid>
      <dc:creator>MJD</dc:creator>
      <dc:date>2024-03-22T08:21:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP WiFI/BT bring up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WiFI-BT-bring-up/m-p/1983798#M230238</link>
      <description>Hi，Could you please info me you how to sovlve this problem?</description>
      <pubDate>Tue, 29 Oct 2024 11:58:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WiFI-BT-bring-up/m-p/1983798#M230238</guid>
      <dc:creator>NealZhang</dc:creator>
      <dc:date>2024-10-29T11:58:44Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP WiFI/BT bring up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WiFI-BT-bring-up/m-p/1984043#M230255</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238713"&gt;@NealZhang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regarding BT it was TX RX connection issue, check the connections.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Oct 2024 17:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-WiFI-BT-bring-up/m-p/1984043#M230255</guid>
      <dc:creator>MJD</dc:creator>
      <dc:date>2024-10-29T17:24:53Z</dc:date>
    </item>
  </channel>
</rss>