<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Audio Codec for i.MX8M Mini</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Audio-Codec-for-i-MX8M-Mini/m-p/1790349#M218815</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227861"&gt;@M8&lt;/a&gt;!&lt;BR /&gt;Thank you for contacting NXP Support!&lt;BR /&gt;&lt;BR /&gt;For carplay, I recommend using iMX8 or iMX8X because are parts compatible with carplay, the iMX8MM doesn't have automotive certification.&lt;BR /&gt;The drivers are implemented on iMX8 and iMX8X I recommend moving for those options.&lt;BR /&gt;&lt;BR /&gt;For the codec, I recommend "WM8960".&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards!&lt;BR /&gt;Chavira&lt;/P&gt;</description>
    <pubDate>Wed, 17 Jan 2024 13:31:16 GMT</pubDate>
    <dc:creator>Chavira</dc:creator>
    <dc:date>2024-01-17T13:31:16Z</dc:date>
    <item>
      <title>Audio Codec for i.MX8M Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-Codec-for-i-MX8M-Mini/m-p/1790228#M218807</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using 8M Mini on a design and we need to support carplay on the same.&lt;/P&gt;&lt;P&gt;Based on 8M Mini datasheet, there is no inbuilt codec for encoding and decoding.&lt;/P&gt;&lt;P&gt;MCIMX6Q-Smart device board has WM8962 and&amp;nbsp;MCIMX8QXP-CPU MEK Platform design has&amp;nbsp;WM8960 as codecs. Which Codec IC would you recommend to be used with 8M Mini to support carplay?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jan 2024 10:26:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-Codec-for-i-MX8M-Mini/m-p/1790228#M218807</guid>
      <dc:creator>M8</dc:creator>
      <dc:date>2024-01-17T10:26:28Z</dc:date>
    </item>
    <item>
      <title>Re: Audio Codec for i.MX8M Mini</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Audio-Codec-for-i-MX8M-Mini/m-p/1790349#M218815</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227861"&gt;@M8&lt;/a&gt;!&lt;BR /&gt;Thank you for contacting NXP Support!&lt;BR /&gt;&lt;BR /&gt;For carplay, I recommend using iMX8 or iMX8X because are parts compatible with carplay, the iMX8MM doesn't have automotive certification.&lt;BR /&gt;The drivers are implemented on iMX8 and iMX8X I recommend moving for those options.&lt;BR /&gt;&lt;BR /&gt;For the codec, I recommend "WM8960".&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards!&lt;BR /&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jan 2024 13:31:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Audio-Codec-for-i-MX8M-Mini/m-p/1790349#M218815</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-01-17T13:31:16Z</dc:date>
    </item>
  </channel>
</rss>