<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PWM interrupt in imxrt1062 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PWM-interrupt-in-imxrt1062/m-p/1789497#M218758</link>
    <description>&lt;P&gt;I am able to generate pwm pulses with what ever parameters required for any modules. I am using this for giving pulses to a stepper motor driver where I need to count the number of pwm pulses given so that I can track the angle the motor rotated.&lt;/P&gt;&lt;P&gt;The method I thought was to count the number of pwm pulses generated. Is there a way to get interrupt triggered for every pwm pulses made by a pwm module. This ISR i need to use for other functionality also apart from counting pulses.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ananth&lt;/P&gt;</description>
    <pubDate>Tue, 16 Jan 2024 12:35:09 GMT</pubDate>
    <dc:creator>Ananth96</dc:creator>
    <dc:date>2024-01-16T12:35:09Z</dc:date>
    <item>
      <title>PWM interrupt in imxrt1062</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PWM-interrupt-in-imxrt1062/m-p/1789497#M218758</link>
      <description>&lt;P&gt;I am able to generate pwm pulses with what ever parameters required for any modules. I am using this for giving pulses to a stepper motor driver where I need to count the number of pwm pulses given so that I can track the angle the motor rotated.&lt;/P&gt;&lt;P&gt;The method I thought was to count the number of pwm pulses generated. Is there a way to get interrupt triggered for every pwm pulses made by a pwm module. This ISR i need to use for other functionality also apart from counting pulses.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ananth&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jan 2024 12:35:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PWM-interrupt-in-imxrt1062/m-p/1789497#M218758</guid>
      <dc:creator>Ananth96</dc:creator>
      <dc:date>2024-01-16T12:35:09Z</dc:date>
    </item>
    <item>
      <title>Re: PWM interrupt in imxrt1062</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PWM-interrupt-in-imxrt1062/m-p/1790549#M218837</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;With the eFlexPWM is possible to generate interrupts with the generation of PWM signals when &lt;EM&gt;VAL2&lt;/EM&gt; and &lt;EM&gt;VAL3&lt;/EM&gt; compare values are meet in &lt;EM&gt;channel A&lt;/EM&gt;, such values indicates the &lt;EM&gt;turn-on edge&lt;/EM&gt; and the &lt;EM&gt;turn-off edge&lt;/EM&gt; if the signal. The same applies for &lt;EM&gt;VAL4&lt;/EM&gt; and &lt;EM&gt;VAL5&lt;/EM&gt; in &lt;EM&gt;channel B&lt;/EM&gt;.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="_Leo__0-1705525013674.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/258673i9298C144E577218A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="_Leo__0-1705525013674.png" alt="_Leo__0-1705525013674.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jan 2024 20:57:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PWM-interrupt-in-imxrt1062/m-p/1790549#M218837</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2024-01-17T20:57:51Z</dc:date>
    </item>
  </channel>
</rss>