<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Example Reference IMX RT 1020 running without SDRAM MCUXpresso Project in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Example-Reference-IMX-RT-1020-running-without-SDRAM-MCUXpresso/m-p/1789444#M218751</link>
    <description>&lt;P&gt;Morning All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I am looking for example / ref of 1020 running without SDRAM (MCUXpresso)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I am on a custom 1020 without SDRAM but XIP with Segger and flashing fine&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Violates at runtime&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Modified SDK's do not provide a stable solution&lt;/P&gt;&lt;P&gt;Best Wishes&lt;/P&gt;&lt;P&gt;Don't hesitate to ask further questions&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 16 Jan 2024 10:46:51 GMT</pubDate>
    <dc:creator>Vliermaal</dc:creator>
    <dc:date>2024-01-16T10:46:51Z</dc:date>
    <item>
      <title>Example Reference IMX RT 1020 running without SDRAM MCUXpresso Project</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Example-Reference-IMX-RT-1020-running-without-SDRAM-MCUXpresso/m-p/1789444#M218751</link>
      <description>&lt;P&gt;Morning All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I am looking for example / ref of 1020 running without SDRAM (MCUXpresso)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I am on a custom 1020 without SDRAM but XIP with Segger and flashing fine&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Violates at runtime&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Modified SDK's do not provide a stable solution&lt;/P&gt;&lt;P&gt;Best Wishes&lt;/P&gt;&lt;P&gt;Don't hesitate to ask further questions&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jan 2024 10:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Example-Reference-IMX-RT-1020-running-without-SDRAM-MCUXpresso/m-p/1789444#M218751</guid>
      <dc:creator>Vliermaal</dc:creator>
      <dc:date>2024-01-16T10:46:51Z</dc:date>
    </item>
    <item>
      <title>Re: Example Reference IMX RT 1020 running without SDRAM MCUXpresso Project</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Example-Reference-IMX-RT-1020-running-without-SDRAM-MCUXpresso/m-p/1790565#M218840</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;One way you can try the SDK examples without using SDRAM is to reallocate the code or the compiled objects and link them to flash by modifying the linker file.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jan 2024 22:14:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Example-Reference-IMX-RT-1020-running-without-SDRAM-MCUXpresso/m-p/1790565#M218840</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-01-17T22:14:08Z</dc:date>
    </item>
  </channel>
</rss>