<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX6 Laird Support</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Laird-Support/m-p/1789102#M218735</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/193268"&gt;@MichaelBMiner&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer lrd-11 version guide&lt;/P&gt;
&lt;P&gt;&lt;A href="https://lairdcp.github.io/guides/LWBp-tutorials/1.0/lrd11/imx6ullevk-lwbplus-lrd-11.html" target="_blank"&gt;https://lairdcp.github.io/guides/LWBp-tutorials/1.0/lrd11/imx6ullevk-lwbplus-lrd-11.html&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 16 Jan 2024 03:20:50 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2024-01-16T03:20:50Z</dc:date>
    <item>
      <title>IMX6 Laird Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Laird-Support/m-p/1788177#M218654</link>
      <description>&lt;P&gt;I have been following&amp;nbsp;&lt;A href="https://lairdcp.github.io/guides/LWBp-tutorials/1.0/imx6ullevk-lwbplus.html" target="_blank" rel="noopener"&gt;this guide&lt;/A&gt;&amp;nbsp;to add meta-summit-laird to my image. I am using Hardknott 3.3 and the meta-summit-laird-pre-3.4 layer. Today I finally got the radio to be recognized by the kernel and show up in ifconfig.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx6ull14x14evk:~# ifconfig
eth0      Link encap:Ethernet  HWaddr E2:EE:EE:EE:EE:EE
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

lo        Link encap:Local Loopback
          inet addr:127.0.0.1  Mask:255.0.0.0
          inet6 addr: ::1/128 Scope:Host
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:9360 errors:0 dropped:0 overruns:0 frame:0
          TX packets:9360 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:581440 (567.8 KiB)  TX bytes:581440 (567.8 KiB)

wlan0     Link encap:Ethernet  HWaddr C0:EE:40:84:83:AA
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

root@imx6ull14x14evk:~# iw dev
phy#0
        Unnamed/non-netdev interface
                wdev 0x2
                addr c2:ee:40:84:83:aa
                type P2P-device
                txpower 31.00 dBm
        Interface wlan0
                ifindex 5
                wdev 0x1
                addr c0:ee:40:84:83:aa
                type managed
                channel 1 (2412 MHz), width: 20 MHz, center1: 2412 MHz
                txpower 31.00 dBm&lt;/LI-CODE&gt;&lt;P&gt;Now I am trying to connect to a network but I do not have wpa_supplicant or nmcli. This is a point of frustration to me.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In local.conf I have&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;PREFERRED_RPROVIDER_wpa-supplicant = "summit-supplicant-lwb"
PREFERRED_RPROVIDER_wpa-supplicant-cli = "summit-supplicant-lwb"
PREFERRED_RPROVIDER_wpa-supplicant-passphrase = "summit-supplicant-lwb"
   
BBMASK += " \
    meta-summit-radio/meta-summit-radio-pre-3.4/recipes-packages/openssl \
    meta-summit-radio/meta-summit-radio-pre-3.4/recipes-packages/.*/.*openssl10.* \
    "
   
PREFERRED_RPROVIDER_wireless-regdb-static = "reg-lwb5-plus"
LWB_REGDOMAIN = "US"&lt;/LI-CODE&gt;&lt;P&gt;In my image file I have&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;# Install necessary libraries
IMAGE_INSTALL_append = " packagegroup-core-ssh-openssh \
    openssl \
    can-utils \
    libsocketcan \
    sudo \
    boost \
    lumissil-kernel-module \
    lumissil \
    logrotate \
    socat \
    u-boot-fw-utils \
    open-plc-utils \
    dbcppp \
    i2c-tools \
    firmware-imx-sdma-imx6q \
    iproute2 \
    rng-tools \
    ca-certificates \
    tzdata \
    alsa-utils \
    htop \
    ethtool \
    iperf3 \
    tcpdump \
    iw wpa-supplicant \
    libgpiod \
    libgpiod-tools \
    hostapd \
    laird-localize-firmware \
    networkinterfaces \
    "
# Laird Libraries    
IMAGE_INSTALL_append = " \
    kernel-module-lwb5p-backports-summit \
    lwb5plus-sdio-sa-firmware \
    summit-supplicant-lwb \
    summit-networkmanager-lwb \
    "&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I program my board or look at the files-in-image.txt I can see&amp;nbsp;-rwxr-xr-x root root 84488 ./usr/sbin/wpa_cli is installed but no other networking tools.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know that the laird recipes remove and provide their own version of wpa_supplicant but they appear to be missing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For more information I am using laird version&amp;nbsp;&lt;A href="https://github.com/LairdCP/meta-summit-radio/tree/lrd-11.39.0.x/meta-summit-radio" target="_self"&gt;lrd-11.39.0.x&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jan 2024 17:57:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Laird-Support/m-p/1788177#M218654</guid>
      <dc:creator>MichaelBMiner</dc:creator>
      <dc:date>2024-01-12T17:57:52Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Laird Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Laird-Support/m-p/1789102#M218735</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/193268"&gt;@MichaelBMiner&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer lrd-11 version guide&lt;/P&gt;
&lt;P&gt;&lt;A href="https://lairdcp.github.io/guides/LWBp-tutorials/1.0/lrd11/imx6ullevk-lwbplus-lrd-11.html" target="_blank"&gt;https://lairdcp.github.io/guides/LWBp-tutorials/1.0/lrd11/imx6ullevk-lwbplus-lrd-11.html&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jan 2024 03:20:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Laird-Support/m-p/1789102#M218735</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-01-16T03:20:50Z</dc:date>
    </item>
  </channel>
</rss>