<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic yocto error in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/yocto-error/m-p/1788735#M218705</link>
    <description>&lt;P&gt;Hello!&lt;BR /&gt;I'm using the branch imx-linux-sumo, the bsp is imx-4.14.98-2.2.0.xml. Based on DISTRO=fsl-imx-xwayland on IMX6Q machine. The following two issue is encountered during the build:&lt;/P&gt;&lt;P&gt;| ninja: build stopped: subcommand failed.&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| ERROR: Function failed: do_compile (log file is located at /home/heshao/imx-yocto-bsp/bld-xwayland/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.1.0 r0/temp /log.do_compile.101040)&lt;BR /&gt;ERROR: Task (/home/heshao/imx-yocto-bsp/sources/poky/meta/recipes-graphics/vulkan/assimp_4.1.0.bb:do_compile) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 3963 tasks of which 0 didn't need to be rerun and 2 failed.&lt;/P&gt;&lt;P&gt;Summary: 2 tasks failed:&lt;BR /&gt;/home/heshao/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-devtools/fmt/fmt_5.3.0.bb:do_compile&lt;BR /&gt;/home/heshao/imx-yocto-bsp/sources/poky/meta/recipes-graphics/vulkan/assimp_4.1.0.bb:do_compile&lt;/P&gt;&lt;P&gt;Below is the error log! How do you think this can be resolved?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 15 Jan 2024 11:06:56 GMT</pubDate>
    <dc:creator>rainho</dc:creator>
    <dc:date>2024-01-15T11:06:56Z</dc:date>
    <item>
      <title>yocto error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-error/m-p/1788735#M218705</link>
      <description>&lt;P&gt;Hello!&lt;BR /&gt;I'm using the branch imx-linux-sumo, the bsp is imx-4.14.98-2.2.0.xml. Based on DISTRO=fsl-imx-xwayland on IMX6Q machine. The following two issue is encountered during the build:&lt;/P&gt;&lt;P&gt;| ninja: build stopped: subcommand failed.&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| ERROR: Function failed: do_compile (log file is located at /home/heshao/imx-yocto-bsp/bld-xwayland/tmp/work/cortexa9hf-neon-poky-linux-gnueabi/assimp/4.1.0 r0/temp /log.do_compile.101040)&lt;BR /&gt;ERROR: Task (/home/heshao/imx-yocto-bsp/sources/poky/meta/recipes-graphics/vulkan/assimp_4.1.0.bb:do_compile) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 3963 tasks of which 0 didn't need to be rerun and 2 failed.&lt;/P&gt;&lt;P&gt;Summary: 2 tasks failed:&lt;BR /&gt;/home/heshao/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-devtools/fmt/fmt_5.3.0.bb:do_compile&lt;BR /&gt;/home/heshao/imx-yocto-bsp/sources/poky/meta/recipes-graphics/vulkan/assimp_4.1.0.bb:do_compile&lt;/P&gt;&lt;P&gt;Below is the error log! How do you think this can be resolved?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jan 2024 11:06:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-error/m-p/1788735#M218705</guid>
      <dc:creator>rainho</dc:creator>
      <dc:date>2024-01-15T11:06:56Z</dc:date>
    </item>
    <item>
      <title>Re: yocto error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-error/m-p/1790810#M218855</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The old BSP was tested on Ubuntu 16.04, so firstly make sure that you have followed the &amp;lt;Host setup&amp;gt; of this Yocto User guide.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;And bitbake recipe, bitbake&amp;nbsp;&lt;SPAN&gt;assimp, bitbake fmp. if works, bitbake &amp;lt;image&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Also, check your CPU threads.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jan 2024 06:58:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-error/m-p/1790810#M218855</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-01-18T06:58:04Z</dc:date>
    </item>
    <item>
      <title>Re: yocto error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-error/m-p/1791499#M218903</link>
      <description>&lt;P&gt;Hi, thanks for your reply!&lt;BR /&gt;I've canceled the build of the last version. I wanted to use 4.9.88BSP, so I used imx-4.9.88-2.1.0-8mm_alpha.xml for my project this time. During this process, I encountered a compile imx-gpu-sdk error, which I solved by replacing the bb file. But during the final packaging, the following log error about the kernel occurred. Can you help me review it?&lt;/P&gt;&lt;P&gt;In the end, my CPU was i512400, with 16GB of memory. I used VAWARE UBUNTU 1804, with 8 allocated cores and 10GB of memory!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;ERROR: linux-imx-4.9.88-r0 do_package_write_ipk: Error executing a python function in exec_python_func() autogenerated:&lt;/P&gt;&lt;P&gt;The stack trace of python calls that resulted in this exception/failure was:&lt;BR /&gt;File: 'exec_python_func() autogenerated', lineno: 2, function: &amp;lt;module&amp;gt;&lt;BR /&gt;0001:&lt;BR /&gt;*** 0002:do_package_ipk(d)&lt;BR /&gt;0003:&lt;BR /&gt;File: '/home/heshao/imx-yocto-bsp/sources/poky/meta/classes/package_ipk.bbclass', lineno: 87, function: do_package_ipk&lt;BR /&gt;0083:&lt;BR /&gt;0084: os.chdir(oldcwd)&lt;BR /&gt;0085:&lt;BR /&gt;0086: if error:&lt;BR /&gt;*** 0087: raise error&lt;BR /&gt;0088:}&lt;BR /&gt;0089:do_package_ipk[vardeps] += "ipk_write_pkg"&lt;BR /&gt;0090:do_package_ipk[vardepsexclude] = "BB_NUMBER_THREADS"&lt;BR /&gt;0091:&lt;BR /&gt;Exception: subprocess.CalledProcessError: Command 'PATH="/home/heshao/imx-yocto-bsp/sources/poky/scripts:/home/heshao/imx-yocto-bsp/bld-fb/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/recipe-sysroot-native/usr/bin/arm-poky-linux-gnueabi:/home/heshao/imx-yocto-bsp/bld-fb/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/recipe-sysroot/usr/bin/crossscripts:/home/heshao/imx-yocto-bsp/bld-fb/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/recipe-sysroot-native/usr/sbin:/home/heshao/imx-yocto-bsp/bld-fb/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/recipe-sysroot-native/usr/bin:/home/heshao/imx-yocto-bsp/bld-fb/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/recipe-sysroot-native/sbin:/home/heshao/imx-yocto-bsp/bld-fb/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/recipe-sysroot-native/bin:/home/heshao/imx-yocto-bsp/sources/poky/bitbake/bin:/home/heshao/imx-yocto-bsp/bld-fb/tmp/hosttools" opkg-build kernel-module-libcrc32c-4.9.88-imx_4.9.88_imx8mm_alpha+g7bae8af57abb /home/heshao/imx-yocto-bsp/bld-fb/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/deploy-ipks/imx6qsabresd' returned non-zero exit status 1.&lt;/P&gt;&lt;P&gt;Subprocess output:&lt;BR /&gt;kernel-module-libcrc32c-4.9.88-imx_4.9.88_imx8mm_alpha+g7bae8af57abb&lt;BR /&gt;*** Error: Package name contains illegal characters, (other than [a-z0-9.+-])&lt;/P&gt;&lt;P&gt;opkg-build: Please fix the above errors and try again.&lt;/P&gt;&lt;P&gt;ERROR: linux-imx-4.9.88-r0 do_package_write_ipk: Function failed: do_package_ipk&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/heshao/imx-yocto-bsp/bld-fb/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/4.9.88-r0/temp/log.do_package_write_ipk.26353&lt;BR /&gt;ERROR: Task (/home/heshao/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx_4.9.88.bb:do_package_write_ipk) failed with exit code '1'&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jan 2024 02:57:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-error/m-p/1791499#M218903</guid>
      <dc:creator>rainho</dc:creator>
      <dc:date>2024-01-19T02:57:20Z</dc:date>
    </item>
    <item>
      <title>Re: yocto error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-error/m-p/1791513#M218904</link>
      <description>&lt;P&gt;Hi, thanks for your reply!&lt;BR /&gt;I've canceled the build of the last version. I wanted to use 4.9.88BSP, so I used imx-4.9.88-2.1.0-8mm_alpha.xml for my project this time. During this process, I encountered a compile imx-gpu-sdk error, which I solved by replacing the bb file. But during the final packaging, the following log error about the kernel occurred. Can you help me review it?&lt;/P&gt;&lt;P&gt;Finally, my CPU was i512400, with 16GB of memory. I used VAWARE UBUNTU1804, with 8 allocated cores and 10GB of memory.&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jan 2024 03:22:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-error/m-p/1791513#M218904</guid>
      <dc:creator>rainho</dc:creator>
      <dc:date>2024-01-19T03:22:13Z</dc:date>
    </item>
    <item>
      <title>Re: yocto error</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/yocto-error/m-p/1792380#M218956</link>
      <description>&lt;P&gt;&lt;SPAN&gt;"with 8 allocated cores and 10GB of memory" I think that the allocation will cause the compilation error. Have a try to reduce the BB threads -&amp;nbsp;&lt;A href="https://docs.yoctoproject.org/dev-manual/speeding-up-build.html?highlight=bb_number_threads" target="_blank"&gt;13 Speeding Up a Build — The Yocto Project ® 4.3.999 documentation&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 20 Jan 2024 06:02:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/yocto-error/m-p/1792380#M218956</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-01-20T06:02:24Z</dc:date>
    </item>
  </channel>
</rss>