<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMIMXRT1040 - Manufacturing using command line</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1040-Manufacturing-using-command-line/m-p/1788019#M218639</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to organize the manufacturing process using a XRT1040. My application will have to be signed with HAB and Encrypted with OTPMK.&lt;/P&gt;&lt;P&gt;Untill now, all the test I did were made with Secure Provisioning Tool (V 7.0) using the "Write image" tab or using the tools&amp;gt;Manufacturing Tool enviroment.&lt;/P&gt;&lt;P&gt;Now I have to make a step forward because it is not possible to use the Manufacturing Tool in an automatic line process, so I would have the command lines to replicate the procedure.&lt;BR /&gt;&lt;BR /&gt;I tried to replicate what I read in the log windows of SPT after using the Manufacturing Tool&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="riccardo_carlot_0-1705061782772.png" style="width: 685px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/257997iDEF295A63219C559/image-dimensions/685x273?v=v2" width="685" height="273" role="button" title="riccardo_carlot_0-1705061782772.png" alt="riccardo_carlot_0-1705061782772.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;riccardo_carlot_0-1705061782772.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;gt;init_flashloader_win.bat sdphost_connect "-u e80536af"&amp;#29;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;gt;write_image_win.bat close_HAB burn_BEE_key_selection burn_SRK_fuses sdphost_connect "-u e80536af" set_sdphost_baud_rate 115200 blhost_connect "-u a58b2e2d" manufacturing_task_no 0&amp;#29;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I launhced the same commands from the same folders. The procedure runs without errors and the application stars properly. But reading the memory content I discovered that the application saved in flash was in plain text, wihtout any encryption applied.&lt;/P&gt;&lt;P&gt;My question... what is the correct procedure to replicate the Manufacturing Tool passages using the command lines?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 12 Jan 2024 12:36:14 GMT</pubDate>
    <dc:creator>riccardo_carlot</dc:creator>
    <dc:date>2024-01-12T12:36:14Z</dc:date>
    <item>
      <title>MIMXRT1040 - Manufacturing using command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1040-Manufacturing-using-command-line/m-p/1788019#M218639</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to organize the manufacturing process using a XRT1040. My application will have to be signed with HAB and Encrypted with OTPMK.&lt;/P&gt;&lt;P&gt;Untill now, all the test I did were made with Secure Provisioning Tool (V 7.0) using the "Write image" tab or using the tools&amp;gt;Manufacturing Tool enviroment.&lt;/P&gt;&lt;P&gt;Now I have to make a step forward because it is not possible to use the Manufacturing Tool in an automatic line process, so I would have the command lines to replicate the procedure.&lt;BR /&gt;&lt;BR /&gt;I tried to replicate what I read in the log windows of SPT after using the Manufacturing Tool&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="riccardo_carlot_0-1705061782772.png" style="width: 685px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/257997iDEF295A63219C559/image-dimensions/685x273?v=v2" width="685" height="273" role="button" title="riccardo_carlot_0-1705061782772.png" alt="riccardo_carlot_0-1705061782772.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;riccardo_carlot_0-1705061782772.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;gt;init_flashloader_win.bat sdphost_connect "-u e80536af"&amp;#29;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;gt;write_image_win.bat close_HAB burn_BEE_key_selection burn_SRK_fuses sdphost_connect "-u e80536af" set_sdphost_baud_rate 115200 blhost_connect "-u a58b2e2d" manufacturing_task_no 0&amp;#29;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I launhced the same commands from the same folders. The procedure runs without errors and the application stars properly. But reading the memory content I discovered that the application saved in flash was in plain text, wihtout any encryption applied.&lt;/P&gt;&lt;P&gt;My question... what is the correct procedure to replicate the Manufacturing Tool passages using the command lines?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jan 2024 12:36:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1040-Manufacturing-using-command-line/m-p/1788019#M218639</guid>
      <dc:creator>riccardo_carlot</dc:creator>
      <dc:date>2024-01-12T12:36:14Z</dc:date>
    </item>
  </channel>
</rss>