<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX8QXP PMIC I2C</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QXP-PMIC-I2C/m-p/1785487#M218482</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Yes, you are correct the PMIC is managed by the SCFW on a private I2C bus.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Tue, 09 Jan 2024 19:37:07 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2024-01-09T19:37:07Z</dc:date>
    <item>
      <title>iMX8QXP PMIC I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QXP-PMIC-I2C/m-p/1784889#M218417</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a custom board using iMX8QXP. It has an EEPROM and an RTC connected to the PMIC_I2C lines.&lt;/P&gt;&lt;P&gt;While looking into the reference manual (IMX8DQXPRM), I found the PMIC_I2C module at section 9.1.11- SCU Pin Assignments. Does this mean that the PMIC_I2C can be accessed only from the SCFW? Can the A35 core access the above I2C?&lt;/P&gt;&lt;P&gt;Could someone please clarify this?&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;MJames&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jan 2024 05:44:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QXP-PMIC-I2C/m-p/1784889#M218417</guid>
      <dc:creator>MJames</dc:creator>
      <dc:date>2024-01-09T05:44:44Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8QXP PMIC I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8QXP-PMIC-I2C/m-p/1785487#M218482</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Yes, you are correct the PMIC is managed by the SCFW on a private I2C bus.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jan 2024 19:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8QXP-PMIC-I2C/m-p/1785487#M218482</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2024-01-09T19:37:07Z</dc:date>
    </item>
  </channel>
</rss>