<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: bluez5 do_compile undefined reference to `packet_print_error'</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/bluez5-do-compile-undefined-reference-to-packet-print-error/m-p/1783481#M218270</link>
    <description>&lt;P&gt;The one seems having the same problem as&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/tcp-wrappers-7-6-do-compile-undefined-reference/td-p/1782954" target="_blank"&gt;tcp-wrappers_7.6 do compile undefined reference - NXP Community&lt;/A&gt;, please refer to the steps there.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
    <pubDate>Fri, 05 Jan 2024 08:09:32 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2024-01-05T08:09:32Z</dc:date>
    <item>
      <title>bluez5 do_compile undefined reference to `packet_print_error'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bluez5-do-compile-undefined-reference-to-packet-print-error/m-p/1782761#M218198</link>
      <description>&lt;P&gt;repo init -u &lt;A href="https://github.com/nxp-imx/imx-manifest" target="_blank"&gt;https://github.com/nxp-imx/imx-manifest&lt;/A&gt; -b imx-linux-mickledore -m imx-6.1.36-2.1.0.xml&lt;/P&gt;&lt;P&gt;DISTRO=fsl-imx-xwayland MACHINE=imx6qpsabresd source imx-setup-release.sh -b build-qpxwayland&lt;/P&gt;&lt;P&gt;bitbake imx-image-full&lt;/P&gt;&lt;P&gt;nitialising tasks: 100% |########################################################################################################################################| Time: 0:00:04&lt;BR /&gt;Sstate summary: Wanted 449 Local 0 Mirrors 0 Missed 449 Current 3812 (0% match, 89% complete)&lt;BR /&gt;NOTE: Executing Tasks&lt;BR /&gt;ERROR: bluez5-5.66-r0 do_compile: oe_runmake failed&lt;BR /&gt;ERROR: bluez5-5.66-r0 do_compile: ExecutionError('/home/tjt/src/yocto_imx/build-qpxwayland/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/bluez5/5.66-r0/temp/run.do_compile.765468', 1, None, None)&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/tjt/src/yocto_imx/build-qpxwayland/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/bluez5/5.66-r0/temp/log.do_compile.765468&lt;BR /&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing python function autotools_aclocals&lt;BR /&gt;| DEBUG: SITE files ['endian-little', 'bit-32', 'arm-common', 'arm-32', 'common-linux', 'common-glibc', 'arm-linux', 'arm-linux-gnueabi', 'common']&lt;BR /&gt;| DEBUG: Python function autotools_aclocals finished&lt;BR /&gt;| DEBUG: Executing shell function do_compile&lt;BR /&gt;| NOTE: make -j 1&lt;/P&gt;&lt;P&gt;......&lt;/P&gt;&lt;P&gt;ky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/12.3.0/ld: monitor/att.o: in function `att_find_info_rsp':&lt;BR /&gt;| /usr/src/debug/bluez5/5.66-r0/monitor/att.c:2478: undefined reference to `packet_hexdump'&lt;BR /&gt;| /home/tjt/src/yocto_imx/build-qpxwayland/tmp/work/cortexa9t2hf-neon-poky-linux-gnueabi/bluez5/5.66-r0/recipe-sysroot-native/usr/bin/arm-poky-linux-gnueabi/../../libexec/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/12.3.0/ld: monitor/att.o:/usr/src/debug/bluez5/5.66-r0/monitor/att.c:2819: more undefined references to `packet_hexdump' follow&lt;BR /&gt;| collect2: error: ld returned 1 exit status&lt;BR /&gt;| make[1]: *** [Makefile:5693: monitor/btmon] Error 1&lt;BR /&gt;| ERROR: oe_runmake failed&lt;BR /&gt;| WARNING: exit code 1 from a shell command.&lt;BR /&gt;| make: *** [Makefile:4472: all] Error 2&lt;BR /&gt;ERROR: Task (/home/tjt/src/yocto_imx/sources/poky/meta/recipes-connectivity/bluez5/bluez5_5.66.bb:do_compile) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 2416 tasks of which 2415 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;BR /&gt;/home/tjt/src/yocto_imx/sources/poky/meta/recipes-connectivity/bluez5/bluez5_5.66.bb:do_compile&lt;BR /&gt;Summary: There were 2 ERROR messages, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jan 2024 06:58:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bluez5-do-compile-undefined-reference-to-packet-print-error/m-p/1782761#M218198</guid>
      <dc:creator>gufengzi</dc:creator>
      <dc:date>2024-01-04T06:58:22Z</dc:date>
    </item>
    <item>
      <title>Re: bluez5 do_compile undefined reference to `packet_print_error'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/bluez5-do-compile-undefined-reference-to-packet-print-error/m-p/1783481#M218270</link>
      <description>&lt;P&gt;The one seems having the same problem as&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/tcp-wrappers-7-6-do-compile-undefined-reference/td-p/1782954" target="_blank"&gt;tcp-wrappers_7.6 do compile undefined reference - NXP Community&lt;/A&gt;, please refer to the steps there.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jan 2024 08:09:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/bluez5-do-compile-undefined-reference-to-packet-print-error/m-p/1783481#M218270</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-01-05T08:09:32Z</dc:date>
    </item>
  </channel>
</rss>