<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx8mp evk kernel 6.1.36: m7 stops when linux kernel boots, seems to be a clock issue.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-evk-kernel-6-1-36-m7-stops-when-linux-kernel-boots-seems/m-p/1781707#M218093</link>
    <description>&lt;P&gt;We have a m7 issue on the imx8mp, which we could replicate with the evk-board and the evk-image with the kernel version 6.1.36.&lt;/P&gt;&lt;P&gt;We start any included m7 binary in ram in u-boot with the bootaux command and everything works. When we start the linux kernel the m7 stops.&lt;/P&gt;&lt;P&gt;If we add "clk_ignore_unused" to optargs in uboot the m7 keeps running and everything works fine. It seems like a clock gets (temporarly?) deactivated. We only see this with kernel version 6.x, with 5.x everything is fine.&lt;/P&gt;&lt;P&gt;the m7 runs on the sys_pll1 clock in the example binaries, which should not get deactivated, so we dont know what is going on. Can you help us here?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Tue, 02 Jan 2024 12:53:46 GMT</pubDate>
    <dc:creator>kaihus</dc:creator>
    <dc:date>2024-01-02T12:53:46Z</dc:date>
    <item>
      <title>imx8mp evk kernel 6.1.36: m7 stops when linux kernel boots, seems to be a clock issue.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-evk-kernel-6-1-36-m7-stops-when-linux-kernel-boots-seems/m-p/1781707#M218093</link>
      <description>&lt;P&gt;We have a m7 issue on the imx8mp, which we could replicate with the evk-board and the evk-image with the kernel version 6.1.36.&lt;/P&gt;&lt;P&gt;We start any included m7 binary in ram in u-boot with the bootaux command and everything works. When we start the linux kernel the m7 stops.&lt;/P&gt;&lt;P&gt;If we add "clk_ignore_unused" to optargs in uboot the m7 keeps running and everything works fine. It seems like a clock gets (temporarly?) deactivated. We only see this with kernel version 6.x, with 5.x everything is fine.&lt;/P&gt;&lt;P&gt;the m7 runs on the sys_pll1 clock in the example binaries, which should not get deactivated, so we dont know what is going on. Can you help us here?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jan 2024 12:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-evk-kernel-6-1-36-m7-stops-when-linux-kernel-boots-seems/m-p/1781707#M218093</guid>
      <dc:creator>kaihus</dc:creator>
      <dc:date>2024-01-02T12:53:46Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp evk kernel 6.1.36: m7 stops when linux kernel boots, seems to be a clock issue.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-evk-kernel-6-1-36-m7-stops-when-linux-kernel-boots-seems/m-p/1781796#M218105</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227660"&gt;@kaihus&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I hope you're doing well!&lt;/P&gt;
&lt;P&gt;Please try with our latest BSP release (6.1.55_2.2.0​) found at&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;Embedded Linux for i.MX Applications Processors | NXP Semiconductors&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Let me know if the issue still persists after this.&lt;/P&gt;
&lt;P&gt;Thank you.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Hector.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jan 2024 18:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-evk-kernel-6-1-36-m7-stops-when-linux-kernel-boots-seems/m-p/1781796#M218105</guid>
      <dc:creator>hector_delgado</dc:creator>
      <dc:date>2024-01-02T18:28:24Z</dc:date>
    </item>
  </channel>
</rss>