<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRT1176 wake up</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-wake-up/m-p/1781097#M218013</link>
    <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;We are using Rt1176 MCU in our custom board.the wake up pin connected to NOR gate output and NOR gate input will be&amp;nbsp; 2 Digital inputs where MCU should wake up when the digital inputs are High.&lt;/P&gt;&lt;P&gt;In EVK the wake up pin is connected to switch and acts as trigger input.&lt;/P&gt;&lt;P&gt;In our custom board the NOR gate output will remains low until the Digital inputs are low. Is this ok to leave wake up at low state after MCU wakeup?&lt;/P&gt;&lt;P&gt;Attached is the Schematics of wake up pin circuit.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 29 Dec 2023 06:08:30 GMT</pubDate>
    <dc:creator>Chethanbg</dc:creator>
    <dc:date>2023-12-29T06:08:30Z</dc:date>
    <item>
      <title>RT1176 wake up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-wake-up/m-p/1781097#M218013</link>
      <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;We are using Rt1176 MCU in our custom board.the wake up pin connected to NOR gate output and NOR gate input will be&amp;nbsp; 2 Digital inputs where MCU should wake up when the digital inputs are High.&lt;/P&gt;&lt;P&gt;In EVK the wake up pin is connected to switch and acts as trigger input.&lt;/P&gt;&lt;P&gt;In our custom board the NOR gate output will remains low until the Digital inputs are low. Is this ok to leave wake up at low state after MCU wakeup?&lt;/P&gt;&lt;P&gt;Attached is the Schematics of wake up pin circuit.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Dec 2023 06:08:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1176-wake-up/m-p/1781097#M218013</guid>
      <dc:creator>Chethanbg</dc:creator>
      <dc:date>2023-12-29T06:08:30Z</dc:date>
    </item>
    <item>
      <title>Re: RT1176 wake up</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-wake-up/m-p/1781194#M218022</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200437"&gt;@Chethanbg&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp; In fact, no matter how you connect.&lt;/P&gt;
&lt;P&gt;&amp;nbsp; &amp;nbsp;If your WAKEUP pin is low, it will wakeup the chip from the low power mode, so I think, your situation is the same as the EVK, it can wakeup the chip.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Wish it helps you!&lt;/P&gt;
&lt;P&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Kerry&lt;/P&gt;</description>
      <pubDate>Fri, 29 Dec 2023 10:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1176-wake-up/m-p/1781194#M218022</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2023-12-29T10:05:14Z</dc:date>
    </item>
  </channel>
</rss>