<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8ML Plus, PCIE RX and TX lanes functionality Switching in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8ML-Plus-PCIE-RX-and-TX-lanes-functionality-Switching/m-p/1780821#M217986</link>
    <description>&lt;P&gt;We are using the processor MIMX8ML8-based main board - to interface with a custom PCIE edge fingerboard.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It has the RX and TX lanes swapped in the M.2 connector. We would like to run the same board with a standard SSD.&lt;/P&gt;&lt;P&gt;Is there any possibility of switching the functionalities of the RX and TX lanes of the PCIE through any configuration?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please confirm if there is any option that we can consider.&lt;/P&gt;</description>
    <pubDate>Thu, 28 Dec 2023 08:13:55 GMT</pubDate>
    <dc:creator>EJSHY</dc:creator>
    <dc:date>2023-12-28T08:13:55Z</dc:date>
    <item>
      <title>IMX8ML Plus, PCIE RX and TX lanes functionality Switching</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8ML-Plus-PCIE-RX-and-TX-lanes-functionality-Switching/m-p/1780821#M217986</link>
      <description>&lt;P&gt;We are using the processor MIMX8ML8-based main board - to interface with a custom PCIE edge fingerboard.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It has the RX and TX lanes swapped in the M.2 connector. We would like to run the same board with a standard SSD.&lt;/P&gt;&lt;P&gt;Is there any possibility of switching the functionalities of the RX and TX lanes of the PCIE through any configuration?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please confirm if there is any option that we can consider.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Dec 2023 08:13:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8ML-Plus-PCIE-RX-and-TX-lanes-functionality-Switching/m-p/1780821#M217986</guid>
      <dc:creator>EJSHY</dc:creator>
      <dc:date>2023-12-28T08:13:55Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8ML Plus, PCIE RX and TX lanes functionality Switching</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8ML-Plus-PCIE-RX-and-TX-lanes-functionality-Switching/m-p/1781454#M218068</link>
      <description>&lt;P&gt;unfortunately, there is no configuration for swapping RX and TX.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jan 2024 05:40:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8ML-Plus-PCIE-RX-and-TX-lanes-functionality-Switching/m-p/1781454#M218068</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2024-01-02T05:40:52Z</dc:date>
    </item>
  </channel>
</rss>