<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: [jailhouse] boot from linux sd card, root cell from mmc</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/jailhouse-boot-from-linux-sd-card-root-cell-from-mmc/m-p/1780817#M217984</link>
    <description>&lt;P&gt;You need modify imx8mp-evk-root.dts to disable SD and enable eMMC. Then the root cell should be able to use eMMC when you booting from eMMC.&lt;/P&gt;
&lt;P&gt;Then you need update jailhouse cell configs/arm64/imx8mp-inmate-linux.c to assign emmc sdhc controller to it, not sd sdhc controller to it, the memory map and irq map.&lt;/P&gt;
&lt;P&gt;Then you need modify imx8mp-evk-inmate.dts to add sd sdhc in it. since there is no gpio, no regulator as of now, you need force it non-removable and configure regulator ready in root cell, but I guess should not impact.&lt;/P&gt;
&lt;P&gt;Needs some jailhouse knowledge to make it work, hope this hepls&lt;/P&gt;</description>
    <pubDate>Thu, 28 Dec 2023 08:01:07 GMT</pubDate>
    <dc:creator>Peng_Fan</dc:creator>
    <dc:date>2023-12-28T08:01:07Z</dc:date>
    <item>
      <title>[jailhouse] boot from linux sd card, root cell from mmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/jailhouse-boot-from-linux-sd-card-root-cell-from-mmc/m-p/1779136#M217760</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;is it possible to boot the root cell linux from mmc and run the inmae from sdcard? Using jailhouse?&lt;/P&gt;&lt;P&gt;if yes, what are the steps needed?&lt;/P&gt;&lt;P&gt;imx8mp processor.&lt;/P&gt;&lt;P&gt;br, Mircea&lt;/P&gt;</description>
      <pubDate>Fri, 22 Dec 2023 08:37:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/jailhouse-boot-from-linux-sd-card-root-cell-from-mmc/m-p/1779136#M217760</guid>
      <dc:creator>Ahelion</dc:creator>
      <dc:date>2023-12-22T08:37:01Z</dc:date>
    </item>
    <item>
      <title>Re: [jailhouse] boot from linux sd card, root cell from mmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/jailhouse-boot-from-linux-sd-card-root-cell-from-mmc/m-p/1780817#M217984</link>
      <description>&lt;P&gt;You need modify imx8mp-evk-root.dts to disable SD and enable eMMC. Then the root cell should be able to use eMMC when you booting from eMMC.&lt;/P&gt;
&lt;P&gt;Then you need update jailhouse cell configs/arm64/imx8mp-inmate-linux.c to assign emmc sdhc controller to it, not sd sdhc controller to it, the memory map and irq map.&lt;/P&gt;
&lt;P&gt;Then you need modify imx8mp-evk-inmate.dts to add sd sdhc in it. since there is no gpio, no regulator as of now, you need force it non-removable and configure regulator ready in root cell, but I guess should not impact.&lt;/P&gt;
&lt;P&gt;Needs some jailhouse knowledge to make it work, hope this hepls&lt;/P&gt;</description>
      <pubDate>Thu, 28 Dec 2023 08:01:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/jailhouse-boot-from-linux-sd-card-root-cell-from-mmc/m-p/1780817#M217984</guid>
      <dc:creator>Peng_Fan</dc:creator>
      <dc:date>2023-12-28T08:01:07Z</dc:date>
    </item>
    <item>
      <title>Re: [jailhouse] boot from linux sd card, root cell from mmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/jailhouse-boot-from-linux-sd-card-root-cell-from-mmc/m-p/1784117#M218342</link>
      <description>Is there any imx8* that has some form of android+linux thing in jailhouse? so that I can use as reference? I realy do not know how to do the steps you said above, I am a Noob at jailhouse.</description>
      <pubDate>Mon, 08 Jan 2024 06:39:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/jailhouse-boot-from-linux-sd-card-root-cell-from-mmc/m-p/1784117#M218342</guid>
      <dc:creator>Ahelion</dc:creator>
      <dc:date>2024-01-08T06:39:19Z</dc:date>
    </item>
  </channel>
</rss>