<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic [imx8mp] write real time linux in mmc in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-write-real-time-linux-in-mmc/m-p/1780756#M217974</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I saw that the real time linux nxp is offering for imx8mp board is a bit more feature packed than the standart linux.&lt;/P&gt;&lt;P&gt;Cand somebody tell me how do I flash it in the mcc of the board?&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the sd card I want to write android, have the real time linux jailhouse boot it.&lt;/P&gt;&lt;P&gt;Br&lt;/P&gt;&lt;P&gt;Ahelion&lt;/P&gt;</description>
    <pubDate>Thu, 28 Dec 2023 05:57:34 GMT</pubDate>
    <dc:creator>Ahelion</dc:creator>
    <dc:date>2023-12-28T05:57:34Z</dc:date>
    <item>
      <title>[imx8mp] write real time linux in mmc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-write-real-time-linux-in-mmc/m-p/1780756#M217974</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I saw that the real time linux nxp is offering for imx8mp board is a bit more feature packed than the standart linux.&lt;/P&gt;&lt;P&gt;Cand somebody tell me how do I flash it in the mcc of the board?&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the sd card I want to write android, have the real time linux jailhouse boot it.&lt;/P&gt;&lt;P&gt;Br&lt;/P&gt;&lt;P&gt;Ahelion&lt;/P&gt;</description>
      <pubDate>Thu, 28 Dec 2023 05:57:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-write-real-time-linux-in-mmc/m-p/1780756#M217974</guid>
      <dc:creator>Ahelion</dc:creator>
      <dc:date>2023-12-28T05:57:34Z</dc:date>
    </item>
  </channel>
</rss>