<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRestart USB Mass Storage Class FATFS</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Restart-USB-Mass-Storage-Class-FATFS/m-p/1780628#M217954</link>
    <description>&lt;P&gt;I am using an i.MXRT1021 controller with the following SDK package:&lt;/P&gt;&lt;P&gt;SDK_2_10_0_EVK-MIMXRT1020&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My application is implementing a MSC USB drive.&amp;nbsp; There are no issues when the attached test computer (Windows 11 PC) in detecting and performing file operations to the MSC drive.&lt;/P&gt;&lt;P&gt;I have found an issue though that when my firmware removes a file or directory from the drive that the attached computer interface does not detect this change in the FATFS configuration.&lt;/P&gt;&lt;P&gt;Now when the i.MX embedded f/w is restarted, the MSC drive indicates that the file has been removed but I would rather use a more graceful method to have the test system detect that the FATFS has been modified.&lt;/P&gt;&lt;P&gt;How do I trigger the USB interface to detect the changes by the FATFS?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 27 Dec 2023 21:23:54 GMT</pubDate>
    <dc:creator>threeboystech</dc:creator>
    <dc:date>2023-12-27T21:23:54Z</dc:date>
    <item>
      <title>Restart USB Mass Storage Class FATFS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Restart-USB-Mass-Storage-Class-FATFS/m-p/1780628#M217954</link>
      <description>&lt;P&gt;I am using an i.MXRT1021 controller with the following SDK package:&lt;/P&gt;&lt;P&gt;SDK_2_10_0_EVK-MIMXRT1020&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My application is implementing a MSC USB drive.&amp;nbsp; There are no issues when the attached test computer (Windows 11 PC) in detecting and performing file operations to the MSC drive.&lt;/P&gt;&lt;P&gt;I have found an issue though that when my firmware removes a file or directory from the drive that the attached computer interface does not detect this change in the FATFS configuration.&lt;/P&gt;&lt;P&gt;Now when the i.MX embedded f/w is restarted, the MSC drive indicates that the file has been removed but I would rather use a more graceful method to have the test system detect that the FATFS has been modified.&lt;/P&gt;&lt;P&gt;How do I trigger the USB interface to detect the changes by the FATFS?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Dec 2023 21:23:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Restart-USB-Mass-Storage-Class-FATFS/m-p/1780628#M217954</guid>
      <dc:creator>threeboystech</dc:creator>
      <dc:date>2023-12-27T21:23:54Z</dc:date>
    </item>
    <item>
      <title>Re: Restart USB Mass Storage Class FATFS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Restart-USB-Mass-Storage-Class-FATFS/m-p/1781808#M218107</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212174"&gt;@threeboystech&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;I would highly recommend you to update to the latest version of the SDK, as I believe this implementation had failures in SDK versions previous to 2.13, as seen on the following community post:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-RT/USB-msc-host-fatfs-freertos-failures-tested-with-EVK/td-p/1594028" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT/USB-msc-host-fatfs-freertos-failures-tested-with-EVK/td-p/1594028&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also, you can refer to the following &lt;A href="https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/kinetis-sdk%40tkb/214/2/Creating%20an%20USB%20Host%20Project%20(MSD%20+%20fatfs)%20with%20KSDK%201.3%20and%20Processor%20Expert%20support%20in%20KDS.pdf" target="_self"&gt;application note&lt;/A&gt; which, although very old and for the Kinetis family rather than the i.MX RT family, might prove insightful for your application.&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jan 2024 19:21:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Restart-USB-Mass-Storage-Class-FATFS/m-p/1781808#M218107</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2024-01-02T19:21:13Z</dc:date>
    </item>
  </channel>
</rss>