<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to send data though rpmsg from M-core to A-core(linux)? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-send-data-though-rpmsg-from-M-core-to-A-core-linux/m-p/1780533#M217943</link>
    <description>&lt;P&gt;Hello everyone!&lt;BR /&gt;&lt;BR /&gt;How to send data from the M7 processor (imx8mp) to A53? On the Linux side, I just need to read the data. For some reason, I don't have /dev/ttyRPMSG0 on the Linux side, but there is rpmsg char: /dev/rpmsg_ctrl0 and /dev/rpmsg0. I suppose rpmsg0 would also suffice to read the data that the coprocessor sends via rpmsg?&lt;/P&gt;&lt;P&gt;Ideally, I need simple code examples from both sides (both M core and A core).&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 27 Dec 2023 11:50:44 GMT</pubDate>
    <dc:creator>teleportboy</dc:creator>
    <dc:date>2023-12-27T11:50:44Z</dc:date>
    <item>
      <title>How to send data though rpmsg from M-core to A-core(linux)?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-send-data-though-rpmsg-from-M-core-to-A-core-linux/m-p/1780533#M217943</link>
      <description>&lt;P&gt;Hello everyone!&lt;BR /&gt;&lt;BR /&gt;How to send data from the M7 processor (imx8mp) to A53? On the Linux side, I just need to read the data. For some reason, I don't have /dev/ttyRPMSG0 on the Linux side, but there is rpmsg char: /dev/rpmsg_ctrl0 and /dev/rpmsg0. I suppose rpmsg0 would also suffice to read the data that the coprocessor sends via rpmsg?&lt;/P&gt;&lt;P&gt;Ideally, I need simple code examples from both sides (both M core and A core).&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 27 Dec 2023 11:50:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-send-data-though-rpmsg-from-M-core-to-A-core-linux/m-p/1780533#M217943</guid>
      <dc:creator>teleportboy</dc:creator>
      <dc:date>2023-12-27T11:50:44Z</dc:date>
    </item>
    <item>
      <title>Re: How to send data though rpmsg from M-core to A-core(linux)?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-send-data-though-rpmsg-from-M-core-to-A-core-linux/m-p/1780964#M217999</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224753"&gt;@teleportboy&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I hope you're doing well!&lt;/P&gt;
&lt;P&gt;You can find multicore examples with rpmsglite in the SDK demo apps for the i.MX 8M Plus. You'll need to build and download the SDK from&amp;nbsp;&lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_blank"&gt;Welcome | MCUXpresso SDK Builder (nxp.com).&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The multicore demos should be in boards/&amp;lt;your board&amp;gt;/multicore_examples/&lt;/P&gt;
&lt;P&gt;There you should see a ping pong and echo example with RTOS.&lt;/P&gt;
&lt;P&gt;Let me know if this was of any help.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Hector.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Dec 2023 18:23:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-send-data-though-rpmsg-from-M-core-to-A-core-linux/m-p/1780964#M217999</guid>
      <dc:creator>hector_delgado</dc:creator>
      <dc:date>2023-12-28T18:23:06Z</dc:date>
    </item>
  </channel>
</rss>