<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックuboot porting</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/uboot-porting/m-p/1780013#M217866</link>
    <description>&lt;P&gt;Hello, I use mx6sabresd board.&lt;BR /&gt;And I performed DDR calibration instead of dcd table. After compiling, I got uboot.imx and uboot.bin, and then burned the SD card. Execute sudo dd if=u-boot.imx of=/dev/sdb bs=1k seek=1 conv=fsync. The information obtained is that the burning speed is as high as 5MB/s, which should be measured in KB normally. I had doubts about this, and then I booted the board from the SD card, but no information was printed. Is this because the programming was not successful at all? If yes, do you think there is something wrong with my dd command?&lt;BR /&gt;Please reply, thank you!&lt;/P&gt;</description>
    <pubDate>Tue, 26 Dec 2023 09:50:22 GMT</pubDate>
    <dc:creator>rainho</dc:creator>
    <dc:date>2023-12-26T09:50:22Z</dc:date>
    <item>
      <title>uboot porting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/uboot-porting/m-p/1780013#M217866</link>
      <description>&lt;P&gt;Hello, I use mx6sabresd board.&lt;BR /&gt;And I performed DDR calibration instead of dcd table. After compiling, I got uboot.imx and uboot.bin, and then burned the SD card. Execute sudo dd if=u-boot.imx of=/dev/sdb bs=1k seek=1 conv=fsync. The information obtained is that the burning speed is as high as 5MB/s, which should be measured in KB normally. I had doubts about this, and then I booted the board from the SD card, but no information was printed. Is this because the programming was not successful at all? If yes, do you think there is something wrong with my dd command?&lt;BR /&gt;Please reply, thank you!&lt;/P&gt;</description>
      <pubDate>Tue, 26 Dec 2023 09:50:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/uboot-porting/m-p/1780013#M217866</guid>
      <dc:creator>rainho</dc:creator>
      <dc:date>2023-12-26T09:50:22Z</dc:date>
    </item>
  </channel>
</rss>