<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックXen fails to Create another Linux guest OS  with Android Guest OS running as DomU on IMX8QM MEK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Xen-fails-to-Create-another-Linux-guest-OS-with-Android-Guest-OS/m-p/1777952#M217671</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to bring up 2 guest OS Android and Linux with Xen on IMX8QM -MEK,&lt;/P&gt;&lt;P&gt;I initially created Android Guest OS using xl create /etc/xen/domu-imx8qm-mek-androidauto.cfg&lt;/P&gt;&lt;P&gt;Then when I tried creating Linux Guest OS&amp;nbsp; using xl create /etc/xen/domu-imx8qm-mek.cfg&lt;/P&gt;&lt;P&gt;I'm getting below error&lt;/P&gt;&lt;P&gt;&amp;nbsp;xc: error: panic: xc_dom_boot.c:122: xc_dom_boot_mem_init: can't allocate low memory for domain: Out of memory&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached the complete error log and&amp;nbsp; linux guest cfg file&lt;/P&gt;&lt;P&gt;Thanks in Advance,&lt;/P&gt;</description>
    <pubDate>Wed, 20 Dec 2023 12:02:07 GMT</pubDate>
    <dc:creator>LokeshGandham</dc:creator>
    <dc:date>2023-12-20T12:02:07Z</dc:date>
    <item>
      <title>Xen fails to Create another Linux guest OS  with Android Guest OS running as DomU on IMX8QM MEK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-fails-to-Create-another-Linux-guest-OS-with-Android-Guest-OS/m-p/1777952#M217671</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to bring up 2 guest OS Android and Linux with Xen on IMX8QM -MEK,&lt;/P&gt;&lt;P&gt;I initially created Android Guest OS using xl create /etc/xen/domu-imx8qm-mek-androidauto.cfg&lt;/P&gt;&lt;P&gt;Then when I tried creating Linux Guest OS&amp;nbsp; using xl create /etc/xen/domu-imx8qm-mek.cfg&lt;/P&gt;&lt;P&gt;I'm getting below error&lt;/P&gt;&lt;P&gt;&amp;nbsp;xc: error: panic: xc_dom_boot.c:122: xc_dom_boot_mem_init: can't allocate low memory for domain: Out of memory&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached the complete error log and&amp;nbsp; linux guest cfg file&lt;/P&gt;&lt;P&gt;Thanks in Advance,&lt;/P&gt;</description>
      <pubDate>Wed, 20 Dec 2023 12:02:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-fails-to-Create-another-Linux-guest-OS-with-Android-Guest-OS/m-p/1777952#M217671</guid>
      <dc:creator>LokeshGandham</dc:creator>
      <dc:date>2023-12-20T12:02:07Z</dc:date>
    </item>
    <item>
      <title>Re: Xen fails to Create another Linux guest OS  with Android Guest OS running as DomU on IMX8QM MEK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-fails-to-Create-another-Linux-guest-OS-with-Android-Guest-OS/m-p/1778035#M217675</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You have not enough memory on Xen Slave node try:&lt;/P&gt;
&lt;P&gt;xl info | grep memory&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 20 Dec 2023 14:42:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-fails-to-Create-another-Linux-guest-OS-with-Android-Guest-OS/m-p/1778035#M217675</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-12-20T14:42:47Z</dc:date>
    </item>
    <item>
      <title>Re: Xen fails to Create another Linux guest OS  with Android Guest OS running as DomU on IMX8QM MEK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Xen-fails-to-Create-another-Linux-guest-OS-with-Android-Guest-OS/m-p/1780396#M217925</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34846"&gt;@Bio_TICFSL&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for the reply,&lt;/P&gt;&lt;P&gt;As you mentioned there isn't enough free memory to create the second domain(Linux).&lt;/P&gt;&lt;P&gt;So I modified the memory allocation value for both Android and Linux in their respective .cfg files.&lt;/P&gt;&lt;P&gt;I was able to create both the Domains , but I'm unable to attach Android console, it gets stuck with&amp;nbsp;&lt;/P&gt;&lt;P&gt;"Starting Kernel..."&lt;/P&gt;&lt;P&gt;and linux console "end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b"&lt;/P&gt;&lt;P&gt;Attached the complete logs and cfg files.&lt;/P&gt;&lt;P&gt;Thanks in Advance&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Dec 2023 07:31:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Xen-fails-to-Create-another-Linux-guest-OS-with-Android-Guest-OS/m-p/1780396#M217925</guid>
      <dc:creator>LokeshGandham</dc:creator>
      <dc:date>2023-12-27T07:31:09Z</dc:date>
    </item>
  </channel>
</rss>