<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SDcard booting issues on IMX8MPlus in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SDcard-booting-issues-on-IMX8MPlus/m-p/1776878#M217596</link>
    <description>&lt;P&gt;Please try&amp;nbsp;bmaptool to flash wic image.&lt;/P&gt;
&lt;PRE class="language-markup"&gt;&lt;CODE&gt;IMAGE=fsl-image-multimedia-full-imx8mqevk-20181018224131.rootfs.wic
DEVICE=/dev/sdb # The device may change in your system
sudo bmaptool copy $IMAGE $DEVICE --nobmap&lt;/CODE&gt;&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 19 Dec 2023 06:37:06 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2023-12-19T06:37:06Z</dc:date>
    <item>
      <title>SDcard booting issues on IMX8MPlus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDcard-booting-issues-on-IMX8MPlus/m-p/1776819#M217586</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have an IMX8MPlus custom board unable to boot after u-boot.&amp;nbsp;Below is the SD image generated in our build with a size of 260 MB.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;imx8mplus-image-auaq0010-mna00012-7in-usd.wic.zst&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;After this, I flashed this image to a 32GB Sandisk SD card using the below command&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;zstdcat imx8mplus-image-auaq0010-mna00012-7in-usd.wic.zst | sudo dd of=/dev/sdX bs=1M conv=fsync&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Note:&lt;BR /&gt;&lt;/STRONG&gt;1. Format the SD card to "FAT32" before flashing the actual SD image.&lt;BR /&gt;2. Replaced the sdX as "sde" with the one which was detected by our host machine for uSD.&lt;/P&gt;&lt;P&gt;Then we inserted this flashed SD card to our board and tried to boot using SD mode.&lt;/P&gt;&lt;P&gt;However, we are unable to boot from the SD card and observed below-mentioned errors from the console. Please refer to the attached boot log for more details.&lt;/P&gt;&lt;P&gt;Failed to load 'boot.scr'&lt;BR /&gt;Error reading cluster&lt;BR /&gt;** Unable to read file Image **&lt;BR /&gt;Failed to load 'Image'&lt;BR /&gt;END BOOTING&lt;BR /&gt;u-boot=&amp;gt;&lt;/P&gt;&lt;P&gt;u-boot=&amp;gt; mmc part&lt;BR /&gt;Partition Map for MMC device 1 -- Partition Type: DOS&lt;BR /&gt;Part Start Sector Num Sectors UUID Type&lt;BR /&gt;** Can't read partition table on 1:0 **&lt;BR /&gt;u-boot=&amp;gt;&lt;/P&gt;&lt;P&gt;Please provide any other methods/suggestions such as any particular Filesystem Type needs to be considered while flashing the SD card, so that it is easy for me to fix this issue.&lt;/P&gt;</description>
      <pubDate>Tue, 19 Dec 2023 05:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDcard-booting-issues-on-IMX8MPlus/m-p/1776819#M217586</guid>
      <dc:creator>Saravanans1</dc:creator>
      <dc:date>2023-12-19T05:47:29Z</dc:date>
    </item>
    <item>
      <title>Re: SDcard booting issues on IMX8MPlus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDcard-booting-issues-on-IMX8MPlus/m-p/1776878#M217596</link>
      <description>&lt;P&gt;Please try&amp;nbsp;bmaptool to flash wic image.&lt;/P&gt;
&lt;PRE class="language-markup"&gt;&lt;CODE&gt;IMAGE=fsl-image-multimedia-full-imx8mqevk-20181018224131.rootfs.wic
DEVICE=/dev/sdb # The device may change in your system
sudo bmaptool copy $IMAGE $DEVICE --nobmap&lt;/CODE&gt;&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Dec 2023 06:37:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDcard-booting-issues-on-IMX8MPlus/m-p/1776878#M217596</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2023-12-19T06:37:06Z</dc:date>
    </item>
  </channel>
</rss>