<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX 93 LCDIF MIPI-DPI Pin mapping in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1776109#M217517</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This same configuration can be possible in iMX RT-1060 Controllers?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 18 Dec 2023 07:05:21 GMT</pubDate>
    <dc:creator>abilashjoseph</dc:creator>
    <dc:date>2023-12-18T07:05:21Z</dc:date>
    <item>
      <title>iMX 93 LCDIF MIPI-DPI Pin mapping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1772774#M217194</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I was looking on the LCDIF&amp;nbsp;MIPI-DPI for iMX-93 processor. I want to interface a parallel TFT LCD in RGB555 configuration. Anywhere in the datasheet I didn't find the pin multiplexing for RGB DATA (R0-R4, G0-G4, B0-B4) for RGB555 configuration.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Dec 2023 03:12:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1772774#M217194</guid>
      <dc:creator>abilashjoseph</dc:creator>
      <dc:date>2023-12-20T03:12:50Z</dc:date>
    </item>
    <item>
      <title>Re: iMX 93 LCDIF MIPI-DPI Pin mapping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1773557#M217257</link>
      <description>&lt;P&gt;for rgb555,&amp;nbsp; refer to the&lt;/P&gt;
&lt;P&gt;&lt;A href="https://learn.microsoft.com/en-us/windows/win32/directshow/working-with-16-bit-rgb" target="_blank"&gt;https://learn.microsoft.com/en-us/windows/win32/directshow/working-with-16-bit-rgb&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;should be &lt;SPAN&gt;&lt;SPAN class="ui-provider ed bnl bnm bnn bno bnp bnq bnr bns bnt bnu bnv bnw bnx bny bnz boa bob boc bod boe bof bog boh boi boj bok bol bom bon boo bop boq bor bos"&gt;xRRRRRGGGGGBBBBB&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;you can refer to the table as below, then connect as &lt;SPAN&gt;&lt;SPAN class="ui-provider ed bnl bnm bnn bno bnp bnq bnr bns bnt bnu bnv bnw bnx bny bnz boa bob boc bod boe bof bog boh boi boj bok bol bom bon boo bop boq bor bos"&gt;xRRRRRGGGGGBBBBB&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="joanxie_0-1702440006587.png" style="width: 533px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/254098iDC09D1FCE4B61FA8/image-dimensions/533x297?v=v2" width="533" height="297" role="button" title="joanxie_0-1702440006587.png" alt="joanxie_0-1702440006587.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;then choose the register as below&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="joanxie_1-1702440020811.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/254099iE5D4278791B8CA1D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="joanxie_1-1702440020811.png" alt="joanxie_1-1702440020811.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Dec 2023 04:03:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1773557#M217257</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-12-13T04:03:03Z</dc:date>
    </item>
    <item>
      <title>Re: iMX 93 LCDIF MIPI-DPI Pin mapping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1773562#M217259</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;Thanks for the valuable information. One more doubt, which register is used to select the different 16-bit configuration (config 1, config2, config3)&lt;/P&gt;</description>
      <pubDate>Wed, 13 Dec 2023 04:19:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1773562#M217259</guid>
      <dc:creator>abilashjoseph</dc:creator>
      <dc:date>2023-12-13T04:19:12Z</dc:date>
    </item>
    <item>
      <title>Re: iMX 93 LCDIF MIPI-DPI Pin mapping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1773802#M217292</link>
      <description>&lt;P&gt;Define the pixel color coding to be used by using the dpi_color_coding field in the&lt;BR /&gt;DPI_COLOR_CODING register&lt;/P&gt;
&lt;P&gt;so for more detailed information, pls refer to the chapter 52.4.2.6 DPI color coding (DPI_COLOR_CODING)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Dec 2023 09:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1773802#M217292</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-12-13T09:37:13Z</dc:date>
    </item>
    <item>
      <title>Re: iMX 93 LCDIF MIPI-DPI Pin mapping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1773811#M217293</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Ok. Great. Thanks for the support.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Dec 2023 09:41:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1773811#M217293</guid>
      <dc:creator>abilashjoseph</dc:creator>
      <dc:date>2023-12-13T09:41:15Z</dc:date>
    </item>
    <item>
      <title>Re: iMX 93 LCDIF MIPI-DPI Pin mapping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1776109#M217517</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This same configuration can be possible in iMX RT-1060 Controllers?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Dec 2023 07:05:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1776109#M217517</guid>
      <dc:creator>abilashjoseph</dc:creator>
      <dc:date>2023-12-18T07:05:21Z</dc:date>
    </item>
    <item>
      <title>Re: iMX 93 LCDIF MIPI-DPI Pin mapping</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1776362#M217533</link>
      <description>&lt;P&gt;not sure of RT1060, pls create a new case for IMX RT team to double confirm&lt;/P&gt;</description>
      <pubDate>Mon, 18 Dec 2023 11:03:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX-93-LCDIF-MIPI-DPI-Pin-mapping/m-p/1776362#M217533</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-12-18T11:03:25Z</dc:date>
    </item>
  </channel>
</rss>