<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6ULL custom board not boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULL-custom-board-not-boot/m-p/1775457#M217445</link>
    <description>&lt;P&gt;I have a similar problem. Is there any update on this issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ENET1_Error.PNG" style="width: 988px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/254631i358F988525BF8C30/image-size/large?v=v2&amp;amp;px=999" role="button" title="ENET1_Error.PNG" alt="ENET1_Error.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ENET1_Error.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 15 Dec 2023 08:53:15 GMT</pubDate>
    <dc:creator>zmagday</dc:creator>
    <dc:date>2023-12-15T08:53:15Z</dc:date>
    <item>
      <title>IMX6ULL custom board not boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULL-custom-board-not-boot/m-p/1768669#M216848</link>
      <description>&lt;P&gt;My imx6ull board is currently experiencing this situation. Before that it was possible to load u-boot from sd card. Can someone help me?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2023.04-dirty (Dec 04 2023 - 04:17:41 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX6ULL rev1.1 900 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 40C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: i.MX6 ULL 14x14 EVK Board&lt;BR /&gt;Board: MX6ULL 14x14 EVK&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;Core: 77 devices, 22 uclasses, devicetree: separate&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0 (480 x 272)&lt;BR /&gt;[0] lcdif@21c8000, video&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1(part 0) is current device&lt;BR /&gt;Net: Could not get PHY for FEC1: addr 1&lt;BR /&gt;Could not get PHY for FEC1: addr 1&lt;BR /&gt;Get shared mii bus on ethernet@2188000&lt;BR /&gt;:-1645653376 is connected to . Reconnecting to ethernet@2188000&lt;BR /&gt;prefetch abort&lt;BR /&gt;pc : [&amp;lt;005fef6e&amp;gt;] lr : [&amp;lt;00002f58&amp;gt;]&lt;BR /&gt;reloc pc : [&amp;lt;e8f87f6e&amp;gt;] lr : [&amp;lt;e898bf58&amp;gt;]&lt;BR /&gt;sp : 9de6c230 ip : 00000020 fp : 00000017&lt;BR /&gt;r10: 00000001 r9 : 9de74eb0 r8 : 9de766b8&lt;BR /&gt;r7 : 9de76658 r6 : 9de79708 r5 : 00000002 r4 : 9eeefb3c&lt;BR /&gt;r3 : 00002f50 r2 : 0000001f r1 : ffffffff r0 : 9eeefb3c&lt;BR /&gt;Flags: nzCv IRQs off FIQs off Mode SVC_32 (T)&lt;BR /&gt;Code: data abort&lt;BR /&gt;pc : [&amp;lt;9ee78a46&amp;gt;] lr : [&amp;lt;9ee78a2d&amp;gt;]&lt;BR /&gt;reloc pc : [&amp;lt;87801a46&amp;gt;] lr : [&amp;lt;87801a2d&amp;gt;]&lt;BR /&gt;sp : 9de6c138 ip : 00000020 fp : 00000017&lt;BR /&gt;r10: 9eed89c0 r9 : 9de74eb0 r8 : 9eed89b8&lt;BR /&gt;r7 : 00000004 r6 : 00000020 r5 : 005fef6e r4 : fffffffc&lt;BR /&gt;r3 : 00000001 r2 : 9de75298 r1 : 00000000 r0 : 00000006&lt;BR /&gt;Flags: NzCv IRQs on FIQs on Mode SVC_32 (T)&lt;BR /&gt;Code: e8bd 45f0 f04b bc33 (f835) 2014&lt;BR /&gt;Resetting CPU ...&lt;/P&gt;</description>
      <pubDate>Tue, 05 Dec 2023 02:58:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6ULL-custom-board-not-boot/m-p/1768669#M216848</guid>
      <dc:creator>duyhai</dc:creator>
      <dc:date>2023-12-05T02:58:37Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6ULL custom board not boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULL-custom-board-not-boot/m-p/1775457#M217445</link>
      <description>&lt;P&gt;I have a similar problem. Is there any update on this issue?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ENET1_Error.PNG" style="width: 988px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/254631i358F988525BF8C30/image-size/large?v=v2&amp;amp;px=999" role="button" title="ENET1_Error.PNG" alt="ENET1_Error.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ENET1_Error.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Dec 2023 08:53:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6ULL-custom-board-not-boot/m-p/1775457#M217445</guid>
      <dc:creator>zmagday</dc:creator>
      <dc:date>2023-12-15T08:53:15Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6ULL custom board not boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6ULL-custom-board-not-boot/m-p/1922595#M226858</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;We have exactly the same issue. No responses from NXP yet?&lt;/P&gt;&lt;P&gt;We are looking into our schematics, and comparing with the EVK.&lt;/P&gt;&lt;P&gt;Our main disadvantage here is that we are using a different PHY chip (KSZ8081RNA instead of KSZ8081RNB)&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2023.04-lf_v2023.04+gaf7d004eaf (Jun 06 2023 - 14:59:40 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX6ULL rev1.1 900 MHz (running at 396 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 50C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: i.MX6 ULL 14x14 EVK Board&lt;BR /&gt;Board: MX6ULL 14x14 EVK&lt;BR /&gt;DRAM: 512 MiB&lt;BR /&gt;Core: 77 devices, 22 uclasses, devicetree: separate&lt;BR /&gt;MMC: FSL_SDHC: 0, FSL_SDHC: 1&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0 (480 x 272)&lt;BR /&gt;[0] lcdif@21c8000, video&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc1(part 0) is current device&lt;BR /&gt;Net: Could not get PHY for FEC1: addr 1&lt;BR /&gt;Could not get PHY for FEC1: addr 1&lt;BR /&gt;Get shared mii bus on ethernet@2188000&lt;BR /&gt;:-1645649280 is connected to . Reconnecting to ethernet@2188000&lt;BR /&gt;prefetch abort&lt;BR /&gt;pc : [&amp;lt;005fef6e&amp;gt;] lr : [&amp;lt;00002f58&amp;gt;]&lt;BR /&gt;reloc pc : [&amp;lt;e8f86f6e&amp;gt;] lr : [&amp;lt;e898af58&amp;gt;]&lt;BR /&gt;sp : 9de6d170 ip : 00000020 fp : 87800020&lt;BR /&gt;r10: 00000001 r9 : 9de75eb0 r8 : 9de776b8&lt;BR /&gt;r7 : 9de77658 r6 : 9de7a708 r5 : 00000002 r4 : 9eef0348&lt;BR /&gt;r3 : 00002f50 r2 : 0000001f r1 : ffffffff r0 : 9eef0348&lt;BR /&gt;Flags: nzCv IRQs off FIQs off Mode SVC_32 (T)&lt;BR /&gt;Code: data abort&lt;BR /&gt;pc : [&amp;lt;9ee79a46&amp;gt;] lr : [&amp;lt;9ee79a2d&amp;gt;]&lt;BR /&gt;reloc pc : [&amp;lt;87801a46&amp;gt;] lr : [&amp;lt;87801a2d&amp;gt;]&lt;BR /&gt;sp : 9de6d078 ip : 00000020 fp : 87800020&lt;BR /&gt;r10: 9eed8f37 r9 : 9de75eb0 r8 : 9eed8f2f&lt;BR /&gt;r7 : 00000004 r6 : 00000020 r5 : 005fef6e r4 : fffffffc&lt;BR /&gt;r3 : 00000001 r2 : 9de76298 r1 : 00000000 r0 : 00000006&lt;BR /&gt;Flags: NzCv IRQs on FIQs on Mode SVC_32 (T)&lt;BR /&gt;Code: e8bd 45f0 f04a bfa7 (f835) 2014&lt;BR /&gt;Resetting CPU ...&lt;/P&gt;&lt;P&gt;resetting ...&lt;/P&gt;</description>
      <pubDate>Thu, 01 Aug 2024 06:35:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6ULL-custom-board-not-boot/m-p/1922595#M226858</guid>
      <dc:creator>V_Palacio</dc:creator>
      <dc:date>2024-08-01T06:35:09Z</dc:date>
    </item>
  </channel>
</rss>