<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックDoes flex spi support simultaneous read/write?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Does-flex-spi-support-simultaneous-read-write/m-p/1774082#M217310</link>
    <description>&lt;P&gt;Hi I am wondering - does the Flex SPI controller support simultaneous read / write?&lt;/P&gt;&lt;P&gt;Let me explain what I mean.&lt;/P&gt;&lt;P&gt;I have the device - FPGA - which once it's clocked immediately sends some data on MISO line.&lt;/P&gt;&lt;P&gt;Eg when I want to issue read operation on FPGA I send the following byte stream:(cmd, addr, length)&lt;/P&gt;&lt;P&gt;MOSI: 0x80 | 0x12 0x34 0x56 | 0x4&lt;/P&gt;&lt;P&gt;MISO: 0x11 | 0xXX 0xXX 0xXX | data[0]... data[3]&lt;/P&gt;&lt;P&gt;As you can see the 0x11 byte is pushed by the FPGA on the same clock cycle as the first byte on MOSI. This is something like a status that allows to verify the device type. The rest 3 bytes are undefined, data[0]...data[3] is actual data that was requested.&lt;/P&gt;&lt;P&gt;Any ideas how can I achieve this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 13 Dec 2023 16:20:05 GMT</pubDate>
    <dc:creator>rdr3e</dc:creator>
    <dc:date>2023-12-13T16:20:05Z</dc:date>
    <item>
      <title>Does flex spi support simultaneous read/write?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-flex-spi-support-simultaneous-read-write/m-p/1774082#M217310</link>
      <description>&lt;P&gt;Hi I am wondering - does the Flex SPI controller support simultaneous read / write?&lt;/P&gt;&lt;P&gt;Let me explain what I mean.&lt;/P&gt;&lt;P&gt;I have the device - FPGA - which once it's clocked immediately sends some data on MISO line.&lt;/P&gt;&lt;P&gt;Eg when I want to issue read operation on FPGA I send the following byte stream:(cmd, addr, length)&lt;/P&gt;&lt;P&gt;MOSI: 0x80 | 0x12 0x34 0x56 | 0x4&lt;/P&gt;&lt;P&gt;MISO: 0x11 | 0xXX 0xXX 0xXX | data[0]... data[3]&lt;/P&gt;&lt;P&gt;As you can see the 0x11 byte is pushed by the FPGA on the same clock cycle as the first byte on MOSI. This is something like a status that allows to verify the device type. The rest 3 bytes are undefined, data[0]...data[3] is actual data that was requested.&lt;/P&gt;&lt;P&gt;Any ideas how can I achieve this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Dec 2023 16:20:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-flex-spi-support-simultaneous-read-write/m-p/1774082#M217310</guid>
      <dc:creator>rdr3e</dc:creator>
      <dc:date>2023-12-13T16:20:05Z</dc:date>
    </item>
    <item>
      <title>Re: Does flex spi support simultaneous read/write?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-flex-spi-support-simultaneous-read-write/m-p/1774855#M217384</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;No, is matter of 1uSec but no simultaneously,try to implement this.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Dec 2023 14:13:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-flex-spi-support-simultaneous-read-write/m-p/1774855#M217384</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-12-14T14:13:27Z</dc:date>
    </item>
    <item>
      <title>Re: Does flex spi support simultaneous read/write?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Does-flex-spi-support-simultaneous-read-write/m-p/1774921#M217395</link>
      <description>&lt;P&gt;Can you elaborate on this: "No, is matter of 1uSec"?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Dec 2023 16:04:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Does-flex-spi-support-simultaneous-read-write/m-p/1774921#M217395</guid>
      <dc:creator>rdr3e</dc:creator>
      <dc:date>2023-12-14T16:04:34Z</dc:date>
    </item>
  </channel>
</rss>