<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Changing SCU UART Pins</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Changing-SCU-UART-Pins/m-p/1773775#M217289</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using a custom board with iMX8QXP. For debug purposes, I had to change the SCU UART pins to the M4 UART pins. I did the following change in the board.c file according to the document:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Use-UART0-RX-TX-as-SCU-UART-debug-port-on-iMX8QXP-boards/ta-p/1119371" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Use-UART0-RX-TX-as-SCU-UART-debug-port-on-iMX8QXP-boards/ta-p/1119371&lt;/A&gt;&lt;/P&gt;&lt;P&gt;#define ALT_DEBUG_UART and #define&amp;nbsp;ALT_DEBUG_SCU_UART. I added these to the board.c file. It worked and I was able to get prints from the SCU on the M4 core console.&lt;/P&gt;&lt;P&gt;The initial SCU UART pins used are:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;SCU_GPIO0_00 &amp;amp; SCU_GPIO0_01&lt;/P&gt;&lt;P&gt;The M4 UART pins used are:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;ADC_IN2 &amp;amp; ADC_IN3&lt;/P&gt;&lt;P&gt;I would like to revert to the previous settings. I removed the above change and rebuilt the SCFW. But now I am getting SCU prints on both the M4 console and on the original SCU UART pins. I even tried re-flashing the board with a firmware, built from a fresh source code. But still no change. How can I fix this?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/4760"&gt;@qiang_li-mpu_se&lt;/a&gt;&amp;nbsp;Could you please look into this?&lt;/P&gt;</description>
    <pubDate>Thu, 14 Dec 2023 05:40:55 GMT</pubDate>
    <dc:creator>MJames</dc:creator>
    <dc:date>2023-12-14T05:40:55Z</dc:date>
    <item>
      <title>Changing SCU UART Pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Changing-SCU-UART-Pins/m-p/1773775#M217289</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using a custom board with iMX8QXP. For debug purposes, I had to change the SCU UART pins to the M4 UART pins. I did the following change in the board.c file according to the document:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Use-UART0-RX-TX-as-SCU-UART-debug-port-on-iMX8QXP-boards/ta-p/1119371" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Use-UART0-RX-TX-as-SCU-UART-debug-port-on-iMX8QXP-boards/ta-p/1119371&lt;/A&gt;&lt;/P&gt;&lt;P&gt;#define ALT_DEBUG_UART and #define&amp;nbsp;ALT_DEBUG_SCU_UART. I added these to the board.c file. It worked and I was able to get prints from the SCU on the M4 core console.&lt;/P&gt;&lt;P&gt;The initial SCU UART pins used are:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;SCU_GPIO0_00 &amp;amp; SCU_GPIO0_01&lt;/P&gt;&lt;P&gt;The M4 UART pins used are:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;ADC_IN2 &amp;amp; ADC_IN3&lt;/P&gt;&lt;P&gt;I would like to revert to the previous settings. I removed the above change and rebuilt the SCFW. But now I am getting SCU prints on both the M4 console and on the original SCU UART pins. I even tried re-flashing the board with a firmware, built from a fresh source code. But still no change. How can I fix this?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/4760"&gt;@qiang_li-mpu_se&lt;/a&gt;&amp;nbsp;Could you please look into this?&lt;/P&gt;</description>
      <pubDate>Thu, 14 Dec 2023 05:40:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Changing-SCU-UART-Pins/m-p/1773775#M217289</guid>
      <dc:creator>MJames</dc:creator>
      <dc:date>2023-12-14T05:40:55Z</dc:date>
    </item>
    <item>
      <title>Re: Changing SCU UART Pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Changing-SCU-UART-Pins/m-p/1774147#M217317</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Please make sure that all changes made are reverted. &lt;BR /&gt;Also, you may try using a fresh source code instead.&lt;BR /&gt;&lt;BR /&gt;Saludos,&lt;BR /&gt;Aldo&lt;/P&gt;</description>
      <pubDate>Wed, 13 Dec 2023 18:32:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Changing-SCU-UART-Pins/m-p/1774147#M217317</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2023-12-13T18:32:25Z</dc:date>
    </item>
    <item>
      <title>Re: Changing SCU UART Pins</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Changing-SCU-UART-Pins/m-p/1774383#M217341</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/171173"&gt;@AldoG&lt;/a&gt;,&lt;BR /&gt;I have tried after reverting all the changes, but the issue is not resolved. I have also tried changing the entire firmware, built from a fresh source code. Still there is no change.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Dec 2023 04:13:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Changing-SCU-UART-Pins/m-p/1774383#M217341</guid>
      <dc:creator>MJames</dc:creator>
      <dc:date>2023-12-18T04:13:44Z</dc:date>
    </item>
  </channel>
</rss>