<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 USB Host examples controller</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-Host-examples-controller/m-p/1770542#M217007</link>
    <description>&lt;P&gt;Using the EVKBMIMXRT1060 eval board.&lt;/P&gt;&lt;P&gt;The various USB Host examples I tried have the default to Controller ID 'kUSB_ControllerEhci0'&lt;/P&gt;&lt;P&gt;But as far as I can tell this is not a valid controller for a USB host and must always be changed to&amp;nbsp;kUSB_ControllerEhci1 (and&amp;nbsp; using the OTG2 socket)&lt;/P&gt;&lt;P&gt;Am I missing something, seems strange that the examples all need this setting in order to work?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 07 Dec 2023 08:18:30 GMT</pubDate>
    <dc:creator>Ximen</dc:creator>
    <dc:date>2023-12-07T08:18:30Z</dc:date>
    <item>
      <title>USB Host examples controller</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Host-examples-controller/m-p/1770542#M217007</link>
      <description>&lt;P&gt;Using the EVKBMIMXRT1060 eval board.&lt;/P&gt;&lt;P&gt;The various USB Host examples I tried have the default to Controller ID 'kUSB_ControllerEhci0'&lt;/P&gt;&lt;P&gt;But as far as I can tell this is not a valid controller for a USB host and must always be changed to&amp;nbsp;kUSB_ControllerEhci1 (and&amp;nbsp; using the OTG2 socket)&lt;/P&gt;&lt;P&gt;Am I missing something, seems strange that the examples all need this setting in order to work?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Dec 2023 08:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Host-examples-controller/m-p/1770542#M217007</guid>
      <dc:creator>Ximen</dc:creator>
      <dc:date>2023-12-07T08:18:30Z</dc:date>
    </item>
    <item>
      <title>Re: USB Host examples controller</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-Host-examples-controller/m-p/1772461#M217173</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226755"&gt;@Ximen&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Could you please tell us which SDK and version are you using?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Also, could you explain us why is EHCI0 is not a valid controller for a USB host?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Warm regards, Raul.&lt;/P&gt;</description>
      <pubDate>Mon, 11 Dec 2023 17:53:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-Host-examples-controller/m-p/1772461#M217173</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-12-11T17:53:23Z</dc:date>
    </item>
  </channel>
</rss>