<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: OpenWRT i.MX8 Customize</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/OpenWRT-i-MX8-Customize/m-p/1769477#M216919</link>
    <description>Hi Tad,&lt;BR /&gt;You can add a new .mk file to add the new subtarget.&lt;BR /&gt;Take the imx8 for example: target/linux/imx/image/imx8.mk.&lt;BR /&gt;But I don't think you need to add a new subtarget.&lt;BR /&gt;You really need to add a new device or called profile for your customized board.&lt;BR /&gt;If this is the case, you can add a new device item in &lt;BR /&gt;target/linux/imx/image/imx8.mk.&lt;BR /&gt;Take imx8mplus for example:&lt;BR /&gt; 17 define Device/imx8mplus&lt;BR /&gt; 18   DEVICE_VENDOR := NXP&lt;BR /&gt; 19   DEVICE_MODEL := IMX8MPLUS&lt;BR /&gt; 20   DEVICE_VARIANT := SD Card Boot&lt;BR /&gt; 21   PLAT := iMX8MP&lt;BR /&gt; 22   SOC_TYPE := iMX8M&lt;BR /&gt; 23   DEVICE_TYPE := flash_evk&lt;BR /&gt; 24   ENV_NAME:=imx8mp-sdboot&lt;BR /&gt; 25   DEVICE_PACKAGES += \&lt;BR /&gt; 26     atf-imx8mp \&lt;BR /&gt; 27     firmware-imx \&lt;BR /&gt; 28     imx-mkimage \&lt;BR /&gt; 29     u-boot-imx8mp&lt;BR /&gt; 30   DEVICE_DTS := freescale/imx8mp-evk&lt;BR /&gt; 31   IMAGE/sdcard.img := \&lt;BR /&gt; 32     imx-compile-dtb $$(DEVICE_DTS) | \&lt;BR /&gt; 33     imx-create-flash $$(PLAT) $$(DEVICE_TYPE) | \&lt;BR /&gt; 34     imx-clean | \&lt;BR /&gt; 35     imx-append-sdhead $(1) | pad-to 32K | \&lt;BR /&gt; 36     imx-append-boot $$(SOC_TYPE) | pad-to 4M | \&lt;BR /&gt; 37     imx-append $$(ENV_NAME)-uboot-env.bin | pad-to $(IMX_SD_KERNELPART_OFFSET)M | \&lt;BR /&gt; 38     imx-append-kernel $$(DEVICE_DTS) | pad-to $(IMX_SD_ROOTFSPART_OFFSET)M | \&lt;BR /&gt; 39     append-rootfs | pad-to $(IMX_SD_IMAGE_SIZE)M&lt;BR /&gt; 40 endef&lt;BR /&gt; 41 TARGET_DEVICES += imx8mplus&lt;BR /&gt;&lt;BR /&gt;</description>
    <pubDate>Wed, 06 Dec 2023 06:03:24 GMT</pubDate>
    <dc:creator>Andy_Tang</dc:creator>
    <dc:date>2023-12-06T06:03:24Z</dc:date>
    <item>
      <title>OpenWRT i.MX8 Customize</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenWRT-i-MX8-Customize/m-p/1758230#M215823</link>
      <description>&lt;P&gt;Hi everyone:&lt;/P&gt;&lt;P&gt;I found the OpenWRT for imx8 on github, And I have customize board with i.MX8M Plus, How can I do make the customize target profile? I see the target/imx folder but I don't get it how to safe make the new subtarget&lt;/P&gt;&lt;P&gt;imx openwrt source code:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/nxp-imx/imx_openwrt/" target="_blank"&gt;https://github.com/nxp-imx/imx_openwrt/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;reference:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com.cn/docs/zh/training-reference-material/TIP-5G-IOT-OPENWRT-2.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/zh/training-reference-material/TIP-5G-IOT-OPENWRT-2.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Nov 2023 08:51:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenWRT-i-MX8-Customize/m-p/1758230#M215823</guid>
      <dc:creator>Tad</dc:creator>
      <dc:date>2023-11-16T08:51:02Z</dc:date>
    </item>
    <item>
      <title>Re: OpenWRT i.MX8 Customize</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenWRT-i-MX8-Customize/m-p/1758457#M215833</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225829"&gt;@Tad&lt;/a&gt;!&lt;BR /&gt;Thank you for contacting NXP Support!&lt;BR /&gt;&lt;BR /&gt;NXP doesn't support openWRT, but you can consult the information by following the links:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;UL dir="auto"&gt;
&lt;LI&gt;&lt;A href="https://openwrt.org/docs/guide-quick-start/start" rel="nofollow" target="_blank"&gt;Quick Start Guide&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://openwrt.org/docs/guide-user/start" rel="nofollow" target="_blank"&gt;User Guide&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://openwrt.org/docs/guide-developer/start" rel="nofollow" target="_blank"&gt;Developer Documentation&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://openwrt.org/docs/techref/start" rel="nofollow" target="_blank"&gt;Technical Reference&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Thu, 16 Nov 2023 14:26:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenWRT-i-MX8-Customize/m-p/1758457#M215833</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2023-11-16T14:26:10Z</dc:date>
    </item>
    <item>
      <title>Re: OpenWRT i.MX8 Customize</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/OpenWRT-i-MX8-Customize/m-p/1769477#M216919</link>
      <description>Hi Tad,&lt;BR /&gt;You can add a new .mk file to add the new subtarget.&lt;BR /&gt;Take the imx8 for example: target/linux/imx/image/imx8.mk.&lt;BR /&gt;But I don't think you need to add a new subtarget.&lt;BR /&gt;You really need to add a new device or called profile for your customized board.&lt;BR /&gt;If this is the case, you can add a new device item in &lt;BR /&gt;target/linux/imx/image/imx8.mk.&lt;BR /&gt;Take imx8mplus for example:&lt;BR /&gt; 17 define Device/imx8mplus&lt;BR /&gt; 18   DEVICE_VENDOR := NXP&lt;BR /&gt; 19   DEVICE_MODEL := IMX8MPLUS&lt;BR /&gt; 20   DEVICE_VARIANT := SD Card Boot&lt;BR /&gt; 21   PLAT := iMX8MP&lt;BR /&gt; 22   SOC_TYPE := iMX8M&lt;BR /&gt; 23   DEVICE_TYPE := flash_evk&lt;BR /&gt; 24   ENV_NAME:=imx8mp-sdboot&lt;BR /&gt; 25   DEVICE_PACKAGES += \&lt;BR /&gt; 26     atf-imx8mp \&lt;BR /&gt; 27     firmware-imx \&lt;BR /&gt; 28     imx-mkimage \&lt;BR /&gt; 29     u-boot-imx8mp&lt;BR /&gt; 30   DEVICE_DTS := freescale/imx8mp-evk&lt;BR /&gt; 31   IMAGE/sdcard.img := \&lt;BR /&gt; 32     imx-compile-dtb $$(DEVICE_DTS) | \&lt;BR /&gt; 33     imx-create-flash $$(PLAT) $$(DEVICE_TYPE) | \&lt;BR /&gt; 34     imx-clean | \&lt;BR /&gt; 35     imx-append-sdhead $(1) | pad-to 32K | \&lt;BR /&gt; 36     imx-append-boot $$(SOC_TYPE) | pad-to 4M | \&lt;BR /&gt; 37     imx-append $$(ENV_NAME)-uboot-env.bin | pad-to $(IMX_SD_KERNELPART_OFFSET)M | \&lt;BR /&gt; 38     imx-append-kernel $$(DEVICE_DTS) | pad-to $(IMX_SD_ROOTFSPART_OFFSET)M | \&lt;BR /&gt; 39     append-rootfs | pad-to $(IMX_SD_IMAGE_SIZE)M&lt;BR /&gt; 40 endef&lt;BR /&gt; 41 TARGET_DEVICES += imx8mplus&lt;BR /&gt;&lt;BR /&gt;</description>
      <pubDate>Wed, 06 Dec 2023 06:03:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/OpenWRT-i-MX8-Customize/m-p/1769477#M216919</guid>
      <dc:creator>Andy_Tang</dc:creator>
      <dc:date>2023-12-06T06:03:24Z</dc:date>
    </item>
  </channel>
</rss>