<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Device Tree file in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-file/m-p/1769110#M216895</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184278"&gt;@VinithNama&lt;/a&gt;&amp;nbsp; ,&lt;BR /&gt;&lt;BR /&gt;you can check either of any&lt;BR /&gt;1. DTBO is implemented which is overwriting your dts configuration&lt;BR /&gt;2. Check the md5sum of the actual generated dtb vs on board dtb&lt;BR /&gt;3. In U-boot check weather the dtbo is actually being taken into account while booting kernel using printenv command&lt;BR /&gt;4. Perhaps the same GPIO is being configured alternatively, the final config can be checked post booting /sys/kernel/debug/gpio ?&lt;BR /&gt;&lt;BR /&gt;--&lt;BR /&gt;Rutvij Trivedi&lt;BR /&gt;&lt;A href="https://siliconsignals.io/" target="_self"&gt;Silicon Signals Pvt. Ltd&lt;/A&gt;.&lt;BR /&gt;&lt;A href="mailto:info@siliconsignals.io" target="_blank"&gt;info@siliconsignals.io&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;--&lt;BR /&gt;Rutvij Trivedi&lt;/P&gt;</description>
    <pubDate>Tue, 05 Dec 2023 14:43:47 GMT</pubDate>
    <dc:creator>r_trivedi123</dc:creator>
    <dc:date>2023-12-05T14:43:47Z</dc:date>
    <item>
      <title>Device Tree file</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-file/m-p/1291812#M175476</link>
      <description>&lt;P&gt;Hi Sir/Madam,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I'm working on imx8m mini EVK on Linux environment, I'm modifying the imx8mm-evk .dts file in the kernel-source/aarch/arm64/boot/dts/freescale location after modifying the file I'm building the dts file using&amp;nbsp;&lt;STRONG&gt;bitbake –c menuconfig linux-imx &lt;/STRONG&gt;after building the dts file, I'm generating the images using bitbake imx-image-full and copying the images to the sdcard when i'm booting the evk with this sdcard I'm unable to see the pin what i have modified in dts file.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 08:54:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-file/m-p/1291812#M175476</guid>
      <dc:creator>VinithNama</dc:creator>
      <dc:date>2021-06-14T08:54:02Z</dc:date>
    </item>
    <item>
      <title>Re: Device Tree file</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-file/m-p/1291857#M175480</link>
      <description>&lt;P&gt;Hi Vinith&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;for dts customization one can look at tutorial&lt;/P&gt;
&lt;P&gt;&lt;A href="https://boundarydevices.com/mx6-device-tree-customization/" target="_blank"&gt;https://boundarydevices.com/mx6-device-tree-customization/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-Yocto-Project-How-can-I-quickly-modify-the-kernel-and-test/ta-p/1129551" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-Yocto-Project-How-can-I-quickly-modify-the-kernel-and-test/ta-p/1129551&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 10:12:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-file/m-p/1291857#M175480</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2021-06-14T10:12:06Z</dc:date>
    </item>
    <item>
      <title>Re: Device Tree file</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-file/m-p/1291875#M175484</link>
      <description>&lt;P&gt;I have modified the device tree and added the dtb file in the u-boot time and booted the EVK board, when I'm exporting the gpio pins and checking the voltage levels using multimeter I'm unable to find the difference I have used Imx8m mini evk and the pin number is MX8MM_IOMUXC_SAI5_RXD1_GPIO3_IO22&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;0x19 and I have enable the sai5 group in dts file.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 10:58:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-file/m-p/1291875#M175484</guid>
      <dc:creator>VinithNama</dc:creator>
      <dc:date>2021-06-14T10:58:28Z</dc:date>
    </item>
    <item>
      <title>Re: Device Tree file</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-file/m-p/1769110#M216895</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/184278"&gt;@VinithNama&lt;/a&gt;&amp;nbsp; ,&lt;BR /&gt;&lt;BR /&gt;you can check either of any&lt;BR /&gt;1. DTBO is implemented which is overwriting your dts configuration&lt;BR /&gt;2. Check the md5sum of the actual generated dtb vs on board dtb&lt;BR /&gt;3. In U-boot check weather the dtbo is actually being taken into account while booting kernel using printenv command&lt;BR /&gt;4. Perhaps the same GPIO is being configured alternatively, the final config can be checked post booting /sys/kernel/debug/gpio ?&lt;BR /&gt;&lt;BR /&gt;--&lt;BR /&gt;Rutvij Trivedi&lt;BR /&gt;&lt;A href="https://siliconsignals.io/" target="_self"&gt;Silicon Signals Pvt. Ltd&lt;/A&gt;.&lt;BR /&gt;&lt;A href="mailto:info@siliconsignals.io" target="_blank"&gt;info@siliconsignals.io&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;--&lt;BR /&gt;Rutvij Trivedi&lt;/P&gt;</description>
      <pubDate>Tue, 05 Dec 2023 14:43:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Device-Tree-file/m-p/1769110#M216895</guid>
      <dc:creator>r_trivedi123</dc:creator>
      <dc:date>2023-12-05T14:43:47Z</dc:date>
    </item>
  </channel>
</rss>