<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can IMX8ulp MIPI-DSI support 720P in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-IMX8ulp-MIPI-DSI-support-720P/m-p/1768942#M216880</link>
    <description>&lt;P&gt;Can IMX8ulp's&amp;nbsp; 4 lanes MIPI-DSI support 720P (720 X 3 RGB X 1280)&amp;nbsp; at 60 frames per second? if not, what frame speed can be supported? 30, 20 ,15 or less? Thanks.&lt;/P&gt;</description>
    <pubDate>Tue, 05 Dec 2023 09:43:52 GMT</pubDate>
    <dc:creator>zlxie</dc:creator>
    <dc:date>2023-12-05T09:43:52Z</dc:date>
    <item>
      <title>Can IMX8ulp MIPI-DSI support 720P</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-IMX8ulp-MIPI-DSI-support-720P/m-p/1768942#M216880</link>
      <description>&lt;P&gt;Can IMX8ulp's&amp;nbsp; 4 lanes MIPI-DSI support 720P (720 X 3 RGB X 1280)&amp;nbsp; at 60 frames per second? if not, what frame speed can be supported? 30, 20 ,15 or less? Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 05 Dec 2023 09:43:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-IMX8ulp-MIPI-DSI-support-720P/m-p/1768942#M216880</guid>
      <dc:creator>zlxie</dc:creator>
      <dc:date>2023-12-05T09:43:52Z</dc:date>
    </item>
    <item>
      <title>Re: Can IMX8ulp MIPI-DSI support 720P</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-IMX8ulp-MIPI-DSI-support-720P/m-p/1769616#M216934</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/159450"&gt;@zlxie&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;Please refer to &lt;STRONG&gt;Chapter 61 MIPI-DSI Host Controller (MIPI-DSI)&lt;/STRONG&gt; from the link below.&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/reference-manual/IMX8ULPRM.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/reference-manual/IMX8ULPRM.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;It will help you&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Sanket Parekh&lt;/P&gt;</description>
      <pubDate>Wed, 06 Dec 2023 08:42:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-IMX8ulp-MIPI-DSI-support-720P/m-p/1769616#M216934</guid>
      <dc:creator>Sanket_Parekh</dc:creator>
      <dc:date>2023-12-06T08:42:25Z</dc:date>
    </item>
    <item>
      <title>Re: Can IMX8ulp MIPI-DSI support 720P</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-IMX8ulp-MIPI-DSI-support-720P/m-p/1769624#M216936</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;That doesn't answer the question though. The chapter only mentions:&lt;/P&gt;&lt;P&gt;"This module does not support the 74.25 MHz pixel clock rate generation for 720p60 and 1080p30 resolutions."&lt;/P&gt;&lt;P&gt;But it doesn't say the maximum pixel clock supported and therefore what framerate can be achieved at 720p (45fps)?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gary&lt;/P&gt;</description>
      <pubDate>Wed, 06 Dec 2023 08:50:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-IMX8ulp-MIPI-DSI-support-720P/m-p/1769624#M216936</guid>
      <dc:creator>gary_bisson</dc:creator>
      <dc:date>2023-12-06T08:50:58Z</dc:date>
    </item>
  </channel>
</rss>