<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Disable AGL Reference UI in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Disable-AGL-Reference-UI/m-p/1768585#M216838</link>
    <description>&lt;P&gt;If you are using Yocto from NXP, the start of AGL/weston is controlled by systemctl, you should find that service and disable it.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 05 Dec 2023 01:07:06 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2023-12-05T01:07:06Z</dc:date>
    <item>
      <title>Disable AGL Reference UI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Disable-AGL-Reference-UI/m-p/1766979#M216676</link>
      <description>&lt;P&gt;I have built an AGL image using yocto. But I can't disable the reference ui (home screen of agl).&lt;/P&gt;&lt;P&gt;I tried building other images than agl-demo-platform, like agl-image-weston but then there isn't anything in the display at all.&lt;/P&gt;&lt;P&gt;I've also tried to edit the config files and set the default compositor to weston still it doesn't work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Eighter it shows the refrence ui or it is complete blank(with a single cursor blinking)&lt;/P&gt;&lt;P&gt;How can I Disable the reference ui and replace agl-compositor with weston/wayland.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Dec 2023 06:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Disable-AGL-Reference-UI/m-p/1766979#M216676</guid>
      <dc:creator>donjacobvellathottam</dc:creator>
      <dc:date>2023-12-01T06:28:48Z</dc:date>
    </item>
    <item>
      <title>Re: Disable AGL Reference UI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Disable-AGL-Reference-UI/m-p/1768585#M216838</link>
      <description>&lt;P&gt;If you are using Yocto from NXP, the start of AGL/weston is controlled by systemctl, you should find that service and disable it.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Dec 2023 01:07:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Disable-AGL-Reference-UI/m-p/1768585#M216838</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2023-12-05T01:07:06Z</dc:date>
    </item>
    <item>
      <title>Re: Disable AGL Reference UI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Disable-AGL-Reference-UI/m-p/1780014#M217867</link>
      <description>sorry but i wasn't able to find weston services in systemctl</description>
      <pubDate>Tue, 26 Dec 2023 09:50:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Disable-AGL-Reference-UI/m-p/1780014#M217867</guid>
      <dc:creator>donjacobvellathottam</dc:creator>
      <dc:date>2023-12-26T09:50:53Z</dc:date>
    </item>
  </channel>
</rss>