<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX8M Plus - 8 Lane CSI</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1768188#M216797</link>
    <description>&lt;P&gt;Hi Joan,&lt;/P&gt;&lt;P&gt;I understand each MIPI can support up to 4 lanes.&lt;/P&gt;&lt;P&gt;Can I combine both MIPI 4 lanes to handle a single image sensor that requires 2 x 4 lanes MIPI CSI interface? One example is&amp;nbsp;&lt;SPAN&gt;OMNIVISION’s OV13870. Can iMX8M Plus support this OMNIVISION image sensor? Can the iMX8M Plus merge data from both the MIPI interface to become a single image? Or it will always treat both MIPI interface as 2 separate images?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Usually image sensors with higher number of pixels (&amp;gt; 10MPix) will require more than 4 lanes due to the speed limitation of each lane.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 04 Dec 2023 10:09:16 GMT</pubDate>
    <dc:creator>MPUUser</dc:creator>
    <dc:date>2023-12-04T10:09:16Z</dc:date>
    <item>
      <title>iMX8M Plus - 8 Lane CSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1768061#M216778</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I understand iMX8MPlus supports 2 x 4 lane MIPI CSI-2, i.e. it supports 2 camera each with 4 lane MIPI CSI-2. Can it support a single camera (single image sensor) that requires 2 x 4 lane MIPI CSI-2?&lt;/P&gt;</description>
      <pubDate>Mon, 04 Dec 2023 08:07:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1768061#M216778</guid>
      <dc:creator>MPUUser</dc:creator>
      <dc:date>2023-12-04T08:07:21Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus - 8 Lane CSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1768167#M216793</link>
      <description>&lt;P&gt;each imx8mp mipi csi can support up to 4 lane, couldn't support 8 lane, but could you tell me what camera needs 8 lane?&lt;/P&gt;</description>
      <pubDate>Mon, 04 Dec 2023 09:45:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1768167#M216793</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-12-04T09:45:16Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus - 8 Lane CSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1768188#M216797</link>
      <description>&lt;P&gt;Hi Joan,&lt;/P&gt;&lt;P&gt;I understand each MIPI can support up to 4 lanes.&lt;/P&gt;&lt;P&gt;Can I combine both MIPI 4 lanes to handle a single image sensor that requires 2 x 4 lanes MIPI CSI interface? One example is&amp;nbsp;&lt;SPAN&gt;OMNIVISION’s OV13870. Can iMX8M Plus support this OMNIVISION image sensor? Can the iMX8M Plus merge data from both the MIPI interface to become a single image? Or it will always treat both MIPI interface as 2 separate images?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Usually image sensors with higher number of pixels (&amp;gt; 10MPix) will require more than 4 lanes due to the speed limitation of each lane.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Dec 2023 10:09:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1768188#M216797</guid>
      <dc:creator>MPUUser</dc:creator>
      <dc:date>2023-12-04T10:09:16Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus - 8 Lane CSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1770317#M216987</link>
      <description>&lt;P&gt;Can iMX8M Plus support this OMNIVISION image sensor?&lt;/P&gt;
&lt;P&gt;&amp;gt;yes, current bsp supports ov2775 and ov5640 as default&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Usually image sensors with higher number of pixels (&amp;gt; 10MPix) will require more than 4 lanes due to the speed limitation of each lane.&lt;/P&gt;
&lt;P&gt;&amp;gt;imx8mp mipi csi can support 1.5Gx4=6Gbps, if your sensor &lt;A href="mailto:i@30," target="_blank"&gt;i&lt;/A&gt;s &lt;A href="mailto:10M@30," target="_blank"&gt;10M@30,&lt;/A&gt; this is 10x30x16=4.8G&amp;lt;6G, and you can current ISP can support up to 12M camera, so I don't think you need use dual mipi csi to one camera&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="joanxie_1-1701915576036.png" style="width: 594px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/253290i6587B6D1120EA80D/image-dimensions/594x143?v=v2" width="594" height="143" role="button" title="joanxie_1-1701915576036.png" alt="joanxie_1-1701915576036.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Dec 2023 02:19:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1770317#M216987</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-12-07T02:19:50Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus - 8 Lane CSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1770519#M217006</link>
      <description>&lt;P&gt;Hi Joan,&lt;/P&gt;&lt;P&gt;What about&amp;nbsp;&lt;SPAN&gt;OV13870. Can it be supported?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There are sensors with much higher resolution (eg 20MP) and they need 2 x 4 MIPI lanes per sensor.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can iMX8M Plus support such sensors?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Dec 2023 07:55:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1770519#M217006</guid>
      <dc:creator>MPUUser</dc:creator>
      <dc:date>2023-12-07T07:55:11Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus - 8 Lane CSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1770731#M217018</link>
      <description>&lt;P&gt;unfortunately imx8mp couldn't support this&lt;/P&gt;</description>
      <pubDate>Thu, 07 Dec 2023 12:08:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1770731#M217018</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-12-07T12:08:55Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8M Plus - 8 Lane CSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1770763#M217021</link>
      <description>&lt;P&gt;imx8mp doesn't support vc&lt;/P&gt;</description>
      <pubDate>Thu, 07 Dec 2023 12:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8M-Plus-8-Lane-CSI/m-p/1770763#M217021</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-12-07T12:53:46Z</dc:date>
    </item>
  </channel>
</rss>