<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.MX8mP: RC side does not recognize EP side</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8mP-RC-side-does-not-recognize-EP-side/m-p/1766719#M216653</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Unfortunately cannot comment much on this issue, since we cannot replicate this on our EVK, I would recommend checking if there is some communication going from your board to the host PC.&lt;BR /&gt;&lt;BR /&gt;Also, I would recommend checking with your board supplier if there si some issues when using the connector you're using.&lt;BR /&gt;&lt;BR /&gt;Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Thu, 30 Nov 2023 19:35:02 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2023-11-30T19:35:02Z</dc:date>
    <item>
      <title>i.MX8mP: RC side does not recognize EP side</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8mP-RC-side-does-not-recognize-EP-side/m-p/1765716#M216556</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;My goal is to set the i.MX8mP board to EP mode and access EP through the PCIe connection on the RC side (PC). I have successfully set the board to EP mode using &lt;EM&gt;&lt;STRONG&gt;setenv imx8mp-evk-pcie-ep.dts&lt;/STRONG&gt;.&lt;/EM&gt; Here is the boot environment configuration and the dmesg of the development board:&lt;/SPAN&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;fdt_addr=0x43000000
fdt_file=imx8mp-evk-pcie-ep.dtb
fdt_high=0xffffffffffffffff&lt;/LI-CODE&gt;&lt;LI-CODE lang="markup"&gt;root@OK8MP:~# dmesg | grep pcie
[    2.810289] imx6q-pcie 33800000.pcie_ep: 33800000.pcie_ep supply epdev_on not found, using dummy regulator
[    2.829085] imx6q-pcie 33800000.pcie_ep: EXT REF_CLK is used!.
[    2.835560] imx6q-pcie 33800000.pcie_ep: PCIe PHY PLL clock is locked.
[    2.842165] imx6q-pcie 33800000.pcie_ep: PCIe PLL locked after 0 us.&lt;/LI-CODE&gt;&lt;P&gt;&lt;SPAN&gt;However, when I check with lspci on the RC side, I found that the new device is not recognized. The Device Manager in Windows 10 also does not show any new devices. My PCIe connection cable is like this:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="微信图片_20231129211027.jpg" style="width: 200px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/252120iAFA4EABB47E94198/image-size/small?v=v2&amp;amp;px=200" role="button" title="微信图片_20231129211027.jpg" alt="微信图片_20231129211027.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I can directly power the i.MX8mP from the PC motherboard using the PCIe connection cable without the need for power from the board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have also referred to this article(&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX6Q-PCIe-EP-RC-Validation-System/ta-p/1126624" target="_self"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX6Q-PCIe-EP-RC-Validation-System/ta-p/1126624&lt;/A&gt;&amp;nbsp;), but the difference is that my board is from the supplier Forlinx, and it has a PCIe 3.0x1 slot on the baseboard.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is this a problem with the connection cable or the PCIe power supply? How can I solve this problem?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Nov 2023 13:25:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8mP-RC-side-does-not-recognize-EP-side/m-p/1765716#M216556</guid>
      <dc:creator>22721579</dc:creator>
      <dc:date>2023-11-29T13:25:53Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8mP: RC side does not recognize EP side</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8mP-RC-side-does-not-recognize-EP-side/m-p/1766719#M216653</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Unfortunately cannot comment much on this issue, since we cannot replicate this on our EVK, I would recommend checking if there is some communication going from your board to the host PC.&lt;BR /&gt;&lt;BR /&gt;Also, I would recommend checking with your board supplier if there si some issues when using the connector you're using.&lt;BR /&gt;&lt;BR /&gt;Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Thu, 30 Nov 2023 19:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8mP-RC-side-does-not-recognize-EP-side/m-p/1766719#M216653</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2023-11-30T19:35:02Z</dc:date>
    </item>
  </channel>
</rss>