<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: YOLO tflite code Request to run on IMX8 Board C++ in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/1766641#M216647</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207096"&gt;@brian14&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thank you for the reply.&lt;/P&gt;&lt;P&gt;No I didn't use model using eIQ Toolkit. I have trained and converted yolov8 on custom dataset using their GitHub page here is for your reference the link and as well as quantized model.&lt;BR /&gt;&lt;BR /&gt;I have check eIQ Toolkit and can't find a model for yolov8 or v5 built in as it has mobileNet and Yolov4.&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/ultralytics/ultralytic" target="_blank" rel="noopener"&gt;https://github.com/ultralytics/ultralytic&lt;/A&gt;&lt;/P&gt;&lt;P&gt;For Quantization command:&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;yolo export &lt;/SPAN&gt;&lt;SPAN&gt;model&lt;/SPAN&gt;&lt;SPAN&gt;=&lt;/SPAN&gt;&lt;SPAN&gt;'best.pt'&lt;/SPAN&gt; &lt;SPAN&gt;format&lt;/SPAN&gt;&lt;SPAN&gt;=&lt;/SPAN&gt;&lt;SPAN&gt;tflite &lt;/SPAN&gt;&lt;SPAN&gt;int8&lt;/SPAN&gt;&lt;SPAN&gt;=&lt;/SPAN&gt;&lt;SPAN&gt;True&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Thu, 30 Nov 2023 16:48:29 GMT</pubDate>
    <dc:creator>wamiq_raza</dc:creator>
    <dc:date>2023-11-30T16:48:29Z</dc:date>
    <item>
      <title>YOLO tflite code Request to run on IMX8 Board C++</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/1759987#M216012</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;Can someone provide a complete C++ code of tflite deployment on board. I am having problem to find the code also&amp;nbsp;I can't find on yolo repository for tflite model. I wrote but it has a lot of errors jso it is not the correct version I think.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 17:01:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/1759987#M216012</guid>
      <dc:creator>wamiqraza</dc:creator>
      <dc:date>2023-11-20T17:01:04Z</dc:date>
    </item>
    <item>
      <title>Re: YOLO tflite code Request to run on IMX8 Board C++</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/1762109#M216209</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225987"&gt;@wamiqraza&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can use the following code as an example:&lt;BR /&gt;&lt;A href="https://github.com/nxp-imx/tensorflow-imx/blob/lf-6.1.36_2.1.0/tensorflow/lite/examples/label_image/label_image.cc" target="_blank"&gt;tensorflow-imx/tensorflow/lite/examples/label_image/label_image.cc at lf-6.1.36_2.1.0 · nxp-imx/tensorflow-imx · GitHub&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I hope this information will be helpful.&lt;/P&gt;
&lt;P&gt;Have a great day!&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 17:23:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/1762109#M216209</guid>
      <dc:creator>brian14</dc:creator>
      <dc:date>2023-11-22T17:23:41Z</dc:date>
    </item>
    <item>
      <title>Re: YOLO tflite code Request to run on IMX8 Board C++</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/1764738#M216456</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207096"&gt;@brian14&lt;/a&gt;Thank you for the reference. I have also gone through documentation of NXP and was able to deploy MobileNetV2 pre-trained, MobileNetV2 trained on custom dataset bot int8 quantized and then yolov8 on custom dataset float32 quantized and int8 respectively. I am using GStreamer pipeline, as its for production project and some details will share here. Due to privacy reason full code I can't disclose in public. Would request for meeting if the team can contact via my email: &lt;A href="mailto:wamiq.raza@kineton.it" target="_blank" rel="noopener"&gt;wamiq.raza@kineton.it&lt;/A&gt;&lt;/P&gt;&lt;P&gt;As the product is about to launch and one of the barrier we are facing in detection. For instance model has low FPS and not utilizing GPU.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is the part of code that load the model:&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;std&lt;/SPAN&gt;&lt;SPAN&gt;::unique_ptr&lt;/SPAN&gt;&lt;SPAN&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN&gt;tflite&lt;/SPAN&gt;&lt;SPAN&gt;::Interpreter&lt;/SPAN&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt; interpreter;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;// ================== Load model ==================&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;std&lt;/SPAN&gt;&lt;SPAN&gt;::unique_ptr&lt;/SPAN&gt;&lt;SPAN&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN&gt;tflite&lt;/SPAN&gt;&lt;SPAN&gt;::FlatBufferModel&lt;/SPAN&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt; model &lt;/SPAN&gt;&lt;SPAN&gt;=&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;tflite&lt;/SPAN&gt;&lt;SPAN&gt;::&lt;/SPAN&gt;&lt;SPAN&gt;FlatBufferModel&lt;/SPAN&gt;&lt;SPAN&gt;::&lt;/SPAN&gt;&lt;SPAN&gt;BuildFromFile&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;modelPath&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;SPAN&gt;c_str&lt;/SPAN&gt;&lt;SPAN&gt;());&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;std&lt;/SPAN&gt;&lt;SPAN&gt;::&lt;/SPAN&gt;&lt;SPAN&gt;cout&lt;/SPAN&gt; &lt;SPAN&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN&gt;std&lt;/SPAN&gt;&lt;SPAN&gt;::&lt;/SPAN&gt;&lt;SPAN&gt;endl&lt;/SPAN&gt; &lt;SPAN&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN&gt;"Model Loaded!"&lt;/SPAN&gt; &lt;SPAN&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN&gt;std&lt;/SPAN&gt;&lt;SPAN&gt;::&lt;/SPAN&gt;&lt;SPAN&gt;endl&lt;/SPAN&gt; &lt;SPAN&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN&gt;std&lt;/SPAN&gt;&lt;SPAN&gt;::&lt;/SPAN&gt;&lt;SPAN&gt;endl&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;SPAN&gt;TFLITE_MINIMAL_CHECK&lt;/SPAN&gt;&lt;SPAN&gt;(model &lt;/SPAN&gt;&lt;SPAN&gt;!=&lt;/SPAN&gt; &lt;SPAN&gt;nullptr&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;// ================== Define Interpreter ==================&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;tflite&lt;/SPAN&gt;&lt;SPAN&gt;::&lt;/SPAN&gt;&lt;SPAN&gt;ops&lt;/SPAN&gt;&lt;SPAN&gt;::&lt;/SPAN&gt;&lt;SPAN&gt;builtin&lt;/SPAN&gt;&lt;SPAN&gt;::BuiltinOpResolver resolver;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;tflite&lt;/SPAN&gt;&lt;SPAN&gt;::&lt;/SPAN&gt;&lt;SPAN&gt;InterpreterBuilder&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;*&lt;/SPAN&gt;&lt;SPAN&gt;model, resolver)(&lt;/SPAN&gt;&lt;SPAN&gt;&amp;amp;&lt;/SPAN&gt;&lt;SPAN&gt;interpreter);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;TFLITE_MINIMAL_CHECK&lt;/SPAN&gt;&lt;SPAN&gt;(interpreter &lt;/SPAN&gt;&lt;SPAN&gt;!=&lt;/SPAN&gt; &lt;SPAN&gt;nullptr&lt;/SPAN&gt;&lt;SPAN&gt;);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;// ================== Delegating GPU ==================&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;TfLiteDelegatePtr&lt;/SPAN&gt; &lt;SPAN&gt;ptr&lt;/SPAN&gt; &lt;SPAN&gt;=&lt;/SPAN&gt; &lt;SPAN&gt;CreateTfLiteDelegate&lt;/SPAN&gt;&lt;SPAN&gt;();&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;TFLITE_MINIMAL_CHECK&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;interpreter&lt;/SPAN&gt;&lt;SPAN&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;ModifyGraphWithDelegate&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;std&lt;/SPAN&gt;&lt;SPAN&gt;::&lt;/SPAN&gt;&lt;SPAN&gt;move&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;ptr&lt;/SPAN&gt;&lt;SPAN&gt;)) &lt;/SPAN&gt;&lt;SPAN&gt;==&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;kTfLiteOk);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;// ================== Allocate tensor buffers ==================&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;TFLITE_MINIMAL_CHECK&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;interpreter&lt;/SPAN&gt;&lt;SPAN&gt;-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;AllocateTensors&lt;/SPAN&gt;&lt;SPAN&gt;() &lt;/SPAN&gt;&lt;SPAN&gt;==&lt;/SPAN&gt;&lt;SPAN&gt; kTfLiteOk);&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below are the terminal print for when loading MobileNetV2 for inference.&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;SPAN&gt;Streams opened successfully!&lt;BR /&gt;Vx delegate: allowed_cache_mode set to 0.&lt;BR /&gt;Vx delegate: allowed_builtin_code set to 0.&lt;BR /&gt;Vx delegate: error_during_init set to 0.&lt;BR /&gt;Vx delegate: error_during_prepare set to 0.&lt;BR /&gt;Vx delegate: error_during_invoke set to 0.&lt;BR /&gt;ERROR: Fallback unsupported op 32 to TfLite&lt;BR /&gt;INFO: Created TensorFlow Lite XNNPACK delegate for CPU.&lt;BR /&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;BR /&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;BR /&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;BR /&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;BR /&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;BR /&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;BR /&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;BR /&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;BR /&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;BR /&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;BR /&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;BR /&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;BR /&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Below are the terminal print for when loading Yolov8 for inference. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT color="#FF0000"&gt;Streams opened successfully!&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;Vx delegate: allowed_cache_mode set to 0.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;Vx delegate: allowed_builtin_code set to 0.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;Vx delegate: error_during_init set to 0.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;Vx delegate: error_during_prepare set to 0.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;Vx delegate: error_during_invoke set to 0.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;W [HandleLayoutInfer:268]Op 162: default layout inference pass.&lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;---------------------------------------------------------------------------------------&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Would like to arrange meeting with deep learning model deployment team and suggestion on above details.&lt;BR /&gt;&lt;BR /&gt;Please let me know if you need additional details of information. &lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 08:55:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/1764738#M216456</guid>
      <dc:creator>wamiqraza</dc:creator>
      <dc:date>2023-11-28T08:55:10Z</dc:date>
    </item>
    <item>
      <title>Re: YOLO tflite code Request to run on IMX8 Board C++</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/1766014#M216586</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225987"&gt;@wamiqraza&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your reply.&lt;/P&gt;
&lt;P&gt;To analyze in more detail the problem I would like to check your model. It seems that is not correctly optimized for the i.MX processors. &lt;BR /&gt;Do you trained your model using eIQ Toolkit?&lt;/P&gt;
&lt;P&gt;On other hand, for a meeting and personalized support you can verify this link:&lt;BR /&gt;&lt;A href="https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and-microcontrollers:PREMIUM-SUPPORT" target="_blank"&gt;Professional Support for Processors and Microcontrollers | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Have a great day!&lt;/P&gt;</description>
      <pubDate>Thu, 30 Nov 2023 00:45:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/1766014#M216586</guid>
      <dc:creator>brian14</dc:creator>
      <dc:date>2023-11-30T00:45:41Z</dc:date>
    </item>
    <item>
      <title>Re: YOLO tflite code Request to run on IMX8 Board C++</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/1766641#M216647</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207096"&gt;@brian14&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thank you for the reply.&lt;/P&gt;&lt;P&gt;No I didn't use model using eIQ Toolkit. I have trained and converted yolov8 on custom dataset using their GitHub page here is for your reference the link and as well as quantized model.&lt;BR /&gt;&lt;BR /&gt;I have check eIQ Toolkit and can't find a model for yolov8 or v5 built in as it has mobileNet and Yolov4.&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/ultralytics/ultralytic" target="_blank" rel="noopener"&gt;https://github.com/ultralytics/ultralytic&lt;/A&gt;&lt;/P&gt;&lt;P&gt;For Quantization command:&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;yolo export &lt;/SPAN&gt;&lt;SPAN&gt;model&lt;/SPAN&gt;&lt;SPAN&gt;=&lt;/SPAN&gt;&lt;SPAN&gt;'best.pt'&lt;/SPAN&gt; &lt;SPAN&gt;format&lt;/SPAN&gt;&lt;SPAN&gt;=&lt;/SPAN&gt;&lt;SPAN&gt;tflite &lt;/SPAN&gt;&lt;SPAN&gt;int8&lt;/SPAN&gt;&lt;SPAN&gt;=&lt;/SPAN&gt;&lt;SPAN&gt;True&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 30 Nov 2023 16:48:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/1766641#M216647</guid>
      <dc:creator>wamiq_raza</dc:creator>
      <dc:date>2023-11-30T16:48:29Z</dc:date>
    </item>
    <item>
      <title>Re: YOLO tflite code Request to run on IMX8 Board C++</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/1768399#M216818</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226345"&gt;@wamiq_raza&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your reply.&lt;/P&gt;
&lt;P&gt;I will check your model, and then give you some recommendations.&lt;/P&gt;
&lt;P&gt;Have a great day!&lt;/P&gt;</description>
      <pubDate>Mon, 04 Dec 2023 17:18:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/1768399#M216818</guid>
      <dc:creator>brian14</dc:creator>
      <dc:date>2023-12-04T17:18:22Z</dc:date>
    </item>
    <item>
      <title>Re: YOLO tflite code Request to run on IMX8 Board C++</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/2010525#M231740</link>
      <description>I'm running in to this same issue. Any update?</description>
      <pubDate>Mon, 09 Dec 2024 22:48:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/YOLO-tflite-code-Request-to-run-on-IMX8-Board-C/m-p/2010525#M231740</guid>
      <dc:creator>jb_pdx</dc:creator>
      <dc:date>2024-12-09T22:48:58Z</dc:date>
    </item>
  </channel>
</rss>