<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMXRT1050-EVKB PCB layout file</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1050-EVKB-PCB-layout-file/m-p/1765232#M216485</link>
    <description>&lt;P&gt;When designing the PCB layout for the SDRAM interface, the MIMXRT1050 Hardware Development Guide says "Ideally, route all signals at the same length as the EVK board. See the IMXRT1050-EVKB layout to route all signals at the same length (±50 mils)."&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, the EVK board layout is provided as an Allegro binary file (.brd), which can only be opened on a computer that has Allegro installed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;Is the IMXRT1050-EVKB PCB layout available in a format that can be read with Altium Designer, such as an Allegro ASCII file (.alg) or an Altium Designer layout file (.PcbDoc)?&lt;/P&gt;</description>
    <pubDate>Tue, 28 Nov 2023 22:31:21 GMT</pubDate>
    <dc:creator>dbaselt</dc:creator>
    <dc:date>2023-11-28T22:31:21Z</dc:date>
    <item>
      <title>IMXRT1050-EVKB PCB layout file</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMXRT1050-EVKB-PCB-layout-file/m-p/1765232#M216485</link>
      <description>&lt;P&gt;When designing the PCB layout for the SDRAM interface, the MIMXRT1050 Hardware Development Guide says "Ideally, route all signals at the same length as the EVK board. See the IMXRT1050-EVKB layout to route all signals at the same length (±50 mils)."&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, the EVK board layout is provided as an Allegro binary file (.brd), which can only be opened on a computer that has Allegro installed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;Is the IMXRT1050-EVKB PCB layout available in a format that can be read with Altium Designer, such as an Allegro ASCII file (.alg) or an Altium Designer layout file (.PcbDoc)?&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 22:31:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMXRT1050-EVKB-PCB-layout-file/m-p/1765232#M216485</guid>
      <dc:creator>dbaselt</dc:creator>
      <dc:date>2023-11-28T22:31:21Z</dc:date>
    </item>
  </channel>
</rss>