<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8ULP LPSPI Demo Not working in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8ULP-LPSPI-Demo-Not-working/m-p/1764354#M216428</link>
    <description>&lt;P&gt;When I try to run any of the LPSPI examples on IMX8ULP (ex. lpspi_edma_b2b_transfer_master.c) the data doesn't seem to be read or outputted. On the oscilliscope, I can see that chip select is switching, and sck is switching, but sout doesn't have any data. Setting Sin Low/High Doesn't change recerived data either. Please Help!&lt;/P&gt;</description>
    <pubDate>Tue, 28 Nov 2023 00:12:45 GMT</pubDate>
    <dc:creator>shaunakk</dc:creator>
    <dc:date>2023-11-28T00:12:45Z</dc:date>
    <item>
      <title>IMX8ULP LPSPI Demo Not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8ULP-LPSPI-Demo-Not-working/m-p/1764354#M216428</link>
      <description>&lt;P&gt;When I try to run any of the LPSPI examples on IMX8ULP (ex. lpspi_edma_b2b_transfer_master.c) the data doesn't seem to be read or outputted. On the oscilliscope, I can see that chip select is switching, and sck is switching, but sout doesn't have any data. Setting Sin Low/High Doesn't change recerived data either. Please Help!&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 00:12:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8ULP-LPSPI-Demo-Not-working/m-p/1764354#M216428</guid>
      <dc:creator>shaunakk</dc:creator>
      <dc:date>2023-11-28T00:12:45Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8ULP LPSPI Demo Not working</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8ULP-LPSPI-Demo-Not-working/m-p/1765451#M216510</link>
      <description>&lt;P&gt;Which version of SDK are you using?&lt;/P&gt;
&lt;P&gt;Which board are you using?&lt;/P&gt;
&lt;P&gt;How you connect the two spi?&lt;/P&gt;
&lt;P&gt;Is there any error message?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Nov 2023 07:14:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8ULP-LPSPI-Demo-Not-working/m-p/1765451#M216510</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2023-11-29T07:14:49Z</dc:date>
    </item>
  </channel>
</rss>