<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UUU tool using UART Port in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UUU-tool-using-UART-Port/m-p/1763325#M216349</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226185"&gt;@ahmedmd&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;i.MX8QXP does not support flashing or downloading bootimage over UART.&lt;/P&gt;
&lt;P&gt;It only supports USB 2.0 OTG and USB 3.0 ports.&lt;/P&gt;
&lt;P&gt;Please refer to&lt;STRONG&gt;&amp;nbsp;5.10 Serial Downloader Boot&lt;/STRONG&gt; in&amp;nbsp;i.MX 8DualX/8DualXPlus/8QuadXPlus&lt;BR /&gt;Applications Processor Reference Manual for more information.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
    <pubDate>Fri, 24 Nov 2023 10:52:31 GMT</pubDate>
    <dc:creator>Dhruvit</dc:creator>
    <dc:date>2023-11-24T10:52:31Z</dc:date>
    <item>
      <title>UUU tool using UART Port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UUU-tool-using-UART-Port/m-p/1763264#M216334</link>
      <description>&lt;P&gt;Hello Guys,&lt;BR /&gt;&lt;BR /&gt;There is an use case in which I need to flash a Linux BSP on my iMX8QXP board thorough UART port since only that port is available. How do I configure the UUU tool to flash the board using the UART port ?&lt;/P&gt;</description>
      <pubDate>Fri, 24 Nov 2023 09:40:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UUU-tool-using-UART-Port/m-p/1763264#M216334</guid>
      <dc:creator>ahmedmd</dc:creator>
      <dc:date>2023-11-24T09:40:39Z</dc:date>
    </item>
    <item>
      <title>Re: UUU tool using UART Port</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UUU-tool-using-UART-Port/m-p/1763325#M216349</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226185"&gt;@ahmedmd&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;i.MX8QXP does not support flashing or downloading bootimage over UART.&lt;/P&gt;
&lt;P&gt;It only supports USB 2.0 OTG and USB 3.0 ports.&lt;/P&gt;
&lt;P&gt;Please refer to&lt;STRONG&gt;&amp;nbsp;5.10 Serial Downloader Boot&lt;/STRONG&gt; in&amp;nbsp;i.MX 8DualX/8DualXPlus/8QuadXPlus&lt;BR /&gt;Applications Processor Reference Manual for more information.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Fri, 24 Nov 2023 10:52:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UUU-tool-using-UART-Port/m-p/1763325#M216349</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-11-24T10:52:31Z</dc:date>
    </item>
  </channel>
</rss>