<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using the __libc_init_array() in C in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-the-libc-init-array-in-C/m-p/1762862#M216291</link>
    <description>&lt;P&gt;Hi Bio_TICFSL, how can i put this function before the main?&lt;/P&gt;</description>
    <pubDate>Thu, 23 Nov 2023 16:46:46 GMT</pubDate>
    <dc:creator>andréluis</dc:creator>
    <dc:date>2023-11-23T16:46:46Z</dc:date>
    <item>
      <title>Using the __libc_init_array() in C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-the-libc-init-array-in-C/m-p/1762149#M216216</link>
      <description>&lt;P&gt;Hi, i'm working with a RT1060 and i compile a program using the 4diac with the runtime Forte. The question is the Forte need the&amp;nbsp;__libc_init_array() to run. And need to run in freeRtos with Lwip because the architecture need to be in Freertos. But Lwip work with C. Can i use this function (__libc_init_array()) in C to run the Forte?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 18:47:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-the-libc-init-array-in-C/m-p/1762149#M216216</guid>
      <dc:creator>andréluis</dc:creator>
      <dc:date>2023-11-22T18:47:35Z</dc:date>
    </item>
    <item>
      <title>Re: Using the __libc_init_array() in C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-the-libc-init-array-in-C/m-p/1762806#M216284</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes you can use it but, This serves calling constructors and other library initialization which is necessary before calling main. There is a good description about this as well on :&lt;/P&gt;
&lt;P&gt;&lt;A href="https://stackoverflow.com/questions/15265295/understanding-the-libc-init-array" target="_blank"&gt;https://stackoverflow.com/questions/15265295/understanding-the-libc-init-array&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 14:59:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-the-libc-init-array-in-C/m-p/1762806#M216284</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-11-23T14:59:30Z</dc:date>
    </item>
    <item>
      <title>Re: Using the __libc_init_array() in C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-the-libc-init-array-in-C/m-p/1762862#M216291</link>
      <description>&lt;P&gt;Hi Bio_TICFSL, how can i put this function before the main?&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 16:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-the-libc-init-array-in-C/m-p/1762862#M216291</guid>
      <dc:creator>andréluis</dc:creator>
      <dc:date>2023-11-23T16:46:46Z</dc:date>
    </item>
  </channel>
</rss>