<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックBoot i.MX 8M Plus by sd Card</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX-8M-Plus-by-sd-Card/m-p/1762847#M216289</link>
    <description>&lt;P&gt;Hi everyone.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a a PCB configure in Boot mode&amp;nbsp; (Internal Fuses ( BOOT_MOD3 = 0 //&amp;nbsp;BOOT_MOD2 = 0 //&amp;nbsp;BOOT_MOD1 = 0 //&amp;nbsp;BOOT_MOD0 = 0).&lt;/P&gt;&lt;P&gt;It's no possible to change the pin states and it's no possible to programm by USB.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any option to make the i.MX to boot from sd Card?&lt;/P&gt;&lt;P&gt;Thanks in advance.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 23 Nov 2023 16:25:01 GMT</pubDate>
    <dc:creator>Guiyo</dc:creator>
    <dc:date>2023-11-23T16:25:01Z</dc:date>
    <item>
      <title>Boot i.MX 8M Plus by sd Card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX-8M-Plus-by-sd-Card/m-p/1762847#M216289</link>
      <description>&lt;P&gt;Hi everyone.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a a PCB configure in Boot mode&amp;nbsp; (Internal Fuses ( BOOT_MOD3 = 0 //&amp;nbsp;BOOT_MOD2 = 0 //&amp;nbsp;BOOT_MOD1 = 0 //&amp;nbsp;BOOT_MOD0 = 0).&lt;/P&gt;&lt;P&gt;It's no possible to change the pin states and it's no possible to programm by USB.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any option to make the i.MX to boot from sd Card?&lt;/P&gt;&lt;P&gt;Thanks in advance.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 16:25:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX-8M-Plus-by-sd-Card/m-p/1762847#M216289</guid>
      <dc:creator>Guiyo</dc:creator>
      <dc:date>2023-11-23T16:25:01Z</dc:date>
    </item>
    <item>
      <title>Re: Boot i.MX 8M Plus by sd Card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX-8M-Plus-by-sd-Card/m-p/1762888#M216293</link>
      <description>&lt;P&gt;Hello, I hope you are doing well.&lt;/P&gt;
&lt;P&gt;You could try to use SD/MMC manufacture mode. When the internal boot and recover boot (if enabled) failed, the boot goes to the SD/MMC manufacture mode before the serial download mode. In the manufacture mode, one bit bus width is used despite of the fuse setting.&lt;/P&gt;
&lt;P&gt;By default, the SD/MMC manufacture mode is enabled. Blow the fuse of the RECOVERY_SDMMC_BOOT_DIS to disable it.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 17:41:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX-8M-Plus-by-sd-Card/m-p/1762888#M216293</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2023-11-23T17:41:49Z</dc:date>
    </item>
    <item>
      <title>Re: Boot i.MX 8M Plus by sd Card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX-8M-Plus-by-sd-Card/m-p/1765030#M216478</link>
      <description>&lt;P&gt;Hi Jorge Castañeda&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;First of all thank you for your reply.&lt;/P&gt;&lt;P&gt;We tried everything possible to flash the bootloader and there was no way.&lt;/P&gt;&lt;P&gt;We looked at many forum answers how to force some pins of the uSD to GND and nothing.&lt;/P&gt;&lt;P&gt;The final solution was to drill the PCB and get to pins A72 and A73 and connect them externally to 1.8V.&lt;/P&gt;&lt;P&gt;This way we were able to flash one of the PCBs.&lt;/P&gt;&lt;P&gt;Another PCB I have a new problem because with the same HW and the same uSD it stops at the next point:&lt;BR /&gt;U-Boot SPL 2022.04-lf_v2022.04+g181859317b (Nov 15 2022 - 06:28:05 +0000)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 4000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;SEC0: RNG instantiated&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;Boot Stage: Recovery boot&lt;BR /&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;BR /&gt;NOTICE: BL31: v2.6(release):automotive-13.0.0_1.1.0-0-g3c1583ba0&lt;BR /&gt;NOTICE: BL31: Built : 11:00:38, Nov 21 2022&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;U-Boot 2022.04-lf_v2022.04+g181859317b (Nov 15 2022 - 06:28:05 +0000)&lt;BR /&gt;&lt;BR /&gt;CPU: i.MX8MP[8] rev1.1 1600 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Industrial temperature grade (-40C to 105C) at 35C&lt;BR /&gt;Reset cause: BY&lt;BR /&gt;Model: Laird Connectivity i.MX8M Plus Summit SOM&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;setup_charger: Can't find device id=0x6b&lt;BR /&gt;Core: 171 devices, 21 uclasses, devicetree: separate&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC...&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;New fixes and new problems :S&lt;/P&gt;&lt;P&gt;I hope it's going well&lt;/P&gt;&lt;P&gt;Translated with DeepL.com (free version)&lt;/P&gt;</description>
      <pubDate>Tue, 28 Nov 2023 15:50:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Boot-i-MX-8M-Plus-by-sd-Card/m-p/1765030#M216478</guid>
      <dc:creator>Guiyo</dc:creator>
      <dc:date>2023-11-28T15:50:14Z</dc:date>
    </item>
  </channel>
</rss>