<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: mmc device tree</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mmc-device-tree/m-p/1762764#M216278</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220763"&gt;@mjaafar&lt;/a&gt;!&lt;BR /&gt;Thank you for contacting NXP Support!&lt;BR /&gt;&lt;BR /&gt;You can refer to the device tree of our imx8mp-evk by following the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mp-evk.dts" target="_blank"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mp-evk.dts&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;I attached an image to see the usage on imx8mn-evk, you can use it as an example is the same for imx8mp-evk.&lt;BR /&gt;&lt;BR /&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
    <pubDate>Thu, 23 Nov 2023 13:53:13 GMT</pubDate>
    <dc:creator>Chavira</dc:creator>
    <dc:date>2023-11-23T13:53:13Z</dc:date>
    <item>
      <title>mmc device tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mmc-device-tree/m-p/1762647#M216268</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I m using the imx8mplus and want to add a new mmc to the device tree. Can you please help me define it.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 11:00:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mmc-device-tree/m-p/1762647#M216268</guid>
      <dc:creator>mjaafar</dc:creator>
      <dc:date>2023-11-23T11:00:22Z</dc:date>
    </item>
    <item>
      <title>Re: mmc device tree</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mmc-device-tree/m-p/1762764#M216278</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220763"&gt;@mjaafar&lt;/a&gt;!&lt;BR /&gt;Thank you for contacting NXP Support!&lt;BR /&gt;&lt;BR /&gt;You can refer to the device tree of our imx8mp-evk by following the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mp-evk.dts" target="_blank"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mp-evk.dts&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;I attached an image to see the usage on imx8mn-evk, you can use it as an example is the same for imx8mp-evk.&lt;BR /&gt;&lt;BR /&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 13:53:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mmc-device-tree/m-p/1762764#M216278</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2023-11-23T13:53:13Z</dc:date>
    </item>
  </channel>
</rss>