<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 i.MX8MP - Boot via u-Boot - binary structure</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Boot-via-u-Boot-binary-structure/m-p/1762557#M216254</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to understand how the resulting boot binary must be combined that the i.MX8MP will boot properly by u-Boot bootloader.&lt;/P&gt;&lt;P&gt;I found already some documentation which are addressing this topic (i.MX Linux User's Guide, AN1403: Fast Boot on i.MX8M and i.MX9 using Falcon Mode and Kernel Optimizations) but I did not find a documentation how the SPL+ATF+u-Boot must be fit together so that is will run.&lt;/P&gt;&lt;P&gt;Yes, we can use imx-mkimage, but where is the documenation what has to be done?&lt;/P&gt;&lt;P&gt;Is there already some documentation how the three parts must be combined?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 23 Nov 2023 09:09:17 GMT</pubDate>
    <dc:creator>Heiko_Patz</dc:creator>
    <dc:date>2023-11-23T09:09:17Z</dc:date>
    <item>
      <title>i.MX8MP - Boot via u-Boot - binary structure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Boot-via-u-Boot-binary-structure/m-p/1762557#M216254</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to understand how the resulting boot binary must be combined that the i.MX8MP will boot properly by u-Boot bootloader.&lt;/P&gt;&lt;P&gt;I found already some documentation which are addressing this topic (i.MX Linux User's Guide, AN1403: Fast Boot on i.MX8M and i.MX9 using Falcon Mode and Kernel Optimizations) but I did not find a documentation how the SPL+ATF+u-Boot must be fit together so that is will run.&lt;/P&gt;&lt;P&gt;Yes, we can use imx-mkimage, but where is the documenation what has to be done?&lt;/P&gt;&lt;P&gt;Is there already some documentation how the three parts must be combined?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 09:09:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Boot-via-u-Boot-binary-structure/m-p/1762557#M216254</guid>
      <dc:creator>Heiko_Patz</dc:creator>
      <dc:date>2023-11-23T09:09:17Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8MP - Boot via u-Boot - binary structure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Boot-via-u-Boot-binary-structure/m-p/1763079#M216313</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189084"&gt;@Heiko_Patz&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;As I know, there is no such documentation. Would suggest to refer to (&lt;A href="https://github.com/nxp-imx/imx-mkimage" target="_blank"&gt;GitHub - nxp-imx/imx-mkimage: i.MX Mkimage Bootloader Tool&lt;/A&gt;) to get more information.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 24 Nov 2023 05:53:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-Boot-via-u-Boot-binary-structure/m-p/1763079#M216313</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-11-24T05:53:42Z</dc:date>
    </item>
  </channel>
</rss>