<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX8 SPI chipselect stays active after transfer is complete</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-SPI-chipselect-stays-active-after-transfer-is-complete/m-p/1762174#M216220</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;This may be happening due to the module expect the TXFIFO to be filled to continue with the burst transfer.&lt;BR /&gt;&lt;BR /&gt;This is configured in the&amp;nbsp;ECSPIx_CONFIGREG(SS_CTL)[11-8], when set&amp;nbsp;In master mode - Negate Chip Select (SS) signal between SPI bursts. Multiple SPI bursts will be transmitted. The SPI transfer will automatically stop when the TXFIFO is empty.&lt;BR /&gt;&lt;BR /&gt;Please refer to the reference manual chapter&amp;nbsp;10.1.2.4.1.3 Master Mode with SS_CTL[3:0] Control.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Wed, 22 Nov 2023 20:20:01 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2023-11-22T20:20:01Z</dc:date>
    <item>
      <title>IMX8 SPI chipselect stays active after transfer is complete</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-SPI-chipselect-stays-active-after-transfer-is-complete/m-p/1758029#M215799</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am facing an unusual issue with chipselect on ecspi2 staying active for an extended period of time even after transaction is complete.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This issue occurs on ecspi2 SPI controller talking to MCP2515 SPI device.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="nc87_0-1700105001886.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/250082i89951C58A589E17D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="nc87_0-1700105001886.png" alt="nc87_0-1700105001886.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Here is my device tree&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&amp;amp;ecspi2 {&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;pinctrl-names = "default";&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;pinctrl-0 = &amp;lt;&amp;amp;pinctrl_ecspi2 &amp;amp;pinctrl_ecspi2_cs&amp;gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;cs-gpios = &amp;lt;&amp;amp;gpio5 20 GPIO_ACTIVE_LOW&amp;gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;fsl,spi-num-chipselects = &amp;lt;1&amp;gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;status = "okay";&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;can1: can@0 {&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;compatible = "microchip,mcp2515";&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;//gpio-controller;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;//#gpio-cells = &amp;lt;2&amp;gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;reg = &amp;lt;0&amp;gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;pinctrl-names = "default";&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;spi-max-frequency = &amp;lt;10000000&amp;gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;interrupt-parent = &amp;lt;&amp;amp;gpio5&amp;gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;interrupts = &amp;lt;21 IRQ_TYPE_LEVEL_LOW&amp;gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;clocks = &amp;lt;&amp;amp;can_osc_10m&amp;gt;;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;};&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;};&lt;/DIV&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any suggestions as to what might be going on?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank You,&lt;/P&gt;&lt;P&gt;Naveen&lt;/P&gt;</description>
      <pubDate>Thu, 16 Nov 2023 03:31:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-SPI-chipselect-stays-active-after-transfer-is-complete/m-p/1758029#M215799</guid>
      <dc:creator>nc87</dc:creator>
      <dc:date>2023-11-16T03:31:57Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8 SPI chipselect stays active after transfer is complete</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-SPI-chipselect-stays-active-after-transfer-is-complete/m-p/1760966#M216114</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Could you share the exact i.MX8 that you’re using for your test?&lt;BR /&gt;Also, which BSP version are you working with?&lt;BR /&gt;&lt;BR /&gt;Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Nov 2023 17:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-SPI-chipselect-stays-active-after-transfer-is-complete/m-p/1760966#M216114</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2023-11-21T17:35:19Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8 SPI chipselect stays active after transfer is complete</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-SPI-chipselect-stays-active-after-transfer-is-complete/m-p/1761089#M216119</link>
      <description>&lt;P&gt;Hi Aldo,&lt;/P&gt;&lt;P&gt;I am using IMX8MM with&amp;nbsp;&lt;SPAN&gt;BSP-Yocto-NXP-i.MX8MM-PD22.1.0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I&lt;SPAN&gt;&amp;nbsp;came across an interesting&amp;nbsp;observation - If I &lt;STRONG&gt;increase &lt;/STRONG&gt;the CPU load or even shut off couple of cores this issue almost disappears. But we do need to get the bottom of this. Any help will be appreciated.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank You,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Naveen&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Nov 2023 19:32:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-SPI-chipselect-stays-active-after-transfer-is-complete/m-p/1761089#M216119</guid>
      <dc:creator>nc87</dc:creator>
      <dc:date>2023-11-21T19:32:56Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8 SPI chipselect stays active after transfer is complete</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8-SPI-chipselect-stays-active-after-transfer-is-complete/m-p/1762174#M216220</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;This may be happening due to the module expect the TXFIFO to be filled to continue with the burst transfer.&lt;BR /&gt;&lt;BR /&gt;This is configured in the&amp;nbsp;ECSPIx_CONFIGREG(SS_CTL)[11-8], when set&amp;nbsp;In master mode - Negate Chip Select (SS) signal between SPI bursts. Multiple SPI bursts will be transmitted. The SPI transfer will automatically stop when the TXFIFO is empty.&lt;BR /&gt;&lt;BR /&gt;Please refer to the reference manual chapter&amp;nbsp;10.1.2.4.1.3 Master Mode with SS_CTL[3:0] Control.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 20:20:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8-SPI-chipselect-stays-active-after-transfer-is-complete/m-p/1762174#M216220</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2023-11-22T20:20:01Z</dc:date>
    </item>
  </channel>
</rss>