<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Wi-Fi Disconnection Issue During Bluetooth Device Scanning in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1762108#M216208</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Are you getting log errors when the issue occurs?&lt;/P&gt;
&lt;P&gt;I would recommend checking with Murata, since this could be an issue with the module and/or the firmware.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Wed, 22 Nov 2023 17:20:05 GMT</pubDate>
    <dc:creator>JorgeCas</dc:creator>
    <dc:date>2023-11-22T17:20:05Z</dc:date>
    <item>
      <title>Wi-Fi Disconnection Issue During Bluetooth Device Scanning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1759780#M215981</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm currently using an imx6ull board and have Ubuntu 20.04.6 installed on my PC. I'm attempting to access the board via SSH over Wi-Fi. Initially, I can successfully connect to the board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, I encounter an issue when running the "bluetoothctl" command. Specifically, after executing "scan on," the tool scans for nearby Bluetooth devices for the first 3-5 seconds. Following this initial period, there is a brief pause, and subsequently, the Wi-Fi connection disconnects.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;both of which use the same 2.4GHz chip and antenna.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm seeking assistance in identifying the root cause of this problem and any potential solutions to overcome this issue. Any insights or recommendations would be greatly appreciated.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Akash&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 11:02:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1759780#M215981</guid>
      <dc:creator>akash_akash</dc:creator>
      <dc:date>2023-11-20T11:02:12Z</dc:date>
    </item>
    <item>
      <title>Re: Wi-Fi Disconnection Issue During Bluetooth Device Scanning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1759995#M216013</link>
      <description>&lt;P&gt;Hello, I hope you are doing well.&lt;/P&gt;
&lt;P&gt;Could you please share me more about your hardware setup? Such as board used, Wi-Fi module used, software versions, modifications, etc.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 17:57:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1759995#M216013</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2023-11-20T17:57:01Z</dc:date>
    </item>
    <item>
      <title>Re: Wi-Fi Disconnection Issue During Bluetooth Device Scanning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1760487#M216069</link>
      <description>&lt;P&gt;&lt;BR /&gt;Hello [NXP Team],&lt;/P&gt;&lt;P&gt;I hope this message finds you well. We're currently utilizing the RTC PCF85263A with an iMX6ULL processor, running Linux 5.15 on Yocto 4.0. Additionally, we've integrated the Murata LBEE5HY1MW-518 Wi-Fi and Bluetooth module into our system.&lt;/P&gt;&lt;P&gt;One of our clients is facing a peculiar issue. When attempting SSH connection to the board through Wi-Fi (host mode) and initiating a Bluetooth scan using "bluetoothctl" with "scan on," the Wi-Fi connection drops approximately 5 seconds later. Both Wi-Fi and Bluetooth operate in the 2.4GHz frequency range.&lt;/P&gt;&lt;P&gt;Changing the Wi-Fi configuration to 5GHz resolves the disconnection problem, but our client insists on 2.4GHz usage.&lt;/P&gt;&lt;P&gt;We would greatly appreciate your insights and suggestions on resolving this connectivity issue. If there are specific configurations or optimizations that can be applied to ensure stable coexistence of Wi-Fi and Bluetooth in the 2.4GHz range, please guide us accordingly.&lt;/P&gt;&lt;P&gt;Thank you for your time and assistance.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Akash&lt;/P&gt;</description>
      <pubDate>Tue, 21 Nov 2023 07:25:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1760487#M216069</guid>
      <dc:creator>akash_akash</dc:creator>
      <dc:date>2023-11-21T07:25:05Z</dc:date>
    </item>
    <item>
      <title>Re: Wi-Fi Disconnection Issue During Bluetooth Device Scanning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1760805#M216096</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;
&lt;P&gt;Got it, thank you for the information.&lt;/P&gt;
&lt;P&gt;Which driver are you using on the Wi-Fi/Bluetooth module?&lt;/P&gt;
&lt;P&gt;This issue has not been reported on our side with tested modules.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Nov 2023 13:39:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1760805#M216096</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2023-11-21T13:39:48Z</dc:date>
    </item>
    <item>
      <title>Re: Wi-Fi Disconnection Issue During Bluetooth Device Scanning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1761555#M216142</link>
      <description>&lt;P&gt;Hello [NXP Team],&lt;/P&gt;&lt;P&gt;For the Bluetooth and Wi-Fi module, we are using the &lt;EM&gt;&lt;STRONG&gt;brcmfmac&lt;/STRONG&gt;&lt;/EM&gt; device driver.&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Akash&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 04:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1761555#M216142</guid>
      <dc:creator>akash_akash</dc:creator>
      <dc:date>2023-11-22T04:50:04Z</dc:date>
    </item>
    <item>
      <title>Re: Wi-Fi Disconnection Issue During Bluetooth Device Scanning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1762108#M216208</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Are you getting log errors when the issue occurs?&lt;/P&gt;
&lt;P&gt;I would recommend checking with Murata, since this could be an issue with the module and/or the firmware.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 17:20:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1762108#M216208</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2023-11-22T17:20:05Z</dc:date>
    </item>
    <item>
      <title>Re: Wi-Fi Disconnection Issue During Bluetooth Device Scanning</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1763044#M216306</link>
      <description>&lt;P&gt;Hello [NXP Team],&lt;/P&gt;&lt;P&gt;No, we don't get any log errors ,It just disconnect the Wi-Fi from the connected devices but the WiFi is sill on and we can't able to connect the network until we give &lt;EM&gt;&lt;STRONG&gt;scan off&lt;/STRONG&gt;&lt;/EM&gt; command.&lt;/P&gt;&lt;P&gt;Thank you for your support and valuable information.&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Akash&lt;/P&gt;</description>
      <pubDate>Fri, 24 Nov 2023 05:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Wi-Fi-Disconnection-Issue-During-Bluetooth-Device-Scanning/m-p/1763044#M216306</guid>
      <dc:creator>AkashL_</dc:creator>
      <dc:date>2023-11-24T05:46:30Z</dc:date>
    </item>
  </channel>
</rss>