<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Readingkernel space  memory using the UIO driver in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Readingkernel-space-memory-using-the-UIO-driver/m-p/1761994#M216194</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on communicaiton between the MPU and MCU of the IMX8MP and I want to send data to the MPU from the MCU and the read this data from the user space using the UIO driver.&lt;/P&gt;&lt;P&gt;I tried creating a node in the device tree but the node is not listed in the&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; /sys/class/uio/&lt;/P&gt;&lt;P&gt;The device tree entry is below&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; shared_memory@55000000{&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; compatible = "generic-uio";&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; status = "okay";&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; reg = &amp;lt; 0x55000000 0x8000 &amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; interrupts = &amp;lt; 0 88 0 &amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; interrupt-parent = &amp;lt;&amp;amp;gic&amp;gt;;&lt;/P&gt;&lt;P&gt;What have I left undone or is there an example for this?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 22 Nov 2023 14:35:19 GMT</pubDate>
    <dc:creator>ababatola</dc:creator>
    <dc:date>2023-11-22T14:35:19Z</dc:date>
    <item>
      <title>Readingkernel space  memory using the UIO driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Readingkernel-space-memory-using-the-UIO-driver/m-p/1761994#M216194</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on communicaiton between the MPU and MCU of the IMX8MP and I want to send data to the MPU from the MCU and the read this data from the user space using the UIO driver.&lt;/P&gt;&lt;P&gt;I tried creating a node in the device tree but the node is not listed in the&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; /sys/class/uio/&lt;/P&gt;&lt;P&gt;The device tree entry is below&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; shared_memory@55000000{&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; compatible = "generic-uio";&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; status = "okay";&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; reg = &amp;lt; 0x55000000 0x8000 &amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; interrupts = &amp;lt; 0 88 0 &amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; interrupt-parent = &amp;lt;&amp;amp;gic&amp;gt;;&lt;/P&gt;&lt;P&gt;What have I left undone or is there an example for this?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 14:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Readingkernel-space-memory-using-the-UIO-driver/m-p/1761994#M216194</guid>
      <dc:creator>ababatola</dc:creator>
      <dc:date>2023-11-22T14:35:19Z</dc:date>
    </item>
    <item>
      <title>Re: Readingkernel space  memory using the UIO driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Readingkernel-space-memory-using-the-UIO-driver/m-p/1762805#M216283</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For MCU you refer to an external MCU? because the MX8MP has the M7 inside.&lt;/P&gt;
&lt;P&gt;It depend how to connect your MCU is it from SPI or UART but example are in the device tree of the Linux BSP.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 14:57:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Readingkernel-space-memory-using-the-UIO-driver/m-p/1762805#M216283</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2023-11-23T14:57:41Z</dc:date>
    </item>
    <item>
      <title>Re: Readingkernel space  memory using the UIO driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Readingkernel-space-memory-using-the-UIO-driver/m-p/1767028#M216685</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The MCU and the MPU refers to the core M7 in and the A53 processor in the IMX8MP.&lt;/P&gt;&lt;P&gt;I want to write a user space application that would access the shared memory using the userspace I/O.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 01 Dec 2023 07:24:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Readingkernel-space-memory-using-the-UIO-driver/m-p/1767028#M216685</guid>
      <dc:creator>ababatola</dc:creator>
      <dc:date>2023-12-01T07:24:15Z</dc:date>
    </item>
  </channel>
</rss>