<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx8mp basler add data type</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-basler-add-data-type/m-p/1761652#M216155</link>
    <description>&lt;P&gt;Do you have any suggestions for modifying the OS08a20 driver if I want to perform ISP processing on grayscale images&lt;/P&gt;</description>
    <pubDate>Wed, 22 Nov 2023 07:14:02 GMT</pubDate>
    <dc:creator>lei11</dc:creator>
    <dc:date>2023-11-22T07:14:02Z</dc:date>
    <item>
      <title>imx8mp basler add data type</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-basler-add-data-type/m-p/1757359#M215742</link>
      <description>&lt;P&gt;您好，我正在使用imx8mp的basler模组的驱动，我使用v4l2-ctl --device=/dev/video2 --list-formats-ext获取了它目前支持的数据格式，我想添加一种GREY格式的数据捕获，我该怎么做，我该修改怎么文件，我在basler-camera-driver-vvcam.c文件中没看见看见相关的设置data type的地方&lt;/P&gt;&lt;P&gt;v4l2-ctl --device=/dev/video2 --list-formats-ext&lt;BR /&gt;ioctl: VIDIOC_ENUM_FMT&lt;BR /&gt;Type: Video Capture&lt;/P&gt;&lt;P&gt;[0]: 'YUYV' (YUYV 4:2:2)&lt;BR /&gt;Size: Stepwise 176x144 - 4096x3072 with step 16/8&lt;BR /&gt;[1]: 'NV12' (Y/UV 4:2:0)&lt;BR /&gt;Size: Stepwise 176x144 - 4096x3072 with step 16/8&lt;BR /&gt;[2]: 'NV16' (Y/UV 4:2:2)&lt;BR /&gt;Size: Stepwise 176x144 - 4096x3072 with step 16/8&lt;BR /&gt;[3]: 'BA12' (12-bit Bayer GRGR/BGBG)&lt;BR /&gt;Size: Stepwise 176x144 - 4096x3072 with step 16/8&lt;/P&gt;</description>
      <pubDate>Wed, 15 Nov 2023 06:50:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-basler-add-data-type/m-p/1757359#M215742</guid>
      <dc:creator>lei11</dc:creator>
      <dc:date>2023-11-15T06:50:24Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp basler add data type</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-basler-add-data-type/m-p/1759532#M215937</link>
      <description>&lt;P&gt;for basler, they are not open to customers&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 04:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-basler-add-data-type/m-p/1759532#M215937</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-11-20T04:33:14Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp basler add data type</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-basler-add-data-type/m-p/1761375#M216127</link>
      <description>&lt;P&gt;&amp;nbsp;So if I modify the driver of OS08a20, can I add formatting normally&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 01:25:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-basler-add-data-type/m-p/1761375#M216127</guid>
      <dc:creator>lei11</dc:creator>
      <dc:date>2023-11-22T01:25:37Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp basler add data type</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-basler-add-data-type/m-p/1761652#M216155</link>
      <description>&lt;P&gt;Do you have any suggestions for modifying the OS08a20 driver if I want to perform ISP processing on grayscale images&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 07:14:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-basler-add-data-type/m-p/1761652#M216155</guid>
      <dc:creator>lei11</dc:creator>
      <dc:date>2023-11-22T07:14:02Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp basler add data type</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-basler-add-data-type/m-p/1762417#M216240</link>
      <description>&lt;P&gt;you need check the os08a20 data sheet, to check the register to control this, then set this register in the driver, you need contact os08a20 vendor&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 07:12:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-basler-add-data-type/m-p/1762417#M216240</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-11-23T07:12:25Z</dc:date>
    </item>
  </channel>
</rss>