<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx8mm 1GB RAM issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-1GB-RAM-issue/m-p/1760037#M216016</link>
    <description>&lt;P&gt;I had similar issues a while back and switching to the newest RPA spreadsheet seemed to fix it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Latest LPDDR4 RPA version is '22'&amp;nbsp; It can be downloaded here&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MMini-m845S-DDR-Register-Programming-Aid-RPA/ta-p/1172443" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MMini-m845S-DDR-Register-Programming-Aid-RPA/ta-p/1172443&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Don&lt;/P&gt;</description>
    <pubDate>Mon, 20 Nov 2023 19:22:37 GMT</pubDate>
    <dc:creator>don_gunn</dc:creator>
    <dc:date>2023-11-20T19:22:37Z</dc:date>
    <item>
      <title>imx8mm 1GB RAM issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-1GB-RAM-issue/m-p/1753477#M215367</link>
      <description>&lt;P&gt;Hi.&lt;BR /&gt;Need help with configuration.&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2023-11-06 183013.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/248658iA545E75A862BB415/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot 2023-11-06 183013.png" alt="Screenshot 2023-11-06 183013.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot 2023-11-06 183013.png&lt;/span&gt;&lt;/span&gt;This is schematic of custom MPU module. This works with 2GB RAM but training if 1GB(PN: &lt;A href="https://media-www.micron.com/-/media/client/global/documents/products/data-sheet/dram/mobile-dram/low-power-dram/lpddr4/200b_z11m_non_auto_lpddr4_lpddr4x.pdf?rev=385d650bf2844e6a94546e9d2dc72c31" target="_self"&gt;MT53D512M16D1DS&lt;/A&gt;) fails:&lt;/P&gt;&lt;P&gt;Downloading file 'bin\lpddr4_train1d_string_v201709.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\lpddr4_train2d_string_v201709.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\lpddr4_imem_1d_v201709.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\lpddr4_dmem_1d_v201709.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\lpddr4_imem_2d_v201709.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading file 'bin\lpddr4_dmem_2d_v201709.bin' ..Done&lt;/P&gt;&lt;P&gt;Downloading IVT header...Done&lt;BR /&gt;Downloading file 'bin\m845s_ddr_stress_test.bin' ...Done&lt;/P&gt;&lt;P&gt;Download is complete&lt;BR /&gt;Waiting for the target board boot...&lt;/P&gt;&lt;P&gt;===================hardware_init=====================&lt;/P&gt;&lt;P&gt;********Found PMIC BD718XX**********&lt;BR /&gt;hardware_init exit&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;MX8 DDR Stress Test V3.30&lt;BR /&gt;Built on Nov 24 2021 13:30:14&lt;BR /&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;Waiting for board configuration from PC-end...&lt;/P&gt;&lt;P&gt;--Set up the MMU and enable I and D cache--&lt;BR /&gt;- This is the Cortex-A53 core&lt;BR /&gt;- Check if I cache is enabled&lt;BR /&gt;- Enabling I cache since it was disabled&lt;BR /&gt;- Push base address of TTB to TTBR0_EL3&lt;BR /&gt;- Config TCR_EL3&lt;BR /&gt;- Config MAIR_EL3&lt;BR /&gt;- Enable MMU&lt;BR /&gt;- Data Cache has been enabled&lt;BR /&gt;- Check system memory register, only for debug&lt;/P&gt;&lt;P&gt;- VMCR Check:&lt;BR /&gt;- ttbr0_el3: 0x93d000&lt;BR /&gt;- tcr_el3: 0x2051c&lt;BR /&gt;- mair_el3: 0x774400&lt;BR /&gt;- sctlr_el3: 0xc01815&lt;BR /&gt;- id_aa64mmfr0_el1: 0x1122&lt;/P&gt;&lt;P&gt;- MMU and cache setup complete&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;BR /&gt;ARM clock(CA53) rate: 1800MHz&lt;BR /&gt;DDR Clock: 1500MHz&lt;/P&gt;&lt;P&gt;============================================&lt;BR /&gt;DDR configuration&lt;BR /&gt;DDR type is LPDDR4&lt;BR /&gt;Data width: 16, bank num: 8&lt;BR /&gt;Row size: 16, col size: 10&lt;BR /&gt;One chip select is used&lt;BR /&gt;Number of DDR controllers used on the SoC: 1&lt;BR /&gt;Density per chip select: 1024MB&lt;BR /&gt;Density per controller is: 1024MB&lt;BR /&gt;Total density detected on the board is: 1024MB&lt;BR /&gt;============================================&lt;/P&gt;&lt;P&gt;MX8M-mini: Cortex-A53 is found&lt;/P&gt;&lt;P&gt;*************************************************************************&lt;/P&gt;&lt;P&gt;============ Step 1: DDRPHY Training... ============&lt;BR /&gt;---DDR 1D-Training @1500Mhz...&lt;BR /&gt;PMU10: **** Start LPDDR4 Training. PMU Firmware Revision 0x1000 ****&lt;BR /&gt;PMU10: Setting boot clock divider to 28&lt;BR /&gt;PMU10: PHY TOTALS - NUM_DBYTES 2 NUM_NIBBLES 4 NUM_ANIBS 10&lt;BR /&gt;PMU10: CSA=0x01, CSB=0x00, TSTAGES=0x131F, HDTOUT=5, MMISC=0 DRAMFreq=3000MT DramType=LPDDR4&lt;BR /&gt;PMU10: Pstate0 MRS MR1_A0=0x00D4 MR2_A0=0x002D MR3_A0=0x0031 MR4_A0=0x0000&lt;BR /&gt;PMU5: CA bitmap dump for cs 0&lt;BR /&gt;PMU5: CAA0 ffffffffffffffffffffffffffffffffffffffffffffffff&lt;BR /&gt;PMU5: CAA1 ffffffffffffffffffffffffffffffffffffffffffffffff&lt;BR /&gt;PMU5: CAA2 ffffffffffffffffffffffffffffffffffffffffffffffff&lt;BR /&gt;PMU5: CAA3 ffffffffffffffffffffffffffffffffffffffffffffffff&lt;BR /&gt;PMU5: CAA4 ffffffffffffffffffffffffffffffffffffffffffffffff&lt;BR /&gt;PMU5: CAA5 ffffffffffffffffffffffffffffffffffffffffffffffff&lt;BR /&gt;PMU: Error: CA Training Failed.&lt;BR /&gt;PMU: ***** Assertion Error - terminating *****&lt;BR /&gt;[Result] FAILED&lt;/P&gt;&lt;P&gt;It tries to refer to Bank A(connected to LPDDR4 bank B) but it is not present.&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="2.png" style="width: 640px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/248808i090E46F43FC2B252/image-size/large?v=v2&amp;amp;px=999" role="button" title="2.png" alt="2.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;2.png&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;RPA config:&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2023-11-07 13-39-08.png" style="width: 468px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/248809iB8F638DE5863733F/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2023-11-07 13-39-08.png" alt="Screenshot from 2023-11-07 13-39-08.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot from 2023-11-07 13-39-08.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Nov 2023 11:41:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-1GB-RAM-issue/m-p/1753477#M215367</guid>
      <dc:creator>AmiraniTurmanidze</dc:creator>
      <dc:date>2023-11-07T11:41:12Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mm 1GB RAM issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mm-1GB-RAM-issue/m-p/1760037#M216016</link>
      <description>&lt;P&gt;I had similar issues a while back and switching to the newest RPA spreadsheet seemed to fix it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Latest LPDDR4 RPA version is '22'&amp;nbsp; It can be downloaded here&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MMini-m845S-DDR-Register-Programming-Aid-RPA/ta-p/1172443" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MMini-m845S-DDR-Register-Programming-Aid-RPA/ta-p/1172443&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Don&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 19:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mm-1GB-RAM-issue/m-p/1760037#M216016</guid>
      <dc:creator>don_gunn</dc:creator>
      <dc:date>2023-11-20T19:22:37Z</dc:date>
    </item>
  </channel>
</rss>