<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Linux kernel debugging on i.MX8 Quad Max MEK board using Lauterbach</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Linux-kernel-debugging-on-i-MX8-Quad-Max-MEK-board-using/m-p/1759531#M215936</link>
    <description>&lt;P&gt;pls refer to the enclosed file and check if your debug steps are correct or not&lt;/P&gt;</description>
    <pubDate>Mon, 20 Nov 2023 04:32:04 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2023-11-20T04:32:04Z</dc:date>
    <item>
      <title>Linux kernel debugging on i.MX8 Quad Max MEK board using Lauterbach</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-kernel-debugging-on-i-MX8-Quad-Max-MEK-board-using/m-p/1757444#M215749</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;&lt;BR /&gt;I am trying to debug Linux kernel on IMX8QaudMax MEK board. I built image using Yocto Project. I am using Kirkstone 5.15. I have configured kernel to enable debug symbols (works fine with simulator, but I can only load vmlinux to simulator since I don't have license for simulator). I connected Lauterbach to JTAG connector over JTAG- GEN2 Adapter Card that came with my board. I am using ARMv8-A/R probe.&lt;BR /&gt;&lt;BR /&gt;The problem happens when I try to attach. Board just reboots and I get next warning:&lt;BR /&gt;&lt;STRONG&gt;&lt;SPAN class=""&gt;Warning: CO:0 Erros occurred during initialization of master core, error=0x8c &lt;/SPAN&gt;&lt;/STRONG&gt;&lt;SPAN class=""&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;I tried to attach to the board when board is set to boot from SD card, but SD card is not inserted. I would expect to get bus error, but I am getting this same warning...&lt;BR /&gt;I have also custom board that uses imx8qm and I can use same image, and on custom board I am able to debug, everything works fine.&lt;BR /&gt;&lt;BR /&gt;My question is, should I apply some HW patch to IMX8QuadMax MEK board to enable debugging using JTAG? I have two MEK boards and I have same behavior with both boards...&lt;BR /&gt;I really have never seen this warning. Does anyone have any hints? Thanks!&lt;BR /&gt;Best regards,&lt;BR /&gt;Vanja&lt;/P&gt;</description>
      <pubDate>Wed, 15 Nov 2023 08:12:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-kernel-debugging-on-i-MX8-Quad-Max-MEK-board-using/m-p/1757444#M215749</guid>
      <dc:creator>vzeric</dc:creator>
      <dc:date>2023-11-15T08:12:55Z</dc:date>
    </item>
    <item>
      <title>Re: Linux kernel debugging on i.MX8 Quad Max MEK board using Lauterbach</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-kernel-debugging-on-i-MX8-Quad-Max-MEK-board-using/m-p/1759531#M215936</link>
      <description>&lt;P&gt;pls refer to the enclosed file and check if your debug steps are correct or not&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 04:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-kernel-debugging-on-i-MX8-Quad-Max-MEK-board-using/m-p/1759531#M215936</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-11-20T04:32:04Z</dc:date>
    </item>
    <item>
      <title>Re: Linux kernel debugging on i.MX8 Quad Max MEK board using Lauterbach</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Linux-kernel-debugging-on-i-MX8-Quad-Max-MEK-board-using/m-p/1763094#M216315</link>
      <description>&lt;P&gt;I followed all steps from document you sent me and still I have same issue. But I made some progress with updating Trace32 to last supported version for my license. Warning disappeared.&lt;BR /&gt;Anyway thank you, I appreciate your help, this document is really helpful!&lt;BR /&gt;Best regards,&lt;BR /&gt;Vanja&lt;/P&gt;</description>
      <pubDate>Fri, 24 Nov 2023 06:15:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Linux-kernel-debugging-on-i-MX8-Quad-Max-MEK-board-using/m-p/1763094#M216315</guid>
      <dc:creator>vzeric</dc:creator>
      <dc:date>2023-11-24T06:15:55Z</dc:date>
    </item>
  </channel>
</rss>