<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Cannot write custom android image to PICO-PI-NXP7D (ex-AndroidThings) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-write-custom-android-image-to-PICO-PI-NXP7D-ex/m-p/1758599#M215844</link>
    <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I'm trying to create a Android 9 custom build following the instructions from &lt;A href="https://developer.technexion.com/docs/android-pie-arm32-setup-build-and-flashing" target="_blank" rel="noopener"&gt;Technexion website&lt;/A&gt;&amp;nbsp;. Any prebuilt image from NXP or Technexion is flashed without problems, but I cannot install my own image, although it compiles without errors.&lt;/P&gt;&lt;P&gt;After executing the command&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;./uuu/linux64/uuu -b emmc_imx7_img imx7/pico-imx7/imx7-SPL imx7/pico-imx7/imx7-u-boot.img test.img&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;the image is flashed without errors, but after running I see in the console following:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;RNG instantiation done (3600)&lt;BR /&gt;avb_slot_verify.c:388: ERROR: boot: Hash of data does not match digest in descriptor.&lt;BR /&gt;verify FAIL, state:&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;and nothing else happens&lt;/P&gt;&lt;P&gt;What could be the problem? Will be glad for any help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 16 Nov 2023 20:18:11 GMT</pubDate>
    <dc:creator>KaBoom</dc:creator>
    <dc:date>2023-11-16T20:18:11Z</dc:date>
    <item>
      <title>Cannot write custom android image to PICO-PI-NXP7D (ex-AndroidThings)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-write-custom-android-image-to-PICO-PI-NXP7D-ex/m-p/1758599#M215844</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I'm trying to create a Android 9 custom build following the instructions from &lt;A href="https://developer.technexion.com/docs/android-pie-arm32-setup-build-and-flashing" target="_blank" rel="noopener"&gt;Technexion website&lt;/A&gt;&amp;nbsp;. Any prebuilt image from NXP or Technexion is flashed without problems, but I cannot install my own image, although it compiles without errors.&lt;/P&gt;&lt;P&gt;After executing the command&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;./uuu/linux64/uuu -b emmc_imx7_img imx7/pico-imx7/imx7-SPL imx7/pico-imx7/imx7-u-boot.img test.img&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;the image is flashed without errors, but after running I see in the console following:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;RNG instantiation done (3600)&lt;BR /&gt;avb_slot_verify.c:388: ERROR: boot: Hash of data does not match digest in descriptor.&lt;BR /&gt;verify FAIL, state:&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;and nothing else happens&lt;/P&gt;&lt;P&gt;What could be the problem? Will be glad for any help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Nov 2023 20:18:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-write-custom-android-image-to-PICO-PI-NXP7D-ex/m-p/1758599#M215844</guid>
      <dc:creator>KaBoom</dc:creator>
      <dc:date>2023-11-16T20:18:11Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot write custom android image to PICO-PI-NXP7D (ex-AndroidThings)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-write-custom-android-image-to-PICO-PI-NXP7D-ex/m-p/1759274#M215910</link>
      <description>&lt;P&gt;I'd suggest you to raise the problem to Technexion.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Sat, 18 Nov 2023 04:17:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-write-custom-android-image-to-PICO-PI-NXP7D-ex/m-p/1759274#M215910</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-11-18T04:17:12Z</dc:date>
    </item>
  </channel>
</rss>