<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic UCM-iMX8M-Mini MIPI DSI interface in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UCM-iMX8M-Mini-MIPI-DSI-interface/m-p/1742061#M215768</link>
    <description>&lt;P&gt;Good day,&lt;/P&gt;&lt;P&gt;I am using the iMX8M on the UCM-iMX8M-Mini board and its Evaluation Kit from Compulab, with the LCD that it comes with plugged into the MIPI DSI interface.&lt;/P&gt;&lt;P&gt;Issue #1: At power-up, I can see activity on the MIPI DSI bus (DSI CLK and DSI data lane D0) when probing it with a scope. It is strange though that the waveforms I see on the scope are not in accordance with the LCD controller data sheet or the MIPI spec.&lt;/P&gt;&lt;P&gt;Issue #2:&amp;nbsp;When I remove the LCD and connect the Evaluation Kit's MIPI DSI interface to my own custom hardware, the DSI stops working. There must therefore be some sort of start-up handshaking that takes place between the LCD controller and the iMX8. I am trying to figure out which device says what?&lt;/P&gt;&lt;P&gt;I need to know what default start-up transaction is happening so that I can either change the driver/s to just get the DSI high-speed data (which is the only thing I am really interested in for this application), or&amp;nbsp; design my custom hardware to look like the LCD controller.&lt;/P&gt;&lt;P&gt;Any input on these issues would be greatly appreciated!&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Giovanni&lt;/P&gt;</description>
    <pubDate>Wed, 18 Oct 2023 11:31:42 GMT</pubDate>
    <dc:creator>Giovanni1</dc:creator>
    <dc:date>2023-10-18T11:31:42Z</dc:date>
    <item>
      <title>UCM-iMX8M-Mini MIPI DSI interface</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UCM-iMX8M-Mini-MIPI-DSI-interface/m-p/1742061#M215768</link>
      <description>&lt;P&gt;Good day,&lt;/P&gt;&lt;P&gt;I am using the iMX8M on the UCM-iMX8M-Mini board and its Evaluation Kit from Compulab, with the LCD that it comes with plugged into the MIPI DSI interface.&lt;/P&gt;&lt;P&gt;Issue #1: At power-up, I can see activity on the MIPI DSI bus (DSI CLK and DSI data lane D0) when probing it with a scope. It is strange though that the waveforms I see on the scope are not in accordance with the LCD controller data sheet or the MIPI spec.&lt;/P&gt;&lt;P&gt;Issue #2:&amp;nbsp;When I remove the LCD and connect the Evaluation Kit's MIPI DSI interface to my own custom hardware, the DSI stops working. There must therefore be some sort of start-up handshaking that takes place between the LCD controller and the iMX8. I am trying to figure out which device says what?&lt;/P&gt;&lt;P&gt;I need to know what default start-up transaction is happening so that I can either change the driver/s to just get the DSI high-speed data (which is the only thing I am really interested in for this application), or&amp;nbsp; design my custom hardware to look like the LCD controller.&lt;/P&gt;&lt;P&gt;Any input on these issues would be greatly appreciated!&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Giovanni&lt;/P&gt;</description>
      <pubDate>Wed, 18 Oct 2023 11:31:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UCM-iMX8M-Mini-MIPI-DSI-interface/m-p/1742061#M215768</guid>
      <dc:creator>Giovanni1</dc:creator>
      <dc:date>2023-10-18T11:31:42Z</dc:date>
    </item>
  </channel>
</rss>