<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Recovery/Redundant boot and HAB in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Recovery-Redundant-boot-and-HAB/m-p/1757332#M215740</link>
    <description>&lt;P&gt;If I've understood the reference manual (IMX8MMRM) correctly, SPI NOR recovery boot only kicks in if the SoC can't find a valid IVT on the selected boot device. If HAB verification fails however, PERSIST_SECONDARY_BOOT is set, and upon reset the SoC will try to find a secondary boot image on the same boot device.&lt;/P&gt;&lt;P&gt;Is there a way to have the SoC go into SPI NOR recovery boot upon HAB failure, or do we have to implement both recovery boot and redundant boot to be able to rescue our device in all cases?&lt;/P&gt;</description>
    <pubDate>Wed, 15 Nov 2023 06:29:14 GMT</pubDate>
    <dc:creator>maffan</dc:creator>
    <dc:date>2023-11-15T06:29:14Z</dc:date>
    <item>
      <title>Recovery/Redundant boot and HAB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Recovery-Redundant-boot-and-HAB/m-p/1757332#M215740</link>
      <description>&lt;P&gt;If I've understood the reference manual (IMX8MMRM) correctly, SPI NOR recovery boot only kicks in if the SoC can't find a valid IVT on the selected boot device. If HAB verification fails however, PERSIST_SECONDARY_BOOT is set, and upon reset the SoC will try to find a secondary boot image on the same boot device.&lt;/P&gt;&lt;P&gt;Is there a way to have the SoC go into SPI NOR recovery boot upon HAB failure, or do we have to implement both recovery boot and redundant boot to be able to rescue our device in all cases?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Nov 2023 06:29:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Recovery-Redundant-boot-and-HAB/m-p/1757332#M215740</guid>
      <dc:creator>maffan</dc:creator>
      <dc:date>2023-11-15T06:29:14Z</dc:date>
    </item>
    <item>
      <title>Re: Recovery/Redundant boot and HAB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Recovery-Redundant-boot-and-HAB/m-p/1758945#M215874</link>
      <description>&lt;P&gt;&lt;SPAN&gt;SoC can go into SPI NOR recovery boot before SDP upon HAB failure if SPI NOR set.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Nov 2023 09:04:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Recovery-Redundant-boot-and-HAB/m-p/1758945#M215874</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-11-17T09:04:58Z</dc:date>
    </item>
    <item>
      <title>Re: Recovery/Redundant boot and HAB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Recovery-Redundant-boot-and-HAB/m-p/1759080#M215891</link>
      <description>&lt;P&gt;Thanks for your response &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/192970"&gt;@Harvey021&lt;/a&gt;&amp;nbsp;!&lt;/P&gt;&lt;P&gt;What do you mean with "&lt;SPAN&gt;if SPI NOR set"? Do you mean the "Recovery boot enable" eFUSE, or the "Boot device selection" BOOT_CFG eFUSEs, or something else?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;</description>
      <pubDate>Fri, 17 Nov 2023 14:22:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Recovery-Redundant-boot-and-HAB/m-p/1759080#M215891</guid>
      <dc:creator>maffan</dc:creator>
      <dc:date>2023-11-17T14:22:54Z</dc:date>
    </item>
    <item>
      <title>Re: Recovery/Redundant boot and HAB</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Recovery-Redundant-boot-and-HAB/m-p/1759644#M215965</link>
      <description>&lt;P&gt;&lt;SPAN class="jCAhz ChMk0b"&gt;&lt;SPAN class="ryNqvb"&gt;sorry for the "&lt;SPAN&gt;if SPI NOR set&lt;/SPAN&gt;", by default, SPI NOR should be used as a recovery boot device, if the correct image is in it.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class="jCAhz ChMk0b"&gt;&lt;SPAN class="ryNqvb"&gt;It will not enter download mode.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="jCAhz ChMk0b"&gt;&lt;SPAN class="ryNqvb"&gt;Regards&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="jCAhz ChMk0b"&gt;&lt;SPAN class="ryNqvb"&gt;Harvey&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 07:37:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Recovery-Redundant-boot-and-HAB/m-p/1759644#M215965</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-11-20T07:37:38Z</dc:date>
    </item>
  </channel>
</rss>