<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: About IMX8MP TMDS voltage level</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-IMX8MP-TMDS-voltage-level/m-p/1755225#M215530</link>
    <description>&lt;P&gt;Thank you for your support in this matter.&lt;BR /&gt;I will try using the information you provided.&lt;/P&gt;&lt;P&gt;Thank you.&lt;BR /&gt;yoshihara&lt;/P&gt;</description>
    <pubDate>Fri, 10 Nov 2023 00:34:41 GMT</pubDate>
    <dc:creator>Yoshiharaaa</dc:creator>
    <dc:date>2023-11-10T00:34:41Z</dc:date>
    <item>
      <title>About IMX8MP TMDS voltage level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-IMX8MP-TMDS-voltage-level/m-p/1751740#M215196</link>
      <description>&lt;P&gt;I used a device with IMX8MP and took the certification test for HDMI 1.4b Source device.&lt;BR /&gt;However, the TMDS-VL item resulted in a FAIL determination.&lt;/P&gt;&lt;P&gt;&amp;gt;The FAIL items are as follows&lt;BR /&gt;ID7-2: TMDS-VL&lt;BR /&gt;　VL (L side voltage) of TMDS (D0+/-,D1+/-,D2+/-,DCLK+/-) is lower than the specified value.&lt;BR /&gt;　　Measured value VL=2.575～2.618V&lt;BR /&gt;　　Acceptable range VL=2.700V to 2.900V (max. 0.125V short)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Yoshiharaaa_0-1698998107690.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/248326iE4E321B60DF9B509/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Yoshiharaaa_0-1698998107690.png" alt="Yoshiharaaa_0-1698998107690.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Yoshiharaaa_0-1698998107690.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Since low L-side voltage = large amplitude, we are considering measures to reduce the amplitude itself.&lt;/P&gt;&lt;P&gt;&amp;lt;Questions&lt;BR /&gt;1) Is it possible to change the drive strength of the TMDS line?&lt;BR /&gt;　&lt;BR /&gt;2) The TMDS line is directly connected to a connector from the CPU, with a common mode coil and ESD suppressor in between.&lt;BR /&gt;The EVK sample board has almost the same configuration. Can we expect any effect on the voltage values (amplitude) by changing the DCR value, etc.?&lt;/P&gt;&lt;P&gt;Please let me know how to solve this problem.&lt;/P&gt;&lt;P&gt;Thank you.&lt;BR /&gt;Yoshihara&lt;/P&gt;</description>
      <pubDate>Fri, 03 Nov 2023 07:59:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-IMX8MP-TMDS-voltage-level/m-p/1751740#M215196</guid>
      <dc:creator>Yoshiharaaa</dc:creator>
      <dc:date>2023-11-03T07:59:51Z</dc:date>
    </item>
    <item>
      <title>Re: About IMX8MP TMDS voltage level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-IMX8MP-TMDS-voltage-level/m-p/1751928#M215215</link>
      <description>&lt;P&gt;please try below tuning which has been implemented in latest BSP:&lt;/P&gt;
&lt;P&gt;/unit_tests/memtool -32 0x32fdff5c=0x32&lt;/P&gt;
&lt;P&gt;/unit_tests/memtool -32 0x32fdff60=0x60&lt;/P&gt;</description>
      <pubDate>Fri, 03 Nov 2023 11:33:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-IMX8MP-TMDS-voltage-level/m-p/1751928#M215215</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-11-03T11:33:15Z</dc:date>
    </item>
    <item>
      <title>Re: About IMX8MP TMDS voltage level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-IMX8MP-TMDS-voltage-level/m-p/1753207#M215337</link>
      <description>&lt;P&gt;Thank you for your reply.&lt;BR /&gt;When I tried it right away, I was able to see changes in the voltage level of the waveform.&lt;/P&gt;&lt;P&gt;If you know where this setting is located in the source code, could you please let me know?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Yoshihara&lt;/P&gt;</description>
      <pubDate>Tue, 07 Nov 2023 03:49:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-IMX8MP-TMDS-voltage-level/m-p/1753207#M215337</guid>
      <dc:creator>Yoshiharaaa</dc:creator>
      <dc:date>2023-11-07T03:49:58Z</dc:date>
    </item>
    <item>
      <title>Re: About IMX8MP TMDS voltage level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-IMX8MP-TMDS-voltage-level/m-p/1753807#M215410</link>
      <description>&lt;P&gt;this isn't from source code, they are registers, you can find them from reference manual,&lt;/P&gt;
&lt;P&gt;you can search 13.10.3.1.1 HDMI_TX_PHY memory map from reference manual&lt;/P&gt;
&lt;P&gt;the base address is 32FD_0000h, then you can find these registers&lt;/P&gt;
&lt;P&gt;if you need to know where define them you can refer to the dtis file&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mp.dtsi&amp;quot;" target="_blank"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mp.dtsi"&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;this dtsi file define the phy base address, and phy driver is&lt;/P&gt;
&lt;P&gt;"&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/phy/freescale/phy-fsl-samsung-hdmi.c" target="_blank"&gt;https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/phy/freescale/phy-fsl-samsung-hdmi.c&lt;/A&gt;":&lt;/P&gt;</description>
      <pubDate>Wed, 08 Nov 2023 03:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-IMX8MP-TMDS-voltage-level/m-p/1753807#M215410</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2023-11-08T03:06:28Z</dc:date>
    </item>
    <item>
      <title>Re: About IMX8MP TMDS voltage level</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-IMX8MP-TMDS-voltage-level/m-p/1755225#M215530</link>
      <description>&lt;P&gt;Thank you for your support in this matter.&lt;BR /&gt;I will try using the information you provided.&lt;/P&gt;&lt;P&gt;Thank you.&lt;BR /&gt;yoshihara&lt;/P&gt;</description>
      <pubDate>Fri, 10 Nov 2023 00:34:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-IMX8MP-TMDS-voltage-level/m-p/1755225#M215530</guid>
      <dc:creator>Yoshiharaaa</dc:creator>
      <dc:date>2023-11-10T00:34:41Z</dc:date>
    </item>
  </channel>
</rss>