<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: iMX8MP EVK NXP9098 Wifi 6 Module Issues in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-EVK-NXP9098-Wifi-6-Module-Issues/m-p/1755027#M215512</link>
    <description>&lt;P&gt;&amp;nbsp;HI &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204464"&gt;@user123412&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;To run Wi-Fi, execute the following commands first and follow common commands below:&lt;BR /&gt;• For the following steps, execute these commands using connman&lt;BR /&gt;modprobe moal mod_para=nxp/wifi_mod_para.conf&lt;BR /&gt;$connmanctl&lt;BR /&gt;connmanctl&amp;gt; enable wifi&lt;BR /&gt;connmanctl&amp;gt; scan wifi&lt;BR /&gt;connmanctl&amp;gt; services /* This should list of the network. For&lt;BR /&gt;example wifi_c0e4347f5053_4a62726f_managed_psk*/&lt;BR /&gt;connmanctl&amp;gt; agent on&lt;BR /&gt;connmanctl&amp;gt; connect wifi_c0e4347f5053_4a62726f_managed_psk /* Enter Passphrase */&lt;BR /&gt;Agent RequestInput wifi_c0e4347f5053_4a62726f_managed_psk&lt;BR /&gt;Passphrase = [ Type=psk, Requirement=mandatory ]&lt;BR /&gt;Passphrase?&lt;BR /&gt;connmanctl&amp;gt; quit&lt;/P&gt;
&lt;P&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
    <pubDate>Thu, 09 Nov 2023 14:38:53 GMT</pubDate>
    <dc:creator>Chavira</dc:creator>
    <dc:date>2023-11-09T14:38:53Z</dc:date>
    <item>
      <title>iMX8MP EVK NXP9098 Wifi 6 Module Issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-EVK-NXP9098-Wifi-6-Module-Issues/m-p/1754462#M215470</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using the NXP iMX8MP EVK board, and I am trying to bring up the Murata 2XS module. Based on all of the documentation I have seen, the 9098 chipset should be well supported in kernels 5.10 and 5.15. However, I keep seeing the following issues. Here is the installed firmware:&lt;/P&gt;&lt;P&gt;root@imx8mp-lpddr4-evk:~# ls /lib/firmware/nxp/&lt;BR /&gt;ed_mac_ctrl_V3_8987.conf ed_mac_ctrl_V3_909x.conf pcieuart9098_combo_v1.bin sdiouart8997_combo_v4.bin txpwrlimit_cfg_8987.conf txpwrlimit_cfg_9098.conf&lt;BR /&gt;ed_mac_ctrl_V3_8997.conf pcieuart8997_combo_v4.bin sdiouart8987_combo_v0.bin sdiouartiw416_combo_v0.bin txpwrlimit_cfg_8997.conf wifi_mod_para.conf&lt;/P&gt;&lt;P&gt;I am able to load the moal.ko driver successfully:&lt;/P&gt;&lt;P&gt;root@imx8mp-lpddr4-evk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf&lt;BR /&gt;[ 24.035644] mlan: loading out-of-tree module taints kernel.&lt;BR /&gt;[ 24.060983] wlan: Loading MWLAN driver&lt;BR /&gt;[ 24.065354] wlan_pcie 0000:01:00.0: enabling device (0000 -&amp;gt; 0002)&lt;BR /&gt;[ 24.071650] Attach moal handle ops, card interface type: 0x206&lt;BR /&gt;[ 24.078985] PCIE9098: init module param from usr cfg&lt;BR /&gt;[ 24.083999] card_type: PCIE9098, config block: 0&lt;BR /&gt;[ 24.088647] cfg80211_wext=0xf&lt;BR /&gt;[ 24.091633] wfd_name=p2p&lt;BR /&gt;[ 24.094165] max_vir_bss=1&lt;BR /&gt;[ 24.096811] cal_data_cfg=none&lt;BR /&gt;[ 24.099805] drv_mode = 7&lt;BR /&gt;[ 24.102337] ps_mode = 2&lt;BR /&gt;[ 24.104797] auto_ds = 2&lt;BR /&gt;[ 24.107256] mac_addr=00:50:43:20:12:34&lt;BR /&gt;[ 24.111017] fw_name=nxp/pcieuart9098_combo_v1.bin&lt;BR /&gt;[ 24.115748] rx_work=1 cpu_num=4&lt;BR /&gt;[ 24.118919] Attach mlan adapter operations.card_type is 0x206.&lt;BR /&gt;[ 24.126696] Request firmware: nxp/pcieuart9098_combo_v1.bin&lt;BR /&gt;[ 24.687599] FW download over, size 620764 bytes&lt;BR /&gt;[ 26.094985] WLAN FW is active&lt;BR /&gt;[ 26.097961] on_time is 26095308500&lt;BR /&gt;[ 26.125964] fw_cap_info=0x81c3fa3, dev_cap_mask=0xffffffff&lt;BR /&gt;[ 26.131483] max_p2p_conn = 8, max_sta_conn = 64&lt;BR /&gt;[ 26.152477] wlan: version = PCIE9098--17.92.5.p9-MM5X17266.p4-GPL-(FP92)&lt;BR /&gt;[ 26.161466] wlan_pcie 0000:01:00.1: enabling device (0000 -&amp;gt; 0002)&lt;BR /&gt;[ 26.167872] Attach moal handle ops, card interface type: 0x206&lt;BR /&gt;[ 26.173946] PCIE9098: init module param from usr cfg&lt;BR /&gt;[ 26.179058] card_type: PCIE9098, config block: 1&lt;BR /&gt;[ 26.183809] cfg80211_wext=0xf&lt;BR /&gt;[ 26.186897] wfd_name=p2p&lt;BR /&gt;[ 26.189435] max_vir_bss=1&lt;BR /&gt;[ 26.192139] cal_data_cfg=none&lt;BR /&gt;[ 26.195148] drv_mode = 7&lt;BR /&gt;[ 26.197686] ps_mode = 2&lt;BR /&gt;[ 26.200184] auto_ds = 2&lt;BR /&gt;[ 26.202707] mac_addr=00:50:43:20:52:56&lt;BR /&gt;[ 26.206461] fw_name=nxp/pcieuart9098_combo_v1.bin&lt;BR /&gt;[ 26.211241] rx_work=1 cpu_num=4&lt;BR /&gt;[ 26.214403] Attach mlan adapter operations.card_type is 0x206.&lt;BR /&gt;[ 26.226714] Request firmware: nxp/pcieuart9098_combo_v1.bin&lt;BR /&gt;[ 26.233018] WLAN FW already running! Skip FW download&lt;BR /&gt;[ 26.238142] WLAN FW is active&lt;BR /&gt;[ 26.241188] on_time is 26238534875&lt;BR /&gt;[ 26.248470] fw_cap_info=0x81c3fa3, dev_cap_mask=0xffffffff&lt;BR /&gt;[ 26.254081] max_p2p_conn = 8, max_sta_conn = 64&lt;BR /&gt;[ 26.277970] wlan: version = PCIE9098--17.92.5.p9-MM5X17266.p4-GPL-(FP92)&lt;BR /&gt;[ 26.285658] wlan: Driver loaded successfully&lt;/P&gt;&lt;P&gt;and bring up mlan0:&lt;/P&gt;&lt;P&gt;mlan0: flags=4099&amp;lt;UP,BROADCAST,MULTICAST&amp;gt; mtu 1500&lt;BR /&gt;ether 00:50:43:20:12:34 txqueuelen 1000 (Ethernet)&lt;BR /&gt;RX packets 0 bytes 0 (0.0 B)&lt;BR /&gt;RX errors 0 dropped 0 overruns 0 frame 0&lt;BR /&gt;TX packets 0 bytes 0 (0.0 B)&lt;BR /&gt;TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0&lt;/P&gt;&lt;P&gt;However, I cannot scan or connect to any networks:&lt;/P&gt;&lt;P&gt;root@imx8mp-lpddr4-evk:~# iw dev mlan0 scan&lt;BR /&gt;[ 485.683433] wlan: mlan0 START SCAN&lt;BR /&gt;[ 489.793052] wlan: SCAN COMPLETED: scanned AP count=0&lt;/P&gt;&lt;P&gt;root@imx8mp-lpddr4-evk:~# wpa_supplicant -i mlan0 -D nl80211 -c /etc/wpa_supplicant.conf -B&lt;BR /&gt;Successfully initialized wpa_supplicant&lt;BR /&gt;rfkill: Cannot open RFKILL control device&lt;BR /&gt;root@imx8mp-lpddr4-evk:~# [ 599.874409] wlan: mlan0 START SCAN&lt;BR /&gt;[ 603.983857] wlan: SCAN COMPLETED: scanned AP count=0&lt;BR /&gt;[ 608.994992] wlan: mlan0 START SCAN&lt;BR /&gt;[ 613.104496] wlan: SCAN COMPLETED: scanned AP count=0&lt;BR /&gt;[ 618.116040] wlan: mlan0 START SCAN&lt;BR /&gt;[ 622.222534] wlan: SCAN COMPLETED: scanned AP count=0&lt;BR /&gt;[ 811.540517] wlan: mlan0 START SCAN&lt;BR /&gt;[ 815.650045] wlan: SCAN COMPLETED: scanned AP count=0&lt;/P&gt;&lt;P&gt;I also don't see any RX/TX activity in ifconfig at all.&lt;/P&gt;&lt;P&gt;I have tried building the 5.15.32 BSP with the following commands:&lt;/P&gt;&lt;P&gt;repo init -u &lt;A href="https://github.com/nxp-imx/imx-manifest" target="_blank" rel="noopener"&gt;https://github.com/nxp-imx/imx-manifest&lt;/A&gt; -b imx-linux-kirkstone -m imx-5.15.32-2.0.0.xml&lt;BR /&gt;repo sync&lt;/P&gt;&lt;P&gt;MACHINE=imx8mp-lpddr4-evk DISTRO=fsl-imx-wayland source ./imx-setup-release.sh -b build_8mp_evk&lt;BR /&gt;bitbake imx-image-core&lt;/P&gt;&lt;P&gt;and I have also tried building the Hardknott-5.10.52 release according to this guide from Murata:&amp;nbsp;&lt;A href="https://www.murata.com/-/media/webrenewal/products/connectivitymodule/asset/pub/rfm/data/murata_user_guide_linux_nxp.ashx" target="_blank" rel="noopener"&gt;https://www.murata.com/-/media/webrenewal/products/connectivitymodule/asset/pub/rfm/data/murata_user_guide_linux_nxp.ashx&lt;/A&gt;&amp;nbsp; but the same issues are present.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Nov 2023 21:23:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-EVK-NXP9098-Wifi-6-Module-Issues/m-p/1754462#M215470</guid>
      <dc:creator>user123412</dc:creator>
      <dc:date>2023-11-08T21:23:33Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP EVK NXP9098 Wifi 6 Module Issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-EVK-NXP9098-Wifi-6-Module-Issues/m-p/1755027#M215512</link>
      <description>&lt;P&gt;&amp;nbsp;HI &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204464"&gt;@user123412&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;To run Wi-Fi, execute the following commands first and follow common commands below:&lt;BR /&gt;• For the following steps, execute these commands using connman&lt;BR /&gt;modprobe moal mod_para=nxp/wifi_mod_para.conf&lt;BR /&gt;$connmanctl&lt;BR /&gt;connmanctl&amp;gt; enable wifi&lt;BR /&gt;connmanctl&amp;gt; scan wifi&lt;BR /&gt;connmanctl&amp;gt; services /* This should list of the network. For&lt;BR /&gt;example wifi_c0e4347f5053_4a62726f_managed_psk*/&lt;BR /&gt;connmanctl&amp;gt; agent on&lt;BR /&gt;connmanctl&amp;gt; connect wifi_c0e4347f5053_4a62726f_managed_psk /* Enter Passphrase */&lt;BR /&gt;Agent RequestInput wifi_c0e4347f5053_4a62726f_managed_psk&lt;BR /&gt;Passphrase = [ Type=psk, Requirement=mandatory ]&lt;BR /&gt;Passphrase?&lt;BR /&gt;connmanctl&amp;gt; quit&lt;/P&gt;
&lt;P&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Thu, 09 Nov 2023 14:38:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-EVK-NXP9098-Wifi-6-Module-Issues/m-p/1755027#M215512</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2023-11-09T14:38:53Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP EVK NXP9098 Wifi 6 Module Issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-EVK-NXP9098-Wifi-6-Module-Issues/m-p/1757819#M215777</link>
      <description>&lt;P&gt;Thanks, I have been able to enter the commands to scan for access points on any BSP I have tried, the issue is that on all of the 5.10 and 5.15 BSPs I have tried, no access points are found:&lt;/P&gt;&lt;P&gt;For example, the 5.10.52 image here from NXP has this issue:&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/sps/download/preDownload.jsp" target="_blank" rel="noopener"&gt;https://www.nxp.com/webapp/sps/download/preDownload.jsp&lt;/A&gt;&lt;/P&gt;&lt;P&gt;root@imx8mpevk:~# iw dev mlan0 scan&lt;BR /&gt;[ 363.953055] wlan: mlan0 START SCAN&lt;BR /&gt;[ 368.062051] wlan: SCAN COMPLETED: scanned AP count=0&lt;/P&gt;&lt;P&gt;but the 6.1 image here works and I am able to scan, connect, etc. to Wifi:&amp;nbsp;&lt;A title="" href="https://www.nxp.com/webapp/Download?colCode=L6.1.36_2.1.0_MX8MP&amp;amp;appType=license" target="_blank" rel="noopener noreferrer"&gt;https://www.nxp.com/webapp/Download?colCode=L6.1.36_2.1.0_MX8MP&amp;amp;appType=license&lt;/A&gt;&lt;/P&gt;&lt;P&gt;root@imx8mpevk:~# iw dev mlan0 scan&lt;BR /&gt;[ 236.071394] wlan: mlan0 START SCAN&lt;BR /&gt;[ 239.237120] wlan: SCAN COMPLETED: scanned AP count=19&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can someone point me in the direction of a 5.10 or 5.15 BSP image to flash onto the MX8MP EVK that has functionality for 9098 PCIe/UART? According to NXP/Murata, these kernel versions should work with the 9098 chipset&lt;/P&gt;</description>
      <pubDate>Wed, 15 Nov 2023 19:12:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-EVK-NXP9098-Wifi-6-Module-Issues/m-p/1757819#M215777</guid>
      <dc:creator>user123412</dc:creator>
      <dc:date>2023-11-15T19:12:00Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP EVK NXP9098 Wifi 6 Module Issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-EVK-NXP9098-Wifi-6-Module-Issues/m-p/1757855#M215780</link>
      <description>&lt;P&gt;It looks like the 5.15.71_2.2.1_MX8MP release also works, is there a 5.10 release that is functional?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Nov 2023 20:01:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-EVK-NXP9098-Wifi-6-Module-Issues/m-p/1757855#M215780</guid>
      <dc:creator>user123412</dc:creator>
      <dc:date>2023-11-15T20:01:52Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP EVK NXP9098 Wifi 6 Module Issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-EVK-NXP9098-Wifi-6-Module-Issues/m-p/1757984#M215792</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204464"&gt;@user123412&lt;/a&gt;!&lt;BR /&gt;&lt;BR /&gt;According to our Linux user guide the driver installed on version 5.10.72 supports the wifi module that you are using.&lt;BR /&gt;&lt;BR /&gt;I attached the User Guide for that version, also you can download the documentation and the images to test by following the link:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Thu, 16 Nov 2023 02:29:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-EVK-NXP9098-Wifi-6-Module-Issues/m-p/1757984#M215792</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2023-11-16T02:29:50Z</dc:date>
    </item>
  </channel>
</rss>