<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MIMXRT1170-EVK Boot from Flash troubleshooting in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1170-EVK-Boot-from-Flash-troubleshooting/m-p/1754705#M215489</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207397"&gt;@PeteHawkins&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Which&amp;nbsp;&lt;SPAN&gt;demo app was got stuck in the end?&amp;nbsp; Have you run the demo of&amp;nbsp;SDK_2_14_0_MIMXRT1170-EVK\boards\evkmimxrt1170\driver_examples\flexspi\nor\polling_transfer\cm7 ? did it work as expected? Please kindly clarify.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 09 Nov 2023 06:56:06 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2023-11-09T06:56:06Z</dc:date>
    <item>
      <title>MIMXRT1170-EVK Boot from Flash troubleshooting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1170-EVK-Boot-from-Flash-troubleshooting/m-p/1753673#M215390</link>
      <description>&lt;P&gt;I am using a MIMXRT1170-EVK with MCUXpresso and a J-Link Ultra+ for programming/debugging.&amp;nbsp; This was initially working perfectly with the default QSPI NOR Flash and a variety of the SDK demo applications.&lt;/P&gt;&lt;P&gt;I wanted to switch to Octal Flash, so I changed the resistor and DIP switch settings, but could not get applications to run from the octal flash.&amp;nbsp; The fsl_romapi_cm7 demo app linked to run from RAM also reported an error trying to identify the flash.&amp;nbsp; So, I changed the resistors and DIP switches back to the initial settings for QSPI flash.&lt;/P&gt;&lt;P&gt;On first power up after changing things back, the last demo application I had used with the QSPI flash booted and ran as expected.&amp;nbsp; The fsl_romapi_cm7 demo app (run from RAM) also runs and completes successfully.&amp;nbsp; However, now when I try to program and debug a demo app from the QSPI flash, it appears to get stuck in the NXP ROM bootloader.&amp;nbsp; I have quadruple checked that the resistors are set correctly (and I can apparently read and program the flash successfully), and the DIP switches are set for Internal Boot from QSPI (all switches off except SW1-3).&lt;/P&gt;&lt;P&gt;If I click the "pause" button in MCUXpresso, it breaks with the PC register at 0x23104, which is somewhere in the bootloader ROM.&amp;nbsp; If I dump memory I see the FCFB at 0x30000400 and the Program Vector table at 0x30001030.&amp;nbsp; The program vector table has a program entrypoint of 0x300024e9, and the code at 0x300024e9 appears to be a valid entry point (ResetISR) for the demo app.&lt;/P&gt;&lt;P&gt;How should I go about troubleshooting this to determine why it isn't booting correctly?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Pete&lt;/P&gt;</description>
      <pubDate>Tue, 07 Nov 2023 19:06:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1170-EVK-Boot-from-Flash-troubleshooting/m-p/1753673#M215390</guid>
      <dc:creator>PeteHawkins</dc:creator>
      <dc:date>2023-11-07T19:06:21Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK Boot from Flash troubleshooting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1170-EVK-Boot-from-Flash-troubleshooting/m-p/1754705#M215489</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207397"&gt;@PeteHawkins&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Which&amp;nbsp;&lt;SPAN&gt;demo app was got stuck in the end?&amp;nbsp; Have you run the demo of&amp;nbsp;SDK_2_14_0_MIMXRT1170-EVK\boards\evkmimxrt1170\driver_examples\flexspi\nor\polling_transfer\cm7 ? did it work as expected? Please kindly clarify.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 09 Nov 2023 06:56:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1170-EVK-Boot-from-Flash-troubleshooting/m-p/1754705#M215489</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2023-11-09T06:56:06Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK Boot from Flash troubleshooting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1170-EVK-Boot-from-Flash-troubleshooting/m-p/1755101#M215517</link>
      <description>&lt;P&gt;All apps fail if run from Flash, and work if run from RAM.&amp;nbsp; I have found, that switching from J-Link to CMSIS-DAP fixes the problem.&amp;nbsp; If I switch back to J-Link, it fails again in the same way.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Nov 2023 17:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1170-EVK-Boot-from-Flash-troubleshooting/m-p/1755101#M215517</guid>
      <dc:creator>PeteHawkins</dc:creator>
      <dc:date>2023-11-09T17:25:34Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVK Boot from Flash troubleshooting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1170-EVK-Boot-from-Flash-troubleshooting/m-p/1820922#M220751</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207397"&gt;@PeteHawkins&lt;/a&gt;&amp;nbsp;,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I believe I am having very similar issues. Were you ever able to come up with a solution to this problem? Thanks!!&lt;/P&gt;</description>
      <pubDate>Mon, 04 Mar 2024 23:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMXRT1170-EVK-Boot-from-Flash-troubleshooting/m-p/1820922#M220751</guid>
      <dc:creator>myee_</dc:creator>
      <dc:date>2024-03-04T23:53:46Z</dc:date>
    </item>
  </channel>
</rss>